AM261x MCU+ SDK  11.01.00
ADC Global Force

Introduction

This example demonstrates the Global SOC force feature. The ADCs that need to be forced globally are first selected in the Global Control using the API SOC_enableAdcGlobalForce with the instance number and the enable (TRUE/ FALSE) as arguments. then the API SOC_adcSocGlobalForce can be used to set a software trigger globally on the given SOC number at all the ADCs selected above.

Configurations

  • ADCx SOC0 is configured for Software only trigger and generate interrupt at EOC0. x is 0,1,2,3,4.

External Connections

External connections are arbitrary for this feature demonstration. for instance, ADC0 SOC0 is configured for Channel 0. Feed Analog voltages on ADC0_AIN2

AM263Px-CC E2 or AM261x-SOM E1

  • ADC0_AIN2, i.e., HSEC PIN 15

AM263Px-LP

  • ADC0_AIN2, i.e., J5/7 PIN 66

AM261x-LP

  • ADC0_AIN2, i.e., J5/7 PIN 63

Watch Variables

The below watch variables can be used to view ADC conversion results.

  • gAdc0Results[] : Digital representation of the voltage converted by ADC0 when triggered by Global Software force
  • gAdc1Results[] : Digital representation of the voltage converted by ADC1 when triggered by Global Software force
  • gAdc2Results[] : Digital representation of the voltage converted by ADC2 when triggered by Global Software force
  • gAdc3Results[] : Digital representation of the voltage converted by ADC3 when triggered by Global Software force
  • gAdc4Results[] : Digital representation of the voltage converted by ADC4 when triggered by Global Software force

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am261x-som, am261x-lp
Example folder examples/drivers/adc/adc_global_force/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Using watch variables, view the ADC conversion results.
  • View the ADC conversion results in UART console logs

See Also

ADC

Sample Output

Shown below is a sample output when the application is run,

ADC Triggered by Global Software Force Test Started ...
ADC Triggered by Global Software Force Test Passed
All tests have passed!!