diff --git a/source/drivers/mailbox/v0/mailbox.c b/source/drivers/mailbox/v0/mailbox.c
index 6f9811eb74..1a7f16b1c0 100644
--- a/source/drivers/mailbox/v0/mailbox.c
+++ b/source/drivers/mailbox/v0/mailbox.c
@@ -32,6 +32,23 @@
  */
 
 #include "mailbox_priv.h"
+#include <kernel/dpl/HwiP.h>
+#include <kernel/dpl/ClockP.h>
+
+/* mailbox registers */
+#define R4F_BSS_MBOX_READ_REQ    (CSL_RSS_PROC_CTRL_U_BASE + 0x0CU)
+#define R4F_BSS_MBOX_READ_DONE   (CSL_RSS_PROC_CTRL_U_BASE + 0x10U)
+
+/* CPU bit positions within the mailbox registers */
+#define R5FSS0_0_MBOX_PROC_BIT_POS  ( 0U)
+#define R5FSS0_1_MBOX_PROC_BIT_POS  ( 4U)
+#define RSS_R4_MBOX_PROC_BIT_POS    (12u)
+#define C66SS0_MBOX_PROC_BIT_POS    (16U)
+
+/* A delay of 0.5uSec is recommended before clear pending read request from remote core
+ * This delay is implemented as a loop and is profiled to be approximately 0.6uSec
+ */
+#define MAILBOX_WAIT_CYCLES          (17U)
 
 /* global state of mailbox communication */
 Mailbox_Ctrl gMailbox_ctrl;
@@ -64,16 +81,31 @@ static inline void Mailbox_sendReadAckIntr(const Mailbox_RemoteCoreObj *obj)
     *addr = (uint32_t)(1UL << obj->readAckIntrBitPos);
 }
 
+ #if defined(__aarch64__) || defined(__arm__)
+static inline void Mailbox_dataAndInstructionBarrier(void)
+{
+ __asm__ __volatile__ ( "dsb sy"  "\n\t": : : "memory");
+ __asm__ __volatile__ ( "isb sy"     "\n\t": : : "memory");
+}
+#endif
+
 static int32_t Mailbox_waitWriteAckIntr(const Mailbox_RemoteCoreObj *obj, uint32_t timeToWaitInTicks)
 {
     int32_t status = SystemP_FAILURE;
     uint32_t done = 0, isAck;
     uint32_t curTicks = ClockP_getTicks(), elaspedTicks;
+    volatile uint32_t loopCounter = 0U;
 
     do {
         isAck = Mailbox_isWriteAckIntr(obj);
         if(isAck != 0U)
         {
+            /*
+            * Added delay here so that trasmitting core have sufficient time
+            * to ensure the readback of acknowledgement is correct.
+            */
+            for(loopCounter = 0; loopCounter < MAILBOX_WAIT_CYCLES; loopCounter++);
+
             Mailbox_clearWriteAckIntr(obj);
             status = SystemP_SUCCESS;
             done = 1;
@@ -178,6 +210,9 @@ uint32_t Mailbox_isCoreEnabled(uint32_t coreId)
 int32_t Mailbox_write(uint32_t remoteCoreId, const uint8_t *buffer, uint32_t size, uint32_t timeToWaitInTicks)
 {
     int32_t status = SystemP_FAILURE;
+    uint8_t loop = 0U;
+    uint32_t oldIntState;
+    volatile uint32_t *prtrBSSMboxReadReq = (volatile uint32_t *)R4F_BSS_MBOX_READ_REQ;
 
     if(    (buffer != NULL)
         && (size > 0U)
@@ -190,8 +225,7 @@ int32_t Mailbox_write(uint32_t remoteCoreId, const uint8_t *buffer, uint32_t siz
             (void)memcpy(obj->writeShmBuffer, buffer, size);
 
             #if defined(__aarch64__) || defined(__arm__)
-            __asm__ __volatile__ ( "dsb sy"  "\n\t": : : "memory");
-            __asm__ __volatile__ ( "isb sy"     "\n\t": : : "memory");
+            Mailbox_dataAndInstructionBarrier();
             #endif
             #if defined(_TMS320C6X)
             _mfence();
@@ -199,7 +233,31 @@ int32_t Mailbox_write(uint32_t remoteCoreId, const uint8_t *buffer, uint32_t siz
             #endif
 
             Mailbox_clearWriteAckIntr(obj);
-            Mailbox_sendWriteIntr(obj);
+
+            oldIntState = HwiP_disable();
+            do
+            {
+                Mailbox_sendWriteIntr(obj);
+
+                #if defined(__aarch64__) || defined(__arm__)
+
+                /* Check for the read request confirmation */
+                if(*prtrBSSMboxReadReq & (1U << R5FSS0_0_MBOX_PROC_BIT_POS))
+                    break;
+
+                #endif
+
+                #if defined(_TMS320C6X)
+
+                /* Check for the read request confirmation */
+                if(*prtrBSSMboxReadReq & (1U << C66SS0_MBOX_PROC_BIT_POS))
+                    break;
+
+                #endif
+
+            } while (++loop < 3U);
+
+            HwiP_restore(oldIntState);
 
             status = SystemP_SUCCESS;
 
@@ -247,7 +305,10 @@ int32_t Mailbox_read(uint32_t remoteCoreId, uint8_t *buffer, uint32_t size, uint
 
 int32_t Mailbox_readDone(uint32_t remoteCoreId)
 {
+    uint8_t loop = 0U;
+    uintptr_t oldIntState;
     int32_t status = SystemP_FAILURE;
+    volatile uint32_t *ptrBSSMboxReadDone = (volatile uint32_t *)R4F_BSS_MBOX_READ_DONE;
 
     if(  Mailbox_isCoreEnabled(remoteCoreId) != 0U )
     {
@@ -255,7 +316,30 @@ int32_t Mailbox_readDone(uint32_t remoteCoreId)
 
         obj->curReadSize = 0U;
 
-        Mailbox_sendReadAckIntr(obj);
+        oldIntState = HwiP_disable();
+        do
+        {
+            Mailbox_sendReadAckIntr(obj);
+
+            if(remoteCoreId == CSL_CORE_ID_RSS_R4)
+            {
+                if(*ptrBSSMboxReadDone & (1U << R5FSS0_0_MBOX_PROC_BIT_POS))
+                {
+                    break;
+                }
+                else if(*ptrBSSMboxReadDone & (1U << C66SS0_MBOX_PROC_BIT_POS))
+                {
+
+                    break;
+                }
+                else
+                {
+                    /* */
+                }
+            }
+        } while (++loop < 3);
+
+        HwiP_restore(oldIntState);
 
         status = SystemP_SUCCESS;
     }