diff --git a/source/drivers/ipc_rpmsg/ipc_rpmsg.c b/source/drivers/ipc_rpmsg/ipc_rpmsg.c
index 95212bce53..dc254758a8 100755
--- a/source/drivers/ipc_rpmsg/ipc_rpmsg.c
+++ b/source/drivers/ipc_rpmsg/ipc_rpmsg.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2018-2021 Texas Instruments Incorporated
+ *  Copyright (C) 2018-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -97,7 +97,7 @@ int32_t RPMessage_getEndPtMsg(RPMessage_Object *obj, RPMessage_QueueElem **pMsg,
             {
                 done = 1;
             }
-            if(status == SystemP_SUCCESS && obj->doRecvUnblock)
+            if((status == SystemP_SUCCESS) && ((obj->doRecvUnblock)!=0U))
             {
                 status = SystemP_TIMEOUT;
                 done = 1;
@@ -108,7 +108,7 @@ int32_t RPMessage_getEndPtMsg(RPMessage_Object *obj, RPMessage_QueueElem **pMsg,
             status = SystemP_SUCCESS;
             done = 1;
         }
-    } while( ! done );
+    } while(done!=1U);
 
     return status;
 }
@@ -194,17 +194,17 @@ void RPMessage_recvHandler(uint32_t remoteCoreId)
 
 void RPMessage_notifyCallback(uint32_t remoteCoreId, uint16_t localClientId, uint32_t msgValue, void *args)
 {
-    if(gIpcRpmsgCtrl.isCoreEnable[remoteCoreId] && gIpcRpmsgCtrl.isCoreInitialized[remoteCoreId])
+    if((gIpcRpmsgCtrl.isCoreEnable[remoteCoreId]!=0U) && (gIpcRpmsgCtrl.isCoreInitialized[remoteCoreId]!=0U))
     {
         uint16_t rxMsgValue = RPMESSAGE_MSG_VRING_NEW_FULL;
 
-        if(RPMessage_isLinuxCore(remoteCoreId))
+        if((RPMessage_isLinuxCore(remoteCoreId)!=0U))
         {
             rxMsgValue = RPMESSAGE_LINUX_RX_VRING_ID; /* In linux, we get RX VRING ID, which is 1 in linux */
         }
         if(msgValue == rxMsgValue)
         {   /* check full ring */
-            while(RPMessage_vringIsFullRxBuf(remoteCoreId))
+            while((RPMessage_vringIsFullRxBuf(remoteCoreId)!=0U))
             {
                 RPMessage_recvHandler(remoteCoreId);
             }
@@ -226,10 +226,11 @@ int32_t RPMessage_send( void*    data,
                         uint32_t timeout
                       )
 {
+    uint16_t dataLength = dataLen;
     int32_t status = SystemP_FAILURE;
 
-    if(remoteCoreId < CSL_CORE_ID_MAX && gIpcRpmsgCtrl.isCoreEnable[remoteCoreId]
-        && data != NULL && dataLen != 0
+    if(((remoteCoreId < CSL_CORE_ID_MAX)) && ((gIpcRpmsgCtrl.isCoreEnable[remoteCoreId] != 0U))
+        && ((data != NULL)) && ((dataLength != 0U)) && (localEndPt < RPMESSAGE_MAX_LOCAL_ENDPT)
         )
     {
         uint16_t vringBufId;
@@ -241,9 +242,9 @@ int32_t RPMessage_send( void*    data,
             uint16_t vringBufLen = RPMessage_vringGetTxBufLen(remoteCoreId, vringBufId);
             RPMessage_Header *header = (RPMessage_Header *)vringBufAddr;
 
-            if(dataLen > (vringBufLen - sizeof(RPMessage_Header)) )
+            if(dataLength > (vringBufLen - sizeof(RPMessage_Header)) )
             {
-                dataLen = vringBufLen - sizeof(RPMessage_Header);
+                dataLength = vringBufLen - sizeof(RPMessage_Header);
 
                 DebugP_logWarn("[IPC RPMSG] Message send to remote core %d @ %d end point truncated due to lack of space in vring buffer !!!\r\n",
                     remoteCoreId, remoteEndPt);
@@ -253,11 +254,11 @@ int32_t RPMessage_send( void*    data,
             header->dstEndPt = remoteEndPt;
             header->srcCoreId = gIpcRpmsgCtrl.selfCoreId;
             header->flags = 0;
-            header->dataLen = dataLen;
+            header->dataLen = dataLength;
 
-            memcpy( &vringBufAddr[sizeof(RPMessage_Header)], data, dataLen);
+            memcpy((void *) &vringBufAddr[sizeof(RPMessage_Header)], (const void *) data, (size_t)dataLength);
 
-            RPMessage_vringPutFullTxBuf(remoteCoreId, vringBufId, dataLen + sizeof(RPMessage_Header));
+            RPMessage_vringPutFullTxBuf(remoteCoreId, vringBufId, dataLength + sizeof(RPMessage_Header));
         }
         else
         {
@@ -280,14 +281,14 @@ int32_t RPMessage_recv(RPMessage_Object *handle, void* data, uint16_t *dataLen,
     int32_t status = SystemP_FAILURE;
     RPMessage_Object *obj = handle;
 
-    if( data != NULL && dataLen != NULL && remoteCoreId != NULL && remoteEndPt != NULL
-        && obj->recvCallback == NULL /* i.e non-callback mode */
+   if( (data != NULL) && (dataLen != NULL) && (remoteCoreId != NULL) && (remoteEndPt != NULL)
+        && (obj->recvCallback == NULL) /* i.e non-callback mode */
       )
     {
         RPMessage_QueueElem *elem;

         status = RPMessage_getEndPtMsg(obj, &elem, timeout);
-        if(status == SystemP_SUCCESS && pMsg != NULL)
+        if((status == SystemP_SUCCESS) && (pMsg != NULL))
         {
             uint32_t isAllocPending = 0;
             uint16_t vringBufId = elem->vringBufId;
@@ -308,11 +309,11 @@ int32_t RPMessage_recv(RPMessage_Object *handle, void* data, uint16_t *dataLen,
                 *dataLen = header->dataLen;
             }
 
-            memcpy( data, &vringBufAddr[sizeof(RPMessage_Header)], *dataLen);
+            memcpy((void *) data,(const void *) &vringBufAddr[sizeof(RPMessage_Header)],(size_t) *dataLen);
 
             RPMessage_vringPutEmptyRxBuf(*remoteCoreId, vringBufId);
             isAllocPending = RPMessage_freeEndPtMsg(*remoteCoreId, elem);
-            if(isAllocPending)
+            if(isAllocPending!=0U)
             {   /* if any messages are pending message pointer due to free Q being empty,
                  * now there will be atleast one element to handle any pending vring requests.
                  * So check vring and handle pending messages if any
@@ -325,12 +326,9 @@ int32_t RPMessage_recv(RPMessage_Object *handle, void* data, uint16_t *dataLen,
         }
         else
         {
-            if(status != SystemP_TIMEOUT)
-            {
-                DebugP_logError("[IPC RPMSG] Message recv @ %d local end point failed due to invalid end point Q !!!\r\n",
+            DebugP_logError("[IPC RPMSG] Message recv @ %d local end point failed due to invalid end point Q !!!\r\n",
                     obj->localEndPt
                     );
-            }
         }
     }
     else
@@ -344,28 +342,39 @@ int32_t RPMessage_recv(RPMessage_Object *handle, void* data, uint16_t *dataLen,
 
void RPMessage_unblock(RPMessage_Object *obj)
{
+    if(obj != NULL)
    {
+    obj->doRecvUnblock = 1;
+    SemaphoreP_post(&obj->newEndPtMsgSem);
    }
}
 
uint16_t RPMessage_getLocalEndPt(const RPMessage_Object *obj)
{
+    DebugP_assert(obj != NULL);
+    return obj->localEndPt;
}
 
 int32_t RPMessage_construct(RPMessage_Object *handle, const RPMessage_CreateParams *createParams)
 {
-    RPMessage_Object *obj = handle;
+    RPMessage_Object *obj;
     int32_t status = SystemP_FAILURE;
 
-    if(createParams->localEndPt < RPMESSAGE_MAX_LOCAL_ENDPT
-        && gIpcRpmsgCtrl.localEndPtObj[createParams->localEndPt] == NULL)
+    if((handle != NULL) && (createParams != NULL))
+    {
+    obj = (RPMessage_Object *)handle;
+    if((createParams->localEndPt < RPMESSAGE_MAX_LOCAL_ENDPT)
+        && (gIpcRpmsgCtrl.localEndPtObj[createParams->localEndPt] == NULL))
     {
         obj->localEndPt = createParams->localEndPt;
         obj->recvCallback = createParams->recvCallback;
@@ -380,15 +389,19 @@ int32_t RPMessage_construct(RPMessage_Object *handle, const RPMessage_CreatePara
 
         status = SystemP_SUCCESS;
     }
+    }
     return status;
 }
 
 void RPMessage_destruct(RPMessage_Object *handle)
 {
+    RPMessage_Object *obj = handle;
 
-    if(obj->localEndPt < RPMESSAGE_MAX_LOCAL_ENDPT &&
-        gIpcRpmsgCtrl.localEndPtObj[obj->localEndPt] != NULL)
+    if(handle != NULL)
+    {
+    obj = (RPMessage_Object *)handle;
+    if((obj->localEndPt < RPMESSAGE_MAX_LOCAL_ENDPT) &&
+        (gIpcRpmsgCtrl.localEndPtObj[obj->localEndPt] != NULL))
     {
         gIpcRpmsgCtrl.localEndPtObj[obj->localEndPt] = NULL;
 
@@ -399,6 +412,7 @@ void RPMessage_destruct(RPMessage_Object *handle)
         RPMessage_queueReset(&obj->endPtQ);
         SemaphoreP_destruct(&obj->newEndPtMsgSem);
     }
+    }
 }
 
 void RPMessage_CreateParams_init(RPMessage_CreateParams *params)
@@ -414,6 +428,8 @@ void RPMessage_Params_init(RPMessage_Params *params)
 {
     uint16_t coreId;
 
+    if(params != NULL)
+    {
     memset(params, 0, sizeof(RPMessage_Params));
 
     for(coreId=0; coreId<CSL_CORE_ID_MAX; coreId++)
@@ -423,9 +439,10 @@ void RPMessage_Params_init(RPMessage_Params *params)
     }
     params->vringNumBuf = 8;
     params->vringMsgSize = 128;
-    params->vringSize = RPMESSAGE_VRING_SIZE(params->vringNumBuf, params->vringMsgSize);
+    params->vringSize = RPMESSAGE_VRING_SIZE((uint32_t)params->vringNumBuf, params->vringMsgSize);
     params->linuxCoreId = CSL_CORE_ID_MAX;
     params->linuxResourceTable = NULL;
+    }
 }
 
 int32_t  RPMessage_coreInit(uint16_t remoteCoreId, const RPMessage_Params *params)
@@ -442,7 +459,7 @@ int32_t  RPMessage_coreInit(uint16_t remoteCoreId, const RPMessage_Params *param
         RPMessage_queuePut(&coreObj->freeQ, &coreObj->localMsgObj[elemId]);
     }
     /* Linux VRINGs we will init later inside RPMessage_waitForLinuxReady() */
-    if(gIpcRpmsgCtrl.isCoreEnable[remoteCoreId] && !RPMessage_isLinuxCore(remoteCoreId))
+    if((gIpcRpmsgCtrl.isCoreEnable[remoteCoreId] != 0U) && (RPMessage_isLinuxCore(remoteCoreId) == 0U))
     {
         /* reset RX ring */
         RPMessage_vringReset(remoteCoreId, 0, params);
@@ -481,7 +498,7 @@ void RPMessage_controlEndPtHandler(RPMessage_Object *obj, void *arg,
         void *data, uint16_t dataLen,
         uint16_t remoteCoreId, uint16_t remoteEndPt)
 {
-    if(gIpcRpmsgCtrl.controlEndPtCallback)
+    if(gIpcRpmsgCtrl.controlEndPtCallback!=NULL)
     {
         /* check if message is of correct size */
         if(dataLen == sizeof(RPMessage_AnnounceMsg))
@@ -519,13 +536,15 @@ void RPMessage_controlEndPtDeInit(void)
 
 int32_t  RPMessage_announce(uint16_t remoteCoreId, uint16_t localEndPt, const char* name)
 {
-    int32_t status;
+    int32_t status = SystemP_FAILURE;
     RPMessage_AnnounceMsg msg;
 
+    if((remoteCoreId < CSL_CORE_ID_MAX) && (localEndPt < RPMESSAGE_MAX_LOCAL_ENDPT) && (name != NULL))
+    {
     msg.type = 0;
     msg.remoteEndPt = localEndPt; /* local end point will be remote end point for the other side */
-    strncpy(msg.name, name, RPMESSAGE_ANNOUNCE_SERVICENAME_LEN-1);
-    msg.name[RPMESSAGE_ANNOUNCE_SERVICENAME_LEN-1] = '\0';
+    strncpy(msg.name, name, RPMESSAGE_ANNOUNCE_SERVICENAME_LEN-1U);
+    msg.name[RPMESSAGE_ANNOUNCE_SERVICENAME_LEN-1U] = '\0';
 
     status = RPMessage_send(
                 &msg,
@@ -535,6 +554,7 @@ int32_t  RPMessage_announce(uint16_t remoteCoreId, uint16_t localEndPt, const ch
                 RPMESSAGE_CTRL_ENDPOINT_ID, /* reply or local end point, set also to control end point */
                 SystemP_WAIT_FOREVER /* wait until message is put in VRING */
     );
+    }
     return status;
 }
 
@@ -543,19 +563,21 @@ void RPMessage_controlEndPtCallback(RPMessage_ControlEndPtCallback controlEndPtC
 {
     uint32_t oldIntState;
 
-    oldIntState = HwiP_disable();
-
-    gIpcRpmsgCtrl.controlEndPtCallback = controlEndPtCallback;
-    gIpcRpmsgCtrl.controlEndPtCallbackArgs = controlEndPtCallbackArgs;
+    if(controlEndPtCallback != NULL)
+    {
+        oldIntState = HwiP_disable();
+        gIpcRpmsgCtrl.controlEndPtCallback = controlEndPtCallback;
+        gIpcRpmsgCtrl.controlEndPtCallbackArgs = controlEndPtCallbackArgs;
 
-    HwiP_restore(oldIntState);
+        HwiP_restore(oldIntState);
+    }
 }
 
 uint32_t RPMessage_isLinuxCore(uint16_t coreId)
 {
     uint32_t isLinuxCore = 0;
 
-    if(coreId == gIpcRpmsgCtrl.linuxCoreId && gIpcRpmsgCtrl.linuxResourceTable)
+    if((coreId == gIpcRpmsgCtrl.linuxCoreId) && (gIpcRpmsgCtrl.linuxResourceTable))
     {
         isLinuxCore = 1;
     }
@@ -567,7 +589,7 @@ int32_t  RPMessage_waitForLinuxReady(uint32_t timeout)
     int32_t status = SystemP_FAILURE;
     volatile RPMessage_ResourceTable *rscTable = (RPMessage_ResourceTable *)gIpcRpmsgCtrl.linuxResourceTable;
 
-    if(rscTable)
+    if(rscTable!=NULL)
     {
         uint32_t elaspedTicks, startTicks = ClockP_getTicks();
         do
@@ -622,6 +644,8 @@ int32_t  RPMessage_init(const RPMessage_Params *params)
     int32_t status = SystemP_SUCCESS;
     uint16_t coreId, localEndPtId;
 
+    if(params != NULL)
+    {
     gIpcRpmsgCtrl.selfCoreId = IpcNotify_getSelfCoreId();
     gIpcRpmsgCtrl.controlEndPtCallback = NULL;
     gIpcRpmsgCtrl.controlEndPtCallbackArgs = NULL;
@@ -640,19 +664,19 @@ int32_t  RPMessage_init(const RPMessage_Params *params)
          */
         gIpcRpmsgCtrl.isCoreEnable[coreId] = 0;
         gIpcRpmsgCtrl.isCoreInitialized[coreId] = 0;
-        if(params->vringTxBaseAddr[coreId] != RPMESSAGE_VRING_ADDR_INVALID
+       if((params->vringTxBaseAddr[coreId] != RPMESSAGE_VRING_ADDR_INVALID)
             &&
-            params->vringRxBaseAddr[coreId] != RPMESSAGE_VRING_ADDR_INVALID
+            (params->vringRxBaseAddr[coreId] != RPMESSAGE_VRING_ADDR_INVALID)
             &&
-            coreId != gIpcRpmsgCtrl.selfCoreId
+            (coreId != gIpcRpmsgCtrl.selfCoreId)
             &&
-            IpcNotify_isCoreEnabled(coreId)
+            ((IpcNotify_isCoreEnabled(coreId))!=0U)
           )
         {
             gIpcRpmsgCtrl.isCoreEnable[coreId] = 1;
         }
-        if(RPMessage_isLinuxCore(coreId)
-            && IpcNotify_isCoreEnabled(coreId)
+        if((RPMessage_isLinuxCore(coreId)!=0U)
+            && (IpcNotify_isCoreEnabled(coreId)!=0U)
             )
         {
             gIpcRpmsgCtrl.isCoreEnable[coreId] = 1;
@@ -661,16 +685,17 @@ int32_t  RPMessage_init(const RPMessage_Params *params)
     }
     for(coreId=0; coreId<CSL_CORE_ID_MAX; coreId++)
     {
-        status |= RPMessage_coreInit(coreId, params);
+        status += RPMessage_coreInit(coreId, params);
     }
 
     /* create control end point */
-    status |= RPMessage_controlEndPtInit();
+    status += RPMessage_controlEndPtInit();
 
     IpcNotify_registerClient(IPC_NOTIFY_CLIENT_ID_RPMSG,
         RPMessage_notifyCallback, NULL
         );
 
+    }
     return status;
 }
 
diff --git a/source/drivers/ipc_rpmsg/ipc_rpmsg_priv.h b/source/drivers/ipc_rpmsg/ipc_rpmsg_priv.h
index 27334eea6c..7072652951 100755
--- a/source/drivers/ipc_rpmsg/ipc_rpmsg_priv.h
+++ b/source/drivers/ipc_rpmsg/ipc_rpmsg_priv.h
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2018-2021 Texas Instruments Incorporated
+ *  Copyright (C) 2018-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -286,9 +286,17 @@ extern IpcRpmsg_Ctrl gIpcRpmsgCtrl;
 /* utility function to align a value, `align` MUST be power of 2 */
 static inline uint32_t RPMessage_align(uint32_t value, uint32_t align)
 {
-    return (value + align - 1) & ~(align-1);
+    return (value + align - 1U) & ~(align-1U);
 }
 
+ #if defined(__aarch64__) || defined(__arm__)
+static inline void IpcRpMsg_dataAndInstructionBarrier(void)
+{
+    __asm__ __volatile__ ( "dsb sy"  "\n\t": : : "memory");
+    __asm__ __volatile__ ( "isb sy"  "\n\t": : : "memory");
+}
+#endif
+
 /* utility function to find if core ID runs linux */
 uint32_t RPMessage_isLinuxCore(uint16_t coreId);
 
@@ -308,6 +316,21 @@ uint32_t RPMessage_vringGetSize(uint16_t numBuf, uint16_t msgSize, uint32_t alig
 void     RPMessage_vringReset(uint16_t remoteCoreId, uint16_t isTx, const RPMessage_Params *params);
 void     RPMessage_vringResetLinux(uint16_t remoteCoreId, uint16_t isTx, const RPMessage_ResourceTable *rscTable);
 
+void RPMessage_vringResetInternal(RPMessage_Vring *vringObj, uint16_t numBuf, uint16_t msgSize, uintptr_t vringBaseAddr, uint32_t offset_desc, uint32_t offset_avail, uint32_t offset_used, uint32_t offset_buf, uint32_t isTx);
+
+RPMessage_QueueElem *RPMessage_allocEndPtMsg(uint32_t remoteCoreId);
+uint32_t RPMessage_freeEndPtMsg(uint16_t remoteCoreId, RPMessage_QueueElem *elem);
+void RPMessage_putEndPtMsg(RPMessage_Object *obj, RPMessage_QueueElem *elem);
+int32_t RPMessage_getEndPtMsg(RPMessage_Object *obj, RPMessage_QueueElem **elem, uint32_t timeout);
+void RPMessage_recvHandler(uint32_t remoteCoreId);
+void RPMessage_notifyCallback(uint32_t remoteCoreId, uint16_t localClientId, uint32_t msgValue, void *args);
+int32_t  RPMessage_coreInit(uint16_t remoteCoreId, const RPMessage_Params *params);
+void RPMessage_coreDeInit(uint16_t remoteCoreId);
+void RPMessage_forceRecvMsgHandlers(void);
+void RPMessage_controlEndPtHandler(RPMessage_Object *obj, void *arg,void *data, uint16_t dataLen,uint16_t remoteCoreId, uint16_t remoteEndPt);
+int32_t RPMessage_controlEndPtInit(void);
+void RPMessage_controlEndPtDeInit(void);
+
 #ifdef __cplusplus
 }
 #endif
diff --git a/source/drivers/ipc_rpmsg/ipc_rpmsg_vring.c b/source/drivers/ipc_rpmsg/ipc_rpmsg_vring.c
index 83bc4e652d..85497a530d 100644
--- a/source/drivers/ipc_rpmsg/ipc_rpmsg_vring.c
+++ b/source/drivers/ipc_rpmsg/ipc_rpmsg_vring.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2018-2021 Texas Instruments Incorporated
+ *  Copyright (C) 2018-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -89,7 +89,7 @@ int32_t RPMessage_vringGetEmptyTxBuf(uint16_t remoteCoreId, uint16_t *vringBufId
             done = 1;
             status = SystemP_SUCCESS;
         }
-    } while( ! done );
+    } while(done!=1U);
 
     HwiP_restore(oldIntState);
 
@@ -104,7 +104,7 @@ void RPMessage_vringPutFullTxBuf(uint16_t remoteCoreId, uint16_t vringBufId, uin
     uint32_t oldIntState;
     uint32_t txMsgValue = RPMESSAGE_MSG_VRING_NEW_FULL;
 
-    if(RPMessage_isLinuxCore(remoteCoreId))
+    if(RPMessage_isLinuxCore(remoteCoreId) != 0U)
     {
         /* for linux we need to send the TX VRING ID in the mailbox message */
         txMsgValue = RPMESSAGE_LINUX_TX_VRING_ID;
@@ -118,8 +118,7 @@ void RPMessage_vringPutFullTxBuf(uint16_t remoteCoreId, uint16_t vringBufId, uin
     vringObj->used->idx++;
 
     #if defined(__aarch64__) || defined(__arm__)
-    __asm__ __volatile__ ( "dsb sy"  "\n\t": : : "memory");
-    __asm__ __volatile__ ( "isb sy"  "\n\t": : : "memory");
+    IpcRpMsg_dataAndInstructionBarrier();
     #endif
     #if defined(_TMS320C6X)
     _mfence();
@@ -151,7 +150,7 @@ void RPMessage_vringCheckEmptyTxBuf(uint16_t remoteCoreId)
 
     HwiP_restore(oldIntState);
 
-    if(isNewEmptyBuf)
+    if(isNewEmptyBuf !=0U)
     {
         SemaphoreP_post(&coreObj->newEmptyVringBufSem);
     }
@@ -183,7 +182,7 @@ int32_t RPMessage_vringGetFullRxBuf(uint16_t remoteCoreId, uint16_t *vringBufId)
 
     oldIntState = HwiP_disable();
 
-    if(RPMessage_isLinuxCore(remoteCoreId))
+    if(RPMessage_isLinuxCore(remoteCoreId) != 0U)
     {
         /* There's nothing available */
         if (vringObj->lastAvailIdx != vringObj->avail->idx)
@@ -226,7 +225,7 @@ void RPMessage_vringPutEmptyRxBuf(uint16_t remoteCoreId, uint16_t vringBufId)
 
     oldIntState = HwiP_disable();
 
-    if(RPMessage_isLinuxCore(remoteCoreId))
+    if(RPMessage_isLinuxCore(remoteCoreId) != 0U)
     {
         struct vring_used_elem *used;
 
@@ -249,8 +248,7 @@ void RPMessage_vringPutEmptyRxBuf(uint16_t remoteCoreId, uint16_t vringBufId)
     }
 
     #if defined(__aarch64__) || defined(__arm__)
-    __asm__ __volatile__ ( "dsb sy"  "\n\t": : : "memory");
-    __asm__ __volatile__ ( "isb sy"  "\n\t": : : "memory");
+    IpcRpMsg_dataAndInstructionBarrier();
     #endif
     #if defined(_TMS320C6X)
     _mfence();
@@ -275,7 +273,7 @@ uint32_t RPMessage_vringIsFullRxBuf(uint16_t remoteCoreId)
 
     oldIntState = HwiP_disable();
 
-    if(RPMessage_isLinuxCore(remoteCoreId))
+    if(RPMessage_isLinuxCore(remoteCoreId) != 0U)
     {
         if (vringObj->lastAvailIdx == vringObj->avail->idx)
         {
@@ -306,17 +304,17 @@ uint8_t *RPMessage_vringGetRxBufAddr(uint16_t remoteCoreId, uint16_t vringBufId)
 uint32_t RPMessage_vringGetSize(uint16_t numBuf, uint16_t msgSize, uint32_t align)
 {
     return  RPMessage_align(
-                sizeof(struct vring_desc) * numBuf /* buffer descriptors for each buffer */
-              + sizeof(uint16_t) * (2 + numBuf)    /* avail queue */
+               (uint32_t)((sizeof(struct vring_desc) * (uint32_t)numBuf) /* buffer descriptors for each buffer */
+              +(uint32_t)(sizeof(uint16_t) * (2U + (uint32_t)numBuf)))    /* avail queue */
               , align
             )
             +
             RPMessage_align(
-                  sizeof(uint16_t) * 2 + sizeof(struct vring_used_elem) * numBuf /* used queue */
+                (uint32_t)((sizeof(uint16_t) * 2U) + (sizeof(struct vring_used_elem) * (uint32_t)numBuf)) /* used queue */
                 , align
                 )
             +
-            numBuf * msgSize /* message buffers */
+            ((uint32_t)numBuf * (uint32_t)msgSize) /* message buffers */
             ;
 }
 
@@ -344,7 +342,7 @@ void RPMessage_vringResetInternal(RPMessage_Vring *vringObj, uint16_t numBuf, ui
     vringObj->bufBaseAddr = (uint8_t            *)(vringBaseAddr + offset_buf);
 
     /* only initialize TX vring, RX vring is initialized by the remote core */
-    if(isTx)
+    if(isTx != 0U)
     {
         /* initialize descriptors with message buffer address and max len */
         bufAddr = vringObj->bufBaseAddr;
@@ -385,7 +383,7 @@ void RPMessage_vringReset(uint16_t remoteCoreId, uint16_t isTx, const RPMessage_
     uint32_t align, vringSize;
     uint16_t numBuf, msgSize;
 
-    if(isTx)
+    if(isTx != 0U)
     {
         vringObj = &coreObj->vringTxObj;
         vringBaseAddr = params->vringTxBaseAddr[remoteCoreId];
@@ -409,9 +407,9 @@ void RPMessage_vringReset(uint16_t remoteCoreId, uint16_t isTx, const RPMessage_
      * relative to vringBaseAddr
      */
     offset_desc  = 0;
-    offset_avail = offset_desc  + sizeof(struct vring_desc) * numBuf;
-    offset_used  = offset_avail + RPMessage_align( sizeof(uint16_t) * (2 + numBuf), align);
-    offset_buf   = offset_used  + RPMessage_align( sizeof(uint16_t) * 2 + sizeof(struct vring_used_elem) * numBuf, align);
+    offset_avail = offset_desc  + (sizeof(struct vring_desc) * numBuf);
+    offset_used  = offset_avail + RPMessage_align( (sizeof(uint16_t) * (uint32_t)(2U + (uint32_t)numBuf)), align);
+    offset_buf   = offset_used  + RPMessage_align( (sizeof(uint16_t) * 2U) + (sizeof(struct vring_used_elem) * (uint32_t)numBuf), align);
 
     RPMessage_vringResetInternal(vringObj,
         numBuf, msgSize,
@@ -433,7 +431,7 @@ void RPMessage_vringResetLinux(uint16_t remoteCoreId, uint16_t isTx, const RPMes
     uint32_t align;
     uint16_t numBuf, msgSize;
 
-    if(isTx)
+    if(isTx != 0U)
     {
         vringObj = &coreObj->vringTxObj;
         vringBaseAddr = rscTable->vring0.da;
@@ -454,13 +452,13 @@ void RPMessage_vringResetLinux(uint16_t remoteCoreId, uint16_t isTx, const RPMes
      * relative to vringBaseAddr
      */
     offset_desc  = 0;
-    offset_avail = offset_desc  + sizeof(struct vring_desc) * numBuf;
-    offset_used  = offset_avail + RPMessage_align( sizeof(uint16_t) * (2 + numBuf), align);
-    offset_buf   = offset_used  + RPMessage_align( sizeof(uint16_t) * 2 + sizeof(struct vring_used_elem) * numBuf, align);
+    offset_avail = offset_desc  + (sizeof(struct vring_desc) * numBuf);
+    offset_used  = offset_avail + RPMessage_align( (sizeof(uint16_t) * (uint32_t)(2U + (uint32_t)numBuf)), align);
+    offset_buf   = offset_used  + RPMessage_align( (sizeof(uint16_t) * 2U) + (sizeof(struct vring_used_elem) * (uint32_t)numBuf), align);
     /* buffer offset is aligned to numBuf*msgSize*2, eg, 512*256*2 = 256KB after offset_used */
-    offset_buf   = RPMessage_align( offset_buf, numBuf*msgSize*2);
+    offset_buf   = RPMessage_align( offset_buf, (uint32_t) numBuf*msgSize*2U);
 
-    if(isTx)
+    if(isTx != 0U)
     {
         /* offset_buf points to TX buffers already */
     }
@@ -469,7 +467,7 @@ void RPMessage_vringResetLinux(uint16_t remoteCoreId, uint16_t isTx, const RPMes
         /* we dont really use offset buf for RX VRING but showing the calculation here for completeness
          * RX buffers are initialized by Linux side
          */
-        offset_buf += numBuf*msgSize - (rscTable->vring1.da - rscTable->vring0.da);
+        offset_buf += ((uint32_t)numBuf*(uint32_t)msgSize) - (rscTable->vring1.da - rscTable->vring0.da);
     }
 
     RPMessage_vringResetInternal(vringObj,