AM261x MCU+ SDK  11.00.00
sdl_ip_tog.h
Go to the documentation of this file.
1 
45 #ifndef SDL_IP_TOG_H_
46 #define SDL_IP_TOG_H_
47 
48 #ifdef __cplusplus
49 extern "C" {
50 #endif
51 
52 /* ========================================================================== */
53 /* Include Files */
54 /* ========================================================================== */
55 
56 #include <stdint.h>
57 #include <stdbool.h>
58 #include "sdlr_tog.h"
59 
60 
93 /* ========================================================================== */
94 /* Macros & Typedefs */
95 /* ========================================================================== */
96 
107 typedef uint32_t SDL_TOG_IntrSrc;
108 
110 #define SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT ((uint32_t) 1U<<0)
111 
112 #define SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE ((uint32_t) 1U<<1)
113 
114 #define SDL_TOG_INTRSRC_COMMAND_TIMEOUT ((uint32_t) 1U<<2)
115 
116 #define SDL_TOG_INTRSRC_ALL (SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT | SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE | SDL_TOG_INTRSRC_COMMAND_TIMEOUT)
117 
119 /* ========================================================================== */
120 /* Function Declarations */
121 /* ========================================================================== */
122 
135 int32_t SDL_TOG_getIntrCountInternal(uint32_t baseAddr, SDL_TOG_IntrSrc intrSrc, uint32_t *pIntrCnt );
136 
149  int32_t SDL_TOG_setTimeoutVal(uint32_t baseAddr, uint32_t timeoutVal );
150 
165 int32_t SDL_TOG_setIntrPending(uint32_t baseAddr, SDL_TOG_IntrSrc intrSrc );
166 
169 #ifdef __cplusplus
170 }
171 #endif
172 
173 #endif /* SDL_IP_TOG_H_ */
174 
175 /* nothing past this point */
SDL_TOG_setTimeoutVal
int32_t SDL_TOG_setTimeoutVal(uint32_t baseAddr, uint32_t timeoutVal)
Set the timeout value.
SDL_TOG_setIntrPending
int32_t SDL_TOG_setIntrPending(uint32_t baseAddr, SDL_TOG_IntrSrc intrSrc)
Set interrupt source(s)
SDL_TOG_getIntrCountInternal
int32_t SDL_TOG_getIntrCountInternal(uint32_t baseAddr, SDL_TOG_IntrSrc intrSrc, uint32_t *pIntrCnt)
Read internal interrupt count.
SDL_TOG_IntrSrc
uint32_t SDL_TOG_IntrSrc
This enumerator defines the possible timeout interrupt sources.
Definition: sdl_ip_tog.h:107
sdlr_tog.h