AM261x MCU+ SDK  11.00.00
sdl_ip_mcrc.h
Go to the documentation of this file.
1 /********************************************************************
2  * Copyright (C) 2022 Texas Instruments Incorporated.
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
33 
34 #ifndef SDL_IP_MCRC_H_
35 #define SDL_IP_MCRC_H_
36 
37 #include <stddef.h>
38 #include <stdbool.h>
39 #include "sdl_mcrc.h"
40 
41 #ifdef __cplusplus
42 extern "C" {
43 #endif
44 
45 
59 #define SDL_MCRC_MAX_CTRL_FLAG_VAL (1U)
60 
71 typedef uint32_t SDL_MCRC_IntrPriority_t;
72 
73 #define SDL_MCRC_INTR_PRIORITY_CH1_FAIL (0x1U)
74 
75 #define SDL_MCRC_INTR_PRIORITY_CH2_FAIL (0x2U)
76 
77 #define SDL_MCRC_INTR_PRIORITY_CH3_FAIL (0x3U)
78 
79 #define SDL_MCRC_INTR_PRIORITY_CH4_FAIL (0x4U)
80 
81 #define SDL_MCRC_INTR_PRIORITY_CH1_COMPRESSION_DONE (0x9U)
82 
83 #define SDL_MCRC_INTR_PRIORITY_CH2_COMPRESSION_DONE (0xaU)
84 
85 #define SDL_MCRC_INTR_PRIORITY_CH3_COMPRESSION_DONE (0xbU)
86 
87 #define SDL_MCRC_INTR_PRIORITY_CH4_COMPRESSION_DONE (0xcU)
88 
89 #define SDL_MCRC_INTR_PRIORITY_CH1_OVERRUN (0x11U)
90 
91 #define SDL_MCRC_INTR_PRIORITY_CH2_OVERRUN (0x12U)
92 
93 #define SDL_MCRC_INTR_PRIORITY_CH3_OVERRUN (0x13U)
94 
95 #define SDL_MCRC_INTR_PRIORITY_CH4_OVERRUN (0x14U)
96 
97 #define SDL_MCRC_INTR_PRIORITY_CH1_UNDERRUN (0x19U)
98 
99 #define SDL_MCRC_INTR_PRIORITY_CH2_UNDERRUN (0x1aU)
100 
101 #define SDL_MCRC_INTR_PRIORITY_CH3_UNDERRUN (0x1bU)
102 
103 #define SDL_MCRC_INTR_PRIORITY_CH4_UNDERRUN (0x1cU)
104 
105 #define SDL_MCRC_INTR_PRIORITY_CH1_TIMEOUT (0x21U)
106 
107 #define SDL_MCRC_INTR_PRIORITY_CH2_TIMEOUT (0x22U)
108 
109 #define SDL_MCRC_INTR_PRIORITY_CH3_TIMEOUT (0x23U)
110 
111 #define SDL_MCRC_INTR_PRIORITY_CH4_TIMEOUT (0x24U)
112 
123 typedef uint32_t SDL_MCRC_DataBusMask_t;
124 
125 #define SDL_MCRC_DATA_BUS_ITCM_MASK (SDL_MCRC_MCRC_BUS_SEL_ITC_MEN_MASK)
126 
127 #define SDL_MCRC_DATA_BUS_DTCM_MASK (SDL_MCRC_MCRC_BUS_SEL_DTC_MEN_MASK)
128 
129 #define SDL_MCRC_DATA_BUS_VBUSM_MASK (SDL_MCRC_MCRC_BUS_SEL_MEN_MASK)
130 
131 #define SDL_MCRC_DATA_BUS_MASK_ALL (SDL_MCRC_MCRC_BUS_SEL_ITC_MEN_MASK | \
132  SDL_MCRC_MCRC_BUS_SEL_DTC_MEN_MASK | \
133  SDL_MCRC_MCRC_BUS_SEL_MEN_MASK)
134 
137 /* ========================================================================== */
138 /* Function Declarations */
139 /* ========================================================================== */
140 
155 int32_t SDL_MCRC_getHighestPriorityIntrStatus(SDL_MCRC_InstType instance, uint32_t *pIntVecAddr);
156 
178  uint32_t ctrlFlag,
179  SDL_MCRC_DataBusMask_t dataBusMask,
180  SDL_MCRC_DataBusMask_t busEnableMask);
181 
201  uint32_t ctrlFlag,
202  SDL_MCRC_DataBusMask_t dataBusMask,
203  SDL_MCRC_DataBusMask_t busEnableMask);
204 
205 #ifdef __cplusplus
206 }
207 #endif
208 #endif /* SDL_IP_MCRC_H_ */
209 
SDL_MCRC_getHighestPriorityIntrStatus
int32_t SDL_MCRC_getHighestPriorityIntrStatus(SDL_MCRC_InstType instance, uint32_t *pIntVecAddr)
This API is used to get the pending interrupt with highest priority.
SDL_MCRC_InstType
SDL_MCRC_InstType
MCRC Instance supported.
Definition: sdl_mcrc_soc.h:61
SDL_MCRC_DataBusMask_t
uint32_t SDL_MCRC_DataBusMask_t
MCRC data bus type mask selected for tracing control.
Definition: sdl_ip_mcrc.h:123
sdl_mcrc.h
This file contains the prototypes of the APIs present in the device abstraction layer file of MCRC....
SDL_MCRC_IntrPriority_t
uint32_t SDL_MCRC_IntrPriority_t
The offset for the highest pending priority interrupt. These interrupt offset returned in SDL_MCRC_ge...
Definition: sdl_ip_mcrc.h:71
SDL_MCRC_verifyBusTracingCtrl
int32_t SDL_MCRC_verifyBusTracingCtrl(SDL_MCRC_InstType instance, uint32_t ctrlFlag, SDL_MCRC_DataBusMask_t dataBusMask, SDL_MCRC_DataBusMask_t busEnableMask)
This API is used to verify the control the MCRC data bus tracing.
SDL_MCRC_dataBusTracingCtrl
int32_t SDL_MCRC_dataBusTracingCtrl(SDL_MCRC_InstType instance, uint32_t ctrlFlag, SDL_MCRC_DataBusMask_t dataBusMask, SDL_MCRC_DataBusMask_t busEnableMask)
This API is used to control the MCRC data bus tracing.