AM261x MCU+ SDK  11.00.00
sdl_ecc_core.h File Reference

Go to the source code of this file.

Functions

int32_t SDL_ECC_configECCRam (uint32_t ramId)
 
uint32_t SDL_ECC_pollErrorEvent (SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType)
 

Function Documentation

◆ SDL_ECC_configECCRam()

int32_t SDL_ECC_configECCRam ( uint32_t  ramId)

◆ SDL_ECC_pollErrorEvent()

uint32_t SDL_ECC_pollErrorEvent ( SDL_ECC_MemType  eccMemType,
SDL_ECC_MemSubType  memSubType,
SDL_ECC_InjectErrorType  errorType 
)