AM261x MCU+ SDK  11.00.00

Introduction

These APIs try are used for the phy tuning

Functions

int32_t OSPI_lld_readCmd (OSPILLD_Handle handle, OSPI_ReadCmdParams *rdParams)
 Function to send specific commands and receive related data from flash. More...
 
int32_t OSPI_lld_writeCmd (OSPILLD_Handle handle, OSPI_WriteCmdParams *wrParams)
 Function to send specific commands and related data to flash. More...
 

Different OSPI Transfer functions

int32_t OSPI_lld_readDirect (OSPILLD_Handle handle, OSPI_Transaction *trans)
 Function to perform direct reads from the flash using DAC controller. More...
 
int32_t OSPI_lld_readDirectDma (OSPILLD_Handle handle, OSPI_Transaction *trans)
 Function to perform direct reads from the flash using DAC controller in DMA mode. More...
 
int32_t OSPI_lld_readIndirect (OSPILLD_Handle handle, OSPI_Transaction *trans)
 Function to perform indirect reads from the flash using INDAC controller. More...
 
int32_t OSPI_lld_writeDirect (OSPILLD_Handle handle, OSPI_Transaction *trans)
 Function to perform direct writes to the flash using DAC controller. More...
 
int32_t OSPI_lld_writeIndirect (OSPILLD_Handle handle, OSPI_Transaction *trans)
 Function to perform indirect writes to the flash using INDAC controller. More...
 

Function Documentation

◆ OSPI_lld_readDirect()

int32_t OSPI_lld_readDirect ( OSPILLD_Handle  handle,
OSPI_Transaction trans 
)

Function to perform direct reads from the flash using DAC controller.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
transPointer to a OSPI_Transaction
Returns
OSPI_SYSTEM_SUCCESS on successful read; else error on failure
See also
OSPI_open

◆ OSPI_lld_readDirectDma()

int32_t OSPI_lld_readDirectDma ( OSPILLD_Handle  handle,
OSPI_Transaction trans 
)

Function to perform direct reads from the flash using DAC controller in DMA mode.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
transPointer to a OSPI_Transaction
Returns
OSPI_SYSTEM_SUCCESS on successful read; else error on failure
See also
OSPI_open

◆ OSPI_lld_readIndirect()

int32_t OSPI_lld_readIndirect ( OSPILLD_Handle  handle,
OSPI_Transaction trans 
)

Function to perform indirect reads from the flash using INDAC controller.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
transPointer to a OSPI_Transaction
Returns
OSPI_SYSTEM_SUCCESS on successful read; else error on failure
See also
OSPI_open

◆ OSPI_lld_writeDirect()

int32_t OSPI_lld_writeDirect ( OSPILLD_Handle  handle,
OSPI_Transaction trans 
)

Function to perform direct writes to the flash using DAC controller.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
transPointer to a OSPI_Transaction
Returns
OSPI_SYSTEM_SUCCESS on successful write; else error on failure
See also
OSPI_open

◆ OSPI_lld_writeIndirect()

int32_t OSPI_lld_writeIndirect ( OSPILLD_Handle  handle,
OSPI_Transaction trans 
)

Function to perform indirect writes to the flash using INDAC controller.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
transPointer to a OSPI_Transaction
Returns
OSPI_SYSTEM_SUCCESS on successful write; else error on failure
See also
OSPI_open

◆ OSPI_lld_readCmd()

int32_t OSPI_lld_readCmd ( OSPILLD_Handle  handle,
OSPI_ReadCmdParams rdParams 
)

Function to send specific commands and receive related data from flash.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
rdParamsPointer to a OSPI_ReadCmdParams
Returns
OSPI_SYSTEM_SUCCESS if command read was successful; else error on failure
See also
OSPI_open

◆ OSPI_lld_writeCmd()

int32_t OSPI_lld_writeCmd ( OSPILLD_Handle  handle,
OSPI_WriteCmdParams wrParams 
)

Function to send specific commands and related data to flash.

Parameters
handleOSPILLD_Handle returned from OSPI_open()
wrParamsPointer to a OSPI_WriteCmdParams
Returns
OSPI_SYSTEM_SUCCESS if command write was successful; else error on failure
See also
OSPI_open