AM261x MCU+ SDK  11.00.00
Release Notes 10.02.00

Attention
1. Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
2. There is a known issue of PMIC Watchdog resetting the SOC every 10 mins in CCS Gel flow. This has been fixed in SBL flow by disabling PMIC Watchdog using I2C interface. Use Flash SBL NULL if CCS Debug is needed or Add the same logic for PMIC Watchdog disable in application if CCS debug using Gel flow is mandatory.
3. DFU Utils tool is not supported on Mac systems due to a build issue.
4. Uniflash 9.1.0 does not support out of the box flashing of AM261x-LP E2 binaries. As a workaround, use Uniflash's custom flasher feature mentioned here Custom Flash Support. Out of box flashing support for E2 board will be available in the next Uniflash release.
4. The default Stack size is 16KB and Heap size 32 KB for SDK examples. This can be adjusted as per application requirement through Memory Configurator in SysCfg or by updating Linker script in case of standalone applications.
5. SDK will be migrated to support CCS Theia from next release (SDK 11.0) and the support for CCS Eclipse will be deprecated.
6. There is a known issue that OSPI pins in SysCfg GUI are getting reset automatically during any module change. The workaround is that OSPI Pins should be locked after proper configuration according to the board Pinout.
7. The default SysCfg linked to CCS is an older version and needs to updated to the SDK supported version mentioned below. Please follow steps mentioned in Check Packages as seen by CCS.
8. CCS 12.8.1 doesn't support AM261x by default. Please follow the steps mentioned in Download, Install and Setup CCS to enable AM261x device support.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
OTFA Safety and Security Support OptiFlash
FreeRTOS MPU Support for R5F and Examples Kernel
EDMA Error Handling Support EDMA
LIN LLD Support LIN
OSPI PSRAM Support OSPI
OSPI NAND and SBL NAND Support OSPI
Rev E2 Launchpad Support Board
FOTA Support OptiFlash
CPSW Cut-through switching functionality is enabled and switching latency performance is benchmarked Networking
Support for RMII, RGMII and MII mode is enabled Networking
AM261-SOM Board Example Support (Loopback, Layer2 and LwIP) Networking

Modules Not tested/supported in this release

  • MMCSD and GPMC drivers are not validated on AM261x LP or SOM Board.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM261x R5F AM261x Launchpad Rev E2 (referred to as am261x-lp in code).
Windows 10 64b or Ubuntu 18.04 64b or MacOS
AM261x R5F AM261x SOM Rev E1 (referred to as am261x-som in code).
Windows 10 64b or Ubuntu 18.04 64b or MacOS

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.8.1
SysConfig R5F 1.23.0 build, build 4000
TI ARM CLANG R5F 4.0.1.LTS
FreeRTOS Kernel R5F 11.1.0
LwIP R5F STABLE-2_2_0_RELEASE
Mbed-TLS R5F 2.13.1

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
- -

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, UART. All R5F's. RPRC, multi-core image format Force Dual Core Mode

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Examples: adc_soc_continuous_dma, adc_alternate_dma_trigger Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA (normal and alternate triggers), EPWM trip through PPB limit, PPB features, Burst mode, Single and Differential mode, Interrupt with Offset from Aquisition Window, EPWM/ECAP/RTI triggered conversions, Trigger Repeater for Undersampling and Oversampling, Global Force on Multiple ADCs, Internal DAC Loopback to Calibration Channels, Safety Checker and Aggregator, Open Short Detection feature External channel selection
Bootloader R5F YES Yes. DMA enabled for SBL OSPI Boot modes: OSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip, digital filter, Calibration CMPSS Dac LoopBack feature

CPSW | R5F | YES | No | MAC & PHY loopback(DP83826-EVM-AM2) with RMII and MII 100Mbps , MAC & PHY loopback(DP83TG720-EVM-AM2) with RGMII 1Gbps, LWIP (DP83TG720-EVM-AM2, DP83826-EVM-AM2): Getting IP, Ping, Layer 2 MAC, Layer 2 PTP Timestamping and Ethernet CPSW Switch support, TSN stack | DAC | R5F | YES | Yes. Example: dac_sine_dma | Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation | - ECAP | R5F | YES | yes. Example : ecap_edma | ECAP APWM mode, PWM capture, DMA trigger in both APWM and Capture Modes, Signal Monitoring features | - EDMA | R5F | YES | NA | DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking, Error Handling | - EPWM | R5F | YES | Yes. Example: epwm_dma, epwm_xcmp_dma | Multiple EPWM Sync from Top Module, PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, chopper module features, type5 features, global load and link feature | - EQEP | R5F | YES | NA | Speed and Position measurement. Frequency Measurement, speed direction, cw-ccw modes | - FSI | R5F | YES | YES | RX, TX, polling, interrupt, DMA mode, single lane loopback. | - FSI Spi Mode GPIO | R5F | YES | NA | Output, Input and Interrupt functionality | - I2C | R5F | YES | No | Controller mode, basic read/write | - IPC Notify | R5F | YES | NA | Mailbox functionality, IPC between RTOS/NORTOS CPUs | M4F core IPC Rpmsg | R5F | YES | NA | RPMessage protocol based IPC | M4F core LIN | R5F | YES | YES | RX, TX, polling, interrupt, DMA mode. | - MCAN | R5F | YES | No | RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode | - MCSPI | R5F | YES | Yes. Example: mcspi_loopback_dma | Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode | - MDIO | R5F | YES | NA | Register read/write, link status and link interrupt enable API | - PINMUX | R5F | YES | NA | Tested with multiple peripheral pinmuxes | - PMU | R5F | NO | NA | Tested various PMU events | Counter overflow detection is not enabled OptiFlash | R5F | Yes | NA | FLC, RL2, RAT functionality, XIP with RL2 enabled, OTFA, FOTA, Optishare, Smart Layout | - OSPI | R5F | YES | Yes. Example: ospi_flash_dma | Read direct, Write indirect, Read/Write commands, DMA for read | - RTI | R5F | YES | No | Counter read, timebase selection, comparator setup for Interrupt, DMA requests | Capture feature, fast enabling/disabling of events not tested SDFM | R5F | YES | No | ECAP Clock LoopBack, Filter data read from CPU, Filter data read with PWM sync, triggered DMA read from the Filter FIFO | - SOC | R5F | YES | NA | Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation | - SPINLOCK | R5F | NA | NA | Lock, unlock HW spinlock | - UART | R5F | YES | Yes. Example: uart_echo_dma | Basic read/write at baud rate 115200, polling, interrupt mode | HW flow control not tested, DMA mode not supported USB | R5F | No | NA | DFU, CDC Echo mode | - WATCHDOG | R5F | YES | NA | Reset mode, Interrupt mode | -

Trigonometric Operations

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
TMU R5F NO NA TMU Operations, Pipelining, Contex Save Square Root, Division Operations. more than 1 Interrupt Nesting for the contex save is not Supported.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
FLASH R5F YES OSPI Flash -
LED R5F YES GPIO -
ETHPHY R5F YES Tested with ethercat_slave_beckhoff_ssc_demo example -
IOEXPANDER R5F YES IO configurability -
PMIC R5F YES Watchdog Reset and disable -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Time-Sensitive Networking(gPTP-IEEE 802.1AS) R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, scatter-gather Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC & PHY loopback with RMII 100Mbps(DP83826-EVM-AM2), MAC & PHY loopback with RMII 100Mbps(DP83TG720-EVM-AM2), Layer 2 MAC, Packet Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer and Classifier MII mode
ICSS-EMAC R5F YES FreeRTOS Switch and MAC features, Storm Prevention (MAC), Host Statistics, Multicast Filtering Promiscuous Mode

Safety Diagnostic Library

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
MCRC R5F NA NORTOS Full CPU, Auto CPU Mode and Semi CPU Auto Mode -
DCC R5F NA NORTOS Single Shot and Continuous modes -
PBIST R5F NA NORTOS Memories supported by MSS PBIST controller. -
ESM R5F NA NORTOS Tested in combination with RTI, DCC -
RTI R5F NA NORTOS WINDOWSIZE_100_PERCENT, WINDOWSIZE_50_PERCENT ,Latency/Propagation timing error(early)(50% window),Latency/Propagation timing error(late)(50% window) -
ECC R5F NA NORTOS ECC of MSS_L2, R5F TCM, MCAN, VIM, ICSSM, TPTC FSS FOTA and OSPI
ECC Bus Safety R5F NA NORTOS AHB, AXI, TPTC -
CCM R5F NA NORTOS CCM Self Test Mode,Error Forcing Mode and Self Test Error Forcing Mode. TMU and RL2 are also validated -
R5F STC(LBIST), Static Register Read R5F NA NORTOS STC of R5F, R5F CPU Static Register Read -
TMU ROM Checksum R5F NA NORTOS ROM checksum for TMU -
Time out Gasket(STOG) R5F NA NORTOS Timeout gasket feature -
Thermal Monitor(VTM) R5F NA NORTOS Over, under and thershold temperature interrupts -
Integrated Example R5F NA FreeRTOS Integrated example with all the SDL modules integrated in to one example. ECC for TPTC, ECC Bus Safety and STC.

Note: SDL is validated only on SOM Board.

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-14052 AM261x: OSPI Phy tuning fails on am261x LP OSPI 10.00.00 onwards AM261x Update in the Phy tuning algorith fixed the issue.
MCUSDK-13874 Syscfg load json function for flash configuration imports does not work OSPI 10.00.00 onwards AM261x, AM263Px, AM263x Fix in SysCfg Meta file.
MCUSDK-13109 RTI Interrupt req is Pulse type and not Level type RTI 10.00.00 onwards AM263x, AM263Px, AM261x Updated interrupt type to Pulse
MCUSDK-13523 McSPI FIFO not enabled in DMA mode McSPI 10.00.00 onwards AM261x Added FIFO support in McSPI driver for Read and Write
MCUSDK-14516 UART ISR Blocking for long time UART 10.00.00 onwards AM263x, AM263Px, AM261x Removed unwanted timeout loop in UART ISR
MCUSDK-13473 UART uniflash script fails with large images ( > 1MB) SBL 10.00.00 onwards AM263x, AM263Px, AM261x Reference before assignment error in python script
MCUSDK-13341 ECAP: Emulation mode does not work. ECAP 9.02.00 onwards AM263x, AM263Px, AM261x Added halt control API for ECAP in soc.c file and emulation mode in syscfg to be emulation free.
MCUSDK-14051 EQEP: CW CCW example doesn't use polling or interrupt EQEP 10.01.00 onwards AM263x, AM263Px, AM261x Modified example to use unit timer interrupt.
MCUSDK-14332 SDFM soc ctrl syscfg: code generates outside callable functions SDFM 10.00.01 onwards AM263x, AM263Px, AM261x Updated code generation of soc ctrl sdfm module in syscfg.
MCUSDK-12238 OUTPUTXBAR input sources from CMPSS needs to be renamed ADC 9.00.01 onwards AM263Px OUTPUTXBAR input sources from CMPSS are renamed as CMPSSA/Bx_CTRIPOUTH/L.
MCUSDK-14367 Update IO Expander for AM261x-SOM support SYSCFG 10.00.01 onwards AM261x Updated ioexpander to unique naming for across boards using board and i2c address identifiers. Added template generation for the ioexpander on SOM.
MCUSDK-14326 Remove extra EPWM instance from DAC Syscfg DAC 10.00.01 onwards AM261x Updated EPWM instances to 10 since device supports only 10 EPWMs.
MCUSDK-14329 ADC: 32 EPWM Sync out sources are listed EPWM 10.00.01 onwards AM261x Updated EPWM Sync out sources to 10 since device supports only 10 EPWMs.
MCUSDK-14330 ADC: 12 ADC Safety checker instances are listed ADC 10.00.01 onwards AM261x Updated ADC safety checker instances to 6.
MCUSDK-14331 ADC: Tile: Selector 1 and Selector 2 allows 6 ADCs ADC 10.00.01 onwards AM261x Fixed ADC instances for safety checker tiles.
MCUSDK-14381 Update CMPSS Channel connection image in Syscfg CMPSS 10.00.01 onwards AM261x Updated CMPSS Channel connection image in Syscfg.
MCUSDK-13828 AM261x: ENET: Iperf TCP failing with 1Gbps Networking 10.02.00 onwards Disabled CCS print logs
MCUSDK-14146 AM261x Networking examples are not detected by CCS Networking 10.00.00 onwards Changed the script to enable networking examples
MCUSDK-14124 MDIO header files having the same IFDEF header guards Networking 10.01.00 onwards Changed the header guard

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-14148 AM261x : ZNC : Package in the early samples has ADC issue. Needs SW checks undone for ADC ADC 10.00.00 onwards Details : ZNC package currently (Jan 2025), has, ADC 0 Reference lines not connected with that of the ADC 1's. There are some packages were shipped with the ADC Reference Monitor checks are Bypassed for the ADC front end enablement in the EFUSE. the SW code gen from the syscfg will assert the ADC init if the monitor throws a fault. It is requested to bypass the SW check as well to enable the customer to use the ADC.
Workaround : only applicable in the devices with forementioned conditions.
1. Go to the file
source/sysconfig/drivers/.meta/soc_ctrl/templates/soc_ctrl_adc_config.c.xdt

2. Find line with
DebugP_assert(SOC_getAdcReferenceStatus(`montior2AdcMap[monitor][0]`) == true);

3.Change it to
//DebugP_assert(SOC_getAdcReferenceStatus(`montior2AdcMap[monitor][0]`) == true);
MCUSDK-13865 HRPWM Deadband sfo example has 1ns jitter EPWM 10.00.00 onwards -
MCUSDK-13755 AM261x: 10% RX align code and CRC errors in port 2 Networking 10.00.00 onwards -
SMCUAPPS-972 AM261x: Gel files upgrade to program the HSDIVIDER clock correctly MCU Apps 10.00.01 onwards -
MCUSDK-14596 AM261x: Enet: GPTP link configuration read failure for RMII and MII Networking 10.00.01 onwards -
MCUSDK-13847 AM261x: GPTP lwIP debug example doesnt fit in RAM Networking 10.00.01 onwards -
MCUSDK-13513 AM263Px, AM261x: UDP IPERF TX is unstable with 100Mbps link speed Networking 10.00.01 onwards -
MCUSDK-14055 SBL DFU and SBL DFU Uniflash Example failure USB 10.00.01 onwards Issue is only in Release mode. Run the examples in Debug mode.
MCUSDK-14056 Klocwork issues on USB Driver USB 10.00.01 onwards -
MCUSDK-14110 Error building examples in CCS in mac Infra Example build fails in CCS only in MAC Machines Building projects in CCS in MAC machines
PINDSW-7715 Dual EMAC instance not working with both ports together for icss_emac_lwip example ICSS-EMAC 10.00.01 onwards None
PINDSW-7746 Low iperf values in TCP and UDP ICSS-EMAC 10.00.01 onwards None
PINDSW-8118 Enabling DHCP mode in icss_emac_lwip example causes assert ICSS-EMAC 10.00.01 onwards None
MCUSDK-13201 HRPWM waveform not generating (in updwon count) when prescaler is non-zero and HRPE is enabled EPWM 10.00.01 onwards None
MCUSDK-13834 EQEP: EQEP frequency measurement example is not working as expected EQEP 10.00.01 onwards None
PROC_SDL-8392 In ECC bus safety example, ECC error is not properly cleared at the source. SDL 10.02.00 onwards None
PROC_SDL-8787 ECC TPTC and STC examples are not supported in SDL integrated example. SDL 10.02.00 onwards Use standalone examples.
PROC_SDL-8857 SDL integrated example does not support ECC Bus Safety. SDL 10.02.00 onwards Use standalone example.
PROC_SDL-9147 VTM Usecase stuck in integrated example SDL 10.02.00 onwards Use standalone example.
PROC_SDL-9163 ECC Aggregators FSS FOTA and OSPI SDL 10.02.00 onwards None
PROC_SDL-9154 VTM Example stuck in UC2 SDL 10.02.00 onwards None
PROC_SDL-9177 ECC MSS-L2 example fail in R5FSS0-1 during release SDL 10.02.00 onwards Use R5FSS0-0 example.
PROC_SDL-9179 Redefinition error in MCU_PBIST Sysconfig SDL 10.02.00 onwards Use sdl examples instead of sbl_null to enable MCU_PBIST SYSCFG and test.
MCUSDK-13513 Multiple chip selects cannot be configured in SysCfg OSPI 10.00.00 onwards -
MCUSDK-13182 SysCfg unexpectedly changes OSPI Pin OSPI 10.00.00 onwards Lock the OSPI Pins in OSPI SysCfg.
MCUSDK-14582 Flash: Incorrect flash name after Loading Flash JSON OSPI 10.00.00 onwards -
MCUSDK-14102 Applications > 1MB not flashing using TI Uniflash tool Uniflash tool 10.00.00 onwards Issues with flashing applications > 1MB in serial session
MCUSDK-14613 XIP image loading not working in CCS for am261x-lp E2 board CCS, XIP 10.02.00 onwards -
MCUSDK-14547 XIP Flashing not supported in SBL JTAG Uniflash example SBL 10.00.00 onwards -
MCUSDK-14502 PMIC WDG QA Example not working on AM261x-LP E2 board PMIC 10.02.00 onwards -
MCUSDK-14609 FOTA Example Failure on AM261x SOM OptiFlash 10.02.00 onwards -
MCUSDK-14610 MCAN External Loopback Failure on AM261x SOM MCAN 10.02.00 onwards -
MCUSDK-14611 LIN External Loopback Failure on AM261x SOM LIN 10.02.00 onwards -
MCUSDK-14606 USB Enumeration fails randomly USB 10.02.00 onwards -

Errata

ID Head Line Module SDK Status
i2189 OSPI: Controller PHY Tuning Algorithm OSPI Implemented
i2311 USART: Spurious DMA Interrupts UART Implemented
i2324 No synchronizer present between GCM and GCD status signals Common Implemented
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2351 OSPI: Controller does not support Continuous Read mode with NAND Flash OSPI Implemented
i2354 SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM Open
i2356 ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set ADC Implemented
i2375 SDFM: SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected SDFM Open
i2383 OSPI: 2-byte address is not supported in PHY DDR mode OSPI Implemented
i2479 OSPI Boot Issue with GPIO61 Reset Pin Configuration OSPI Open
i2480 1µs Glitch on GPIO61/OSPI0_RESET_OUT0 during OSPI Boot GPIO Open

Limitations

ID Head Line Module Reported in release Workaround
- DP83TG720-EVM-AM2 and DP83826-EVM-AM2 dont work simultaneously for switching traffic in AM261-LP boards Networking 10.00.00 onwards -
MCUSDK-13630 Cache should not be enabled at last 32B L2 Bank boundary Cache 10.01.00 Create MPU configurations for last 32B of each L2 Bank with Non Cached attribute

Upgrade and Compatibility Information

Flash Migration in AM261x-LP : E2 to E1

The AM261x-LP E2 has Macronix flash and the sdk supports E2 OOB. In order to migrate to E1 (ISSI flash), the following steps needs to be done -

  1. Open the syscfg gui for the application
  2. Navigate to the flash module and use LOAD from JSON function
  3. Select the "IS25WX064" flash provided in the sdk path - "{MCU_PLUS_SDK_PATH}/source/sysconfig/board/.meta/flash"
  4. Select 8d protocol and rebuild the application.

How to run FOTA examples on AM261x-LP-E1 board

Here, to make FLSOPSKD Benchmark example work with AM261x-LP-E1 board, please

  1. Removed the RUN_XIP_IN_PARALLEL macro.
  2. Change EXT_FLASH_ERASE_EXTOPCODE value to 0x21.

Changes in FLSOPSKD and FOTAAgent driver

These 2 drivers has been revamped from grounds up and there is an API compatibility break from previous release. On how to use the latest drivers please refer to FLSOPSKD and FOTA Agent.

Compiler Options

Module Affected API Change Additional Remarks
- - - -

SOC Device Drivers

Module Affected API Change Additional Remarks
- - - -

Networking

Module Affected API Change Additional Remarks
- - - -