AM261x MCU+ SDK  11.00.00
SDL MCRC Semi CPU

Introduction

This example demonstrates the usage of the MCRC module. The example shows how to setup and use the MCRC controller in the semi mode of operation. Shows the generation of matching CRC as well as non-matching signature due to insertion of error in the block of information on which the CRC is being performed or in the signature provided to the PSA Signature Register (or both, depending on the mode).

Use Cases

Use Case Description
UC-1 Semi CPU-mode signature compute for Channel 1 and comparison against known value.
UC-2 Semi CPU-mode signature compute for Channel 2 and comparison against known value.

Supported Combinations

Steps to Run the Example

See Also

MCRC

Sample Output

Shown below is a sample output when the application is run,