This example demonstrates SEC and DED on MSS TPTC FIFO memories.
Use Cases
Use Case
Description
UC-1
Single bit error injection.
UC-2
Double bit error injection.
Supported Combinations
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)