AM261x MCU+ SDK  11.00.00
MCAN Loopback Polling

Introduction

This example demonstrates the CAN message transmission and reception in digital loop back mode with the following configuration.

  • Classic CAN Message Format.
  • Message ID Type is Extended, Msg Id 0xD0, 0xD1, 0xD2, 0xD3, 0xD4.
  • MCAN is configured in Polling Mode.
  • Arbitration Bit Rate 1Mbps.
  • Data Bit Rate 5Mbps.
  • FIFO mode is used for Tx and RX to store message in message RAM.

5 Messages are transmitted and received back internally using internal loopback mode. When all the 5 messages received with the id and the data matches with the transmitted one, then the example is completed.

Supported Combinations

Steps to Run the Example

See Also

MCAN

Sample Output

Shown below is a sample output when the application is run,

[MCAN] Loopback Polling mode, application started ...
All tests have passed!!