Introduction
This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED on/off for 10 seconds and exits.
Supported Combinations
Steps to Run the Example
See Also
GPIO
Sample Output
Shown below is a sample output when the application is run,
GPIO LED Blink Test Started ...
LED will Blink for 10 seconds ...
GPIO LED Blink Test Passed!!
All tests have passed!!