Introduction
This example uses the DAC to generate a constant voltage on the DAC output.
The example does the below
- Configures the voltage (specified by the APP_DAC_OUT_VOLTAGE macro) in the DAC.
- Waits for the specified time.
- Sets the output voltage back to 0.
External Connections
- DAC output pin can be connected to an oscilloscope to view the constant voltage output.
AM263X-CC or AM263PX-CC or AM261X-SOM E1
Note: To use the reference voltage generated on ControlCard, make sure that the System VREF source select switch on ControlCard is set to position 1-2
When using with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Capture waveform on HSEC Pin 9 (in case of AM261x and AM263Px please take care of IO expander)
AM263X-LP or AM263PX-LP or AM261X-LP
Note: To use the reference voltage generated on LaunchPad, make sure that the DAC_VREF source select switch S1 on LaunchPad is set to position 1-2
With AM263X-LP or AM263Px-LP or AM261x-LP
- Capture waveform on boosterpack header J1/J3 Pin 30.
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am261x-som, am261x-lp |
| Example folder | examples/drivers/dac/dac_constant_voltage/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Use an Oscilloscope to view the constant voltage on DAC output pin.
See Also
DAC
Sample Output
Shown below is a sample output when the application is run,
DAC Constant Voltage Test Started ...
DAC Constant Voltage Test Passed!!
All tests have passed!!