Trigger repeater module
The trigger repeater module allows to achieve an oversampling, undersampling or to apply a trigger delay. The repeater modules can select any of the regular ADC triggers that are selectable by ADCSOCxCTL.TRIGGER register and generate a number of repeated pulses as configured in repeater module. The repeater module can apply four types of trigger modifications:
- Oversample mode - allows multiple back-to-back samples from a single trigger pulse.
- Undersample mode - scale down the trigger frequency for one or more SOCs.
- Phase delay - delay the initial trigger by a specified number of SYSCLK.
- Re-trigger Spread - the additional time between two samples.
Example Description
This example configures ADC for oversampling using trigger repeater block. The ePWM0 is configured to periodically trigger the ADC1_AIN0 and the trigger repeater module is configured to generate 4 repeated pulses. Post-processing block will take the repeated pulses, increment PPB conversion count and generates an oversampling interrupt (OSINT1) which triggers a CPU interrupt. The accumulated samples will be stored in PPB SUM register.
ADC Tigger Repeater Oversampling
ADC Configurations
- SOC0 is triggered by EPWMSOCA. Sample window is set at 16
- SOC0 samples on channel 0 and trigger source is set as repeated trigger
- Trigger repeater module 1 is configured for oversampling
- Trigger count (N) is set to 3, so it will generate N+1 repeated pulses
ISR Configuration
- INTXbar0 is set for EPWM0INT1
- App_epwmISR services this interrupt
- reads ADC OSINT flag to check if oversampling is done
External Connections
ADC1_AIN0 pin should be connected to signals to be converted.
- on AM263Px CC E1 or AM261x-SOM E1, with HSEC Dock
- Feed Analog input to ADC1_AIN0 - HSEC PIN 12
- on AM263Px LP / AM261x LP
- Feed Analog input to ADC1_AIN0 - J1/3 Pin 24
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am261x-som, am261x-lp |
| Example folder | examples/drivers/adc/adc_trigger_repeater_oversampling/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section.
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using the watch variables, view the ADC conversion results.
- View the ADC conversion results in UART console logs
See Also
ADC
Sample Output
Shown below is a sample output when the application is running,
ADC Trigger Repeater Oversampling Test Started...
ADC Trigger Repeater Oversampling results:
Trigger Repeater Oversampling Test Passed!!
All tests have passed!!