AM261x MCU+ SDK  11.00.00
ADC DAC Loopback

Introduction

In AM261x the DAC can be connected internally to the ADC CAL0 Channel.

This example demostrates the ADC-DAC loopback feature. Each ADC has two CAL channels viz. CAL Channel 0 and CAL Channel 1. these CAL channels are common to all the ADCs. While using the ADC-DAC loopback, the following needs to be taken care of,

  1. ADC cal channel should be of high impedence, i.e., no source driving it.
  2. DAC output should be driven only by DAC and there should not be any other source driving it.
  3. ADC sampling times must be increased in this mode. the example uses the 256 Sample and Hold window configuration.
  4. Sampling the DAC voltage with multiple ADCs at the same time will produce inconsistent results. Due to sampling kickback and charge injection. Hence, only one ADC may be used with the given CAL channel at any point of using the DAC-ADC loopback.

Configurations

  • DAC is configured using syscfg
  • ADC SOC0 is configured CAL Channel, with sample and hold window of 256 and generate interrupt at EOC0

External Connections

No external connections required

Watch Variables

The below watch variables can be used to view ADC conversion results.

  • gAdcResults[] : Digital representation of the voltage sample on pin AIN2 of ADC0, triggered by RTI
  • gDac_shadowValues[] : DAC digital values corresponding to the ADC conversions.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am261x-som, am261x-lp
Example folder examples/drivers/adc/adc_dac_loopback/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Using watch variables, view the ADC conversion results.
  • View the ADC conversion results in UART console logs

See Also

ADC

Sample Output

Shown below is a sample output when the application is run,

ADC DAC Loopback Test Started ...
DAC code | ADC Result
100 | 101
--->0.08057V | 0.07891V
200 | 202
--->0.16113V | 0.15781V
300 | 304
--->0.24170V | 0.23750V
400 | 406
--->0.32227V | 0.31719V
500 | 508
--->0.40283V | 0.39687V
600 | 612
--->0.48340V | 0.47813V
700 | 716
--->0.56396V | 0.55937V
800 | 819
--->0.64453V | 0.63984V
900 | 921
--->0.72510V | 0.71953V
1000 | 1024
--->0.80566V | 0.80000V
1100 | 1125
--->0.88623V | 0.87891V
1200 | 1227
--->0.96680V | 0.95859V
1300 | 1328
--->1.04736V | 1.03750V
1400 | 1430
--->1.12793V | 1.11719V
1500 | 1533
--->1.20850V | 1.19766V
1600 | 1636
--->1.28906V | 1.27813V
1700 | 1742
--->1.36963V | 1.36094V
1800 | 1847
--->1.45020V | 1.44297V
1900 | 1954
--->1.53076V | 1.52656V
2000 | 2060
--->1.61133V | 1.60938V
2100 | 2166
--->1.69189V | 1.69219V
2200 | 2269
--->1.77246V | 1.77266V
2300 | 2372
--->1.85303V | 1.85312V
2400 | 2474
--->1.93359V | 1.93281V
2500 | 2577
--->2.01416V | 2.01328V
2600 | 2681
--->2.09473V | 2.09453V
2700 | 2786
--->2.17529V | 2.17656V
2800 | 2890
--->2.25586V | 2.25781V
2900 | 2993
--->2.33643V | 2.33828V
3000 | 3098
--->2.41699V | 2.42031V
3100 | 3201
--->2.49756V | 2.50078V
3200 | 3301
--->2.57812V | 2.57891V
3300 | 3401
--->2.65869V | 2.65703V
3400 | 3502
--->2.73926V | 2.73594V
3500 | 3603
--->2.81982V | 2.81484V
3600 | 3705
--->2.90039V | 2.89453V
3700 | 3809
--->2.98096V | 2.97578V
3800 | 3915
--->3.06152V | 3.05859V
3900 | 4019
--->3.14209V | 3.13984V
ADC DAC loopback Test Passed
All tests have passed!!