AM263Px MCU+ SDK  10.02.00
tmu_rom_checksum/sdl_tmu_rom_checksum.h File Reference

Introduction

This file contains the prototypes of the APIs present in the device abstraction layer file of TMU ROM checksum. This also contains some related macros.

Go to the source code of this file.

Macros

#define SDL_TMU_CRC_GOLDEN_REFL   (0x36CFB524U)
 
#define SDL_TMU_CRC_GOLDEN_REFH   (0xCCDAB254U)
 
#define SDL_TMU_MCRC_PCNT   (0U)
 
#define SDL_TMU_MCRC_SCNT   (1U)
 
#define SDL_TMU_MCRC_WDPRELD   (0U)
 
#define SDL_TMU_MCRC_BLKPRELD   (0U)
 
#define SDL_R5F_CORE   (0U) /* Options 0,1,2,3 */
 
#define SDL_DEF_TMU_ROM_BA   (0x53020000U + (SDL_R5F_CORE * 0x4000U))
 
#define SDL_TMU_ROM_SIZE   (0x3000U) /* 12KB */
 

Functions

int32_t SDL_TMU_ROM_Checksum_compute (SDL_MCRC_Channel_t mcrcChannelNumber, SDL_MCRC_Signature_t *sectSignVal)
 Compute TMU Rom Checksum. More...