AM263Px MCU+ SDK  10.02.00
Diag_Mon_Rotational_Signal_Integrity_data Struct Reference

Detailed Description

Structure to hold the control/status data for Diagnostics mentioned under Monitor rotational signal integrity (DOS)

Values that can be passed to RDC_getDiagnosticsRotationalSignalIntegrityData(), RDC_setDiagnosticsRotationalSignalIntegrityData() as Diag_Mon_Rotational_Signal_Integrity_data parameter

Data Fields

bool cos_neg_zc_peak_mismatch_err
 
bool cos_pos_zc_peak_mismatch_err
 
bool sin_neg_zc_peak_mismatch_err
 
bool sin_pos_zc_peak_mismatch_err
 
bool sin_multi_zc_error_err
 
bool cos_multi_zc_error_err
 
uint8_t cos_multi_zc_error_count
 
uint8_t sin_multi_zc_error_count
 
uint16_t rotpeak_level
 
uint16_t rotfreq_level
 
bool zero_cross_rot_en
 

Field Documentation

◆ cos_neg_zc_peak_mismatch_err

bool Diag_Mon_Rotational_Signal_Integrity_data::cos_neg_zc_peak_mismatch_err

◆ cos_pos_zc_peak_mismatch_err

bool Diag_Mon_Rotational_Signal_Integrity_data::cos_pos_zc_peak_mismatch_err

◆ sin_neg_zc_peak_mismatch_err

bool Diag_Mon_Rotational_Signal_Integrity_data::sin_neg_zc_peak_mismatch_err

◆ sin_pos_zc_peak_mismatch_err

bool Diag_Mon_Rotational_Signal_Integrity_data::sin_pos_zc_peak_mismatch_err

◆ sin_multi_zc_error_err

bool Diag_Mon_Rotational_Signal_Integrity_data::sin_multi_zc_error_err

◆ cos_multi_zc_error_err

bool Diag_Mon_Rotational_Signal_Integrity_data::cos_multi_zc_error_err

◆ cos_multi_zc_error_count

uint8_t Diag_Mon_Rotational_Signal_Integrity_data::cos_multi_zc_error_count

◆ sin_multi_zc_error_count

uint8_t Diag_Mon_Rotational_Signal_Integrity_data::sin_multi_zc_error_count

◆ rotpeak_level

uint16_t Diag_Mon_Rotational_Signal_Integrity_data::rotpeak_level

◆ rotfreq_level

uint16_t Diag_Mon_Rotational_Signal_Integrity_data::rotfreq_level

◆ zero_cross_rot_en

bool Diag_Mon_Rotational_Signal_Integrity_data::zero_cross_rot_en