AM263Px MCU+ SDK  10.02.00

Detailed Description

Struct holds the Resolver Core Configurations Can be passed to RDC_coreParamsInit(Core_config_t* coreParams); Note : this is also called in the RDC_paramsInit(RDC_configParams* params);.

Data Fields

bool BpfDc_bpfEnable
 
bool BpfDc_offsetCorrectionEnable
 
uint8_t BpfDc_dcOffCal1
 
uint8_t BpfDc_dcOffCal2
 
int16_t BpfDc_manualSin
 
int16_t BpfDc_manualCos
 
uint8_t IdealSample_overrideValue
 
uint16_t IdealSample_absThresholdValue
 
uint8_t IdealSample_sampleAdjustCount
 
uint8_t IdealSample_mode
 
bool IdealSample_bottomSampleEnable
 
bool Pg_estimationEnable
 
uint8_t Pg_estimationLimit
 
bool Pg_correctionEnable
 
bool Pg_autoCorrectionEnable
 
uint16_t Pg_sinGainBypassValue
 
uint16_t Pg_cosGainBypassValue
 
int16_t Pg_cosPhaseBypassValue
 
Track2Constants_t track2Constants
 

Field Documentation

◆ BpfDc_bpfEnable

bool Core_config_t::BpfDc_bpfEnable

◆ BpfDc_offsetCorrectionEnable

bool Core_config_t::BpfDc_offsetCorrectionEnable

◆ BpfDc_dcOffCal1

uint8_t Core_config_t::BpfDc_dcOffCal1

◆ BpfDc_dcOffCal2

uint8_t Core_config_t::BpfDc_dcOffCal2

◆ BpfDc_manualSin

int16_t Core_config_t::BpfDc_manualSin

◆ BpfDc_manualCos

int16_t Core_config_t::BpfDc_manualCos

◆ IdealSample_overrideValue

uint8_t Core_config_t::IdealSample_overrideValue

◆ IdealSample_absThresholdValue

uint16_t Core_config_t::IdealSample_absThresholdValue

◆ IdealSample_sampleAdjustCount

uint8_t Core_config_t::IdealSample_sampleAdjustCount

◆ IdealSample_mode

uint8_t Core_config_t::IdealSample_mode

◆ IdealSample_bottomSampleEnable

bool Core_config_t::IdealSample_bottomSampleEnable

◆ Pg_estimationEnable

bool Core_config_t::Pg_estimationEnable

◆ Pg_estimationLimit

uint8_t Core_config_t::Pg_estimationLimit

◆ Pg_correctionEnable

bool Core_config_t::Pg_correctionEnable

◆ Pg_autoCorrectionEnable

bool Core_config_t::Pg_autoCorrectionEnable

◆ Pg_sinGainBypassValue

uint16_t Core_config_t::Pg_sinGainBypassValue

◆ Pg_cosGainBypassValue

uint16_t Core_config_t::Pg_cosGainBypassValue

◆ Pg_cosPhaseBypassValue

int16_t Core_config_t::Pg_cosPhaseBypassValue

◆ track2Constants

Track2Constants_t Core_config_t::track2Constants