AM263Px MCU+ SDK  10.02.00
APIs for DTHE SHA

Introduction

This module contains APIs to program and use the DTHE SHA.

Files

file  dthe_sha.h
 This file contains the prototype of DTHE SHA driver APIs.
 

Data Structures

struct  DTHE_SHA_Params
 Parameters required for SHA Driver. More...
 

Functions

DTHE_SHA_Return_t DTHE_SHA_open (DTHE_Handle handle)
 Function to Open DTHE SHA Driver. More...
 
DTHE_SHA_Return_t DTHE_SHA_compute (DTHE_Handle handle, DTHE_SHA_Params *ptrShaParams, int32_t isLastBlock)
 The function is used to execute the SHA Driver with the specified parameters. More...
 
DTHE_SHA_Return_t DTHE_HMACSHA_compute (DTHE_Handle handle, DTHE_SHA_Params *ptrShaParams)
 The function is used to execute the HMAC SHA Operations with the specified parameters. More...
 
DTHE_SHA_Return_t DTHE_SHA_close (DTHE_Handle handle)
 Function to close DTHE SHA Driver. More...
 

Enumerations

enum  DTHE_SHA_Return_t { DTHE_SHA_RETURN_SUCCESS = 0x67A42DD1U, DTHE_SHA_RETURN_FAILURE = 0x06C2B483U }
 DTHE SHA Driver Error code. More...
 

Macros

#define DTHE_SHA_ALGO_MD5   (0x1U)
 MD5 Flag. More...
 
#define DTHE_SHA_ALGO_SHA384   (0x2U)
 SHA-384 Flag. More...
 
#define DTHE_SHA_ALGO_SHA1   (0x3U)
 SHA-1 Flag. More...
 
#define DTHE_SHA_ALGO_SHA512   (0x4U)
 SHA-512 Flag. More...
 
#define DTHE_SHA_ALGO_SHA224   (0x5U)
 SHA-224 Flag. More...
 
#define DTHE_SHA_ALGO_SHA256   (0x6U)
 SHA-256 Flag. More...
 
#define DTHE_SHA_MAX_DIGEST_SIZE_BYTES   (64U)
 The Maximum Digest Size is 64bytes for the SHA512. More...
 

Macro Definition Documentation

◆ DTHE_SHA_ALGO_MD5

#define DTHE_SHA_ALGO_MD5   (0x1U)

MD5 Flag.

< SHA Algorithms

◆ DTHE_SHA_ALGO_SHA384

#define DTHE_SHA_ALGO_SHA384   (0x2U)

SHA-384 Flag.

◆ DTHE_SHA_ALGO_SHA1

#define DTHE_SHA_ALGO_SHA1   (0x3U)

SHA-1 Flag.

◆ DTHE_SHA_ALGO_SHA512

#define DTHE_SHA_ALGO_SHA512   (0x4U)

SHA-512 Flag.

◆ DTHE_SHA_ALGO_SHA224

#define DTHE_SHA_ALGO_SHA224   (0x5U)

SHA-224 Flag.

◆ DTHE_SHA_ALGO_SHA256

#define DTHE_SHA_ALGO_SHA256   (0x6U)

SHA-256 Flag.

◆ DTHE_SHA_MAX_DIGEST_SIZE_BYTES

#define DTHE_SHA_MAX_DIGEST_SIZE_BYTES   (64U)

The Maximum Digest Size is 64bytes for the SHA512.

Enumeration Type Documentation

◆ DTHE_SHA_Return_t

DTHE SHA Driver Error code.

The enumeration describes all the possible return and error codes which the DTHE SHA Driver can return

Enumerator
DTHE_SHA_RETURN_SUCCESS 

Success/pass return code

DTHE_SHA_RETURN_FAILURE 

General or unspecified failure/error

Function Documentation

◆ DTHE_SHA_open()

DTHE_SHA_Return_t DTHE_SHA_open ( DTHE_Handle  handle)

Function to Open DTHE SHA Driver.

Parameters
handleDTHE_Handle returned from DTHE_open().
Returns
DTHE_SHA_RETURN_SUCCESS if requested operation completed. DTHE_SHA_RETURN_FAILURE if requested operation not completed.

◆ DTHE_SHA_compute()

DTHE_SHA_Return_t DTHE_SHA_compute ( DTHE_Handle  handle,
DTHE_SHA_Params ptrShaParams,
int32_t  isLastBlock 
)

The function is used to execute the SHA Driver with the specified parameters.

Parameters
handleDTHE_Handle returned from DTHE_open().
ptrShaParamsPointer to the parameters to be used to execute the driver.
isLastBlockUsed for singleshot and multishot sha.
Returns
DTHE_SHA_RETURN_SUCCESS if requested operation completed. DTHE_SHA_RETURN_FAILURE if requested operation not completed.

◆ DTHE_HMACSHA_compute()

DTHE_SHA_Return_t DTHE_HMACSHA_compute ( DTHE_Handle  handle,
DTHE_SHA_Params ptrShaParams 
)

The function is used to execute the HMAC SHA Operations with the specified parameters.

Parameters
handleDTHE_Handle returned from DTHE_open().
ptrShaParamsPointer to the parameters to be used to execute the driver.
Returns
DTHE_SHA_RETURN_SUCCESS if requested operation completed. DTHE_SHA_RETURN_FAILURE if requested operation not completed.

◆ DTHE_SHA_close()

DTHE_SHA_Return_t DTHE_SHA_close ( DTHE_Handle  handle)

Function to close DTHE SHA Driver.

Parameters
handleDTHE_Handle returned from DTHE_open().
Returns
DTHE_SHA_RETURN_SUCCESS if requested operation completed. DTHE_SHA_RETURN_FAILURE if requested operation not completed.