AM263Px MCU+ SDK  10.02.00
VTM IP Enumerated Data Types

Introduction

Provides the APIs for VTM IP.

Data Structures

struct  SDL_VTM_Stat_val
 VTM temperature sensor Stat values. More...
 

Typedefs

typedef uint8_t SDL_VTM_configVdCtrl
 This enumerator define for VTM VD configuration valid map. More...
 
typedef uint8_t SDL_VTM_configTsCtrl
 This enumerator define for VTM TS configuration valid map. More...
 
typedef int16_t SDL_VTM_adc_code
 This typedef for VTM temperature sensor ADC code This is the data_out value of the temperature sensor stat register. More...
 

Macros

#define SDL_VTM_VD_CONFIG_CTRL_VID_OPP   (1U)
 
#define SDL_VTM_VD_CONFIG_CTRL_EVT_SEL   (2U)
 
#define SDL_VTM_VD_CONFIG_CTRL_GLB_CFG   (4U)
 
#define SDL_VTM_VD_CONFIG_CTRL_SET_CTL   (1U)
 
#define SDL_VTM_VD_CONFIG_CTRL_OUTRNG_ALRT   (2U)
 
#define SDL_VTM_VD_CONFIG_CTRL_SET_THR   (4U)
 
#define SDL_VTM_BGR_OFF   0x1U
 This enumerator defines the possible VID Codes to set various voltage domain supply voltages. More...
 
#define SDL_VTM_BGR_ON   0x0U
 
#define SDL_VTM_AIP_OFF   0x1U
 
#define SDL_VTM_AIP_ON   0x0U
 
#define SDL_VTM_TMPSOFF_OFF   0x1U
 
#define SDL_VTM_TMPSOFF_ON   0x0U
 
#define SDL_VTM_MUX_HIZ   0x1U
 
#define SDL_VTM_NORMAL_HIZ   0x0U
 
#define SDL_VTM_SENSOR_SEL0   (1U << 0U)
 
#define SDL_VTM_SENSOR_SEL1   (1U << 1U)
 
#define SDL_VTM_SENSOR_SEL2   (1U << 2U)
 
#define SDL_VTM_SENSOR_SEL3   (1U << 3U)
 
#define SDL_VTM_TSENSE_EN   0x1U
 
#define SDL_VTM_TSENSE_DIS   0x0U
 
#define SDL_VTM_TSENSE0_LOW_TH_FLAG   (1U << 0U)
 
#define SDL_VTM_TSENSE0_HOT_FLAG   (1U << 2U)
 
#define SDL_VTM_TSENSE0_COLD_FLAG   (1U << 1U)
 
#define SDL_VTM_TSENSE1_LOW_TH_FLAG   (1U << 4U)
 
#define SDL_VTM_TSENSE1_HOT_FLAG   (1U << 6U)
 
#define SDL_VTM_TSENSE1_COLD_FLAG   (1U << 5U)
 
#define SDL_VTM_OVERRIDE_PATTERN   0x7U
 
#define SDL_VTM_MASK_LOW_TH   (1U)
 
#define SDL_VTM_MASK_COLD   (1U)
 
#define SDL_VTM_MASK_HOT   (1U)
 
#define SDL_VTM_FREEZE_FIFO   1U
 
#define SDL_VTM_CLR_FIFO   1U
 
#define SDL_VTM_CLR_ACCU   1U
 
#define SDL_VTM_BUF_NUM0   0U
 
#define SDL_VTM_BUF_NUM1   1U
 
#define SDL_VTM_BUF_NUM2   2U
 
#define SDL_VTM_BUF_NUM3   3U
 
#define SDL_VTM_TSENSE_OFF   0U
 
#define SDL_VTM_TSENSE_ON   1U
 
#define SDL_VTM_MAXDELAY   0x2FU
 

Macro Definition Documentation

◆ SDL_VTM_VD_CONFIG_CTRL_VID_OPP

#define SDL_VTM_VD_CONFIG_CTRL_VID_OPP   (1U)

◆ SDL_VTM_VD_CONFIG_CTRL_EVT_SEL

#define SDL_VTM_VD_CONFIG_CTRL_EVT_SEL   (2U)

◆ SDL_VTM_VD_CONFIG_CTRL_GLB_CFG

#define SDL_VTM_VD_CONFIG_CTRL_GLB_CFG   (4U)

◆ SDL_VTM_VD_CONFIG_CTRL_SET_CTL

#define SDL_VTM_VD_CONFIG_CTRL_SET_CTL   (1U)

◆ SDL_VTM_VD_CONFIG_CTRL_OUTRNG_ALRT

#define SDL_VTM_VD_CONFIG_CTRL_OUTRNG_ALRT   (2U)

◆ SDL_VTM_VD_CONFIG_CTRL_SET_THR

#define SDL_VTM_VD_CONFIG_CTRL_SET_THR   (4U)

◆ SDL_VTM_BGR_OFF

#define SDL_VTM_BGR_OFF   0x1U

This enumerator defines the possible VID Codes to set various voltage domain supply voltages.

◆ SDL_VTM_BGR_ON

#define SDL_VTM_BGR_ON   0x0U

◆ SDL_VTM_AIP_OFF

#define SDL_VTM_AIP_OFF   0x1U

◆ SDL_VTM_AIP_ON

#define SDL_VTM_AIP_ON   0x0U

◆ SDL_VTM_TMPSOFF_OFF

#define SDL_VTM_TMPSOFF_OFF   0x1U

◆ SDL_VTM_TMPSOFF_ON

#define SDL_VTM_TMPSOFF_ON   0x0U

◆ SDL_VTM_MUX_HIZ

#define SDL_VTM_MUX_HIZ   0x1U

◆ SDL_VTM_NORMAL_HIZ

#define SDL_VTM_NORMAL_HIZ   0x0U

◆ SDL_VTM_SENSOR_SEL0

#define SDL_VTM_SENSOR_SEL0   (1U << 0U)

◆ SDL_VTM_SENSOR_SEL1

#define SDL_VTM_SENSOR_SEL1   (1U << 1U)

◆ SDL_VTM_SENSOR_SEL2

#define SDL_VTM_SENSOR_SEL2   (1U << 2U)

◆ SDL_VTM_SENSOR_SEL3

#define SDL_VTM_SENSOR_SEL3   (1U << 3U)

◆ SDL_VTM_TSENSE_EN

#define SDL_VTM_TSENSE_EN   0x1U

◆ SDL_VTM_TSENSE_DIS

#define SDL_VTM_TSENSE_DIS   0x0U

◆ SDL_VTM_TSENSE0_LOW_TH_FLAG

#define SDL_VTM_TSENSE0_LOW_TH_FLAG   (1U << 0U)

◆ SDL_VTM_TSENSE0_HOT_FLAG

#define SDL_VTM_TSENSE0_HOT_FLAG   (1U << 2U)

◆ SDL_VTM_TSENSE0_COLD_FLAG

#define SDL_VTM_TSENSE0_COLD_FLAG   (1U << 1U)

◆ SDL_VTM_TSENSE1_LOW_TH_FLAG

#define SDL_VTM_TSENSE1_LOW_TH_FLAG   (1U << 4U)

◆ SDL_VTM_TSENSE1_HOT_FLAG

#define SDL_VTM_TSENSE1_HOT_FLAG   (1U << 6U)

◆ SDL_VTM_TSENSE1_COLD_FLAG

#define SDL_VTM_TSENSE1_COLD_FLAG   (1U << 5U)

◆ SDL_VTM_OVERRIDE_PATTERN

#define SDL_VTM_OVERRIDE_PATTERN   0x7U

◆ SDL_VTM_MASK_LOW_TH

#define SDL_VTM_MASK_LOW_TH   (1U)

◆ SDL_VTM_MASK_COLD

#define SDL_VTM_MASK_COLD   (1U)

◆ SDL_VTM_MASK_HOT

#define SDL_VTM_MASK_HOT   (1U)

◆ SDL_VTM_FREEZE_FIFO

#define SDL_VTM_FREEZE_FIFO   1U

◆ SDL_VTM_CLR_FIFO

#define SDL_VTM_CLR_FIFO   1U

◆ SDL_VTM_CLR_ACCU

#define SDL_VTM_CLR_ACCU   1U

◆ SDL_VTM_BUF_NUM0

#define SDL_VTM_BUF_NUM0   0U

◆ SDL_VTM_BUF_NUM1

#define SDL_VTM_BUF_NUM1   1U

◆ SDL_VTM_BUF_NUM2

#define SDL_VTM_BUF_NUM2   2U

◆ SDL_VTM_BUF_NUM3

#define SDL_VTM_BUF_NUM3   3U

◆ SDL_VTM_TSENSE_OFF

#define SDL_VTM_TSENSE_OFF   0U

◆ SDL_VTM_TSENSE_ON

#define SDL_VTM_TSENSE_ON   1U

◆ SDL_VTM_MAXDELAY

#define SDL_VTM_MAXDELAY   0x2FU

Typedef Documentation

◆ SDL_VTM_configVdCtrl

typedef uint8_t SDL_VTM_configVdCtrl

This enumerator define for VTM VD configuration valid map.

◆ SDL_VTM_configTsCtrl

typedef uint8_t SDL_VTM_configTsCtrl

This enumerator define for VTM TS configuration valid map.

◆ SDL_VTM_adc_code

typedef int16_t SDL_VTM_adc_code

This typedef for VTM temperature sensor ADC code This is the data_out value of the temperature sensor stat register.