For more details and example usage, see SOC
Sub Modules | |
| APIs for SOC Reset and Clock Functions | |
| APIs for SOC Xbars | |
Functions | |
| static int32_t | MCSPI_lld_isBaseAddrValid (uint32_t baseAddr) |
| API to validate MCSPI base address. More... | |
| static int32_t | MMCSD_lld_isBaseAddrValid (uint32_t baseAddr) |
| API to validate MMCSD base addresses. More... | |
| int32_t | SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable) |
| Enable clock to specified module. More... | |
| int32_t | SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate) |
| Set module clock to specified frequency. More... | |
| const char * | SOC_getCoreName (uint16_t coreId) |
| Convert a core ID to a user readable name. More... | |
| uint64_t | SOC_getSelfCpuClk (void) |
| Get the clock frequency in Hz of the CPU on which the driver is running. More... | |
| void | SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition) |
| Lock control module partition to prevent writes into control MMRs. More... | |
| void | SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition) |
| Unlock control module partition to allow writes into control MMRs. More... | |
| void | SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable) |
| Enable or disable ePWM time base clock from Control MMR. More... | |
| void | SOC_setMultipleEpwmTbClk (uint32_t epwmMask, uint32_t enable) |
| Enable or disable Multiple ePWM time base clock from Control MMR. More... | |
| void | SOC_enableAdcReference (uint32_t adcInstance) |
| Enable ADC references by writing to Control MMR. More... | |
| void | SOC_enableAdcInternalReference (uint32_t adcInstance, uint32_t enable) |
| Enables the ADC internal reference. More... | |
| void | SOC_enableAdcReferenceMonitor (uint32_t adcInstance, uint32_t enable) |
| Enable ADC reference Monitors by writing to Control MMR. More... | |
| uint32_t | SOC_getAdcReferenceStatus (uint32_t adcInstance) |
| Gets the Reference status. More... | |
| void | SOC_enableAdcOsdChannel (uint32_t adcInstance, uint32_t channel, uint32_t enable) |
| Enable or disable the OSD circuit over the ADC channels. More... | |
| void | SOC_setAdcOsdConfig (uint32_t adcInstance, uint32_t config) |
| Sets the ADC OSD Configuration. More... | |
| void | SOC_enableAdcGlobalForce (uint32_t adcInstance, uint32_t enable) |
| Enable or Disable the ADC instnace for Gloabl SW force. More... | |
| void | SOC_adcSocGlobalForce (uint32_t socNumber) |
| Triggers a global force for the SOC in enabled ADCs the ADCs may be enabled by using SOC_enableAdcGlobalForce() API. More... | |
| void | SOC_selectAdcExtChXbar (uint32_t extChXbarOut, uint32_t extChXbarIn) |
| Selects the ADC External Channel Select bit for the output from each xbar out. More... | |
| void | SOC_selextAdcExtChDelay (uint32_t delay) |
| Mux select to choose delay for ADC Extchsel. More... | |
| void | SOC_enableAdcDacLoopback (uint32_t enable) |
| Enable or Disable the ADC CAL Pin to loopback with DAC. More... | |
| void | SOC_enableCmpssaDacLoopBack (uint32_t cmpssaInstance, uint32_t dacType, uint32_t enable) |
| Enable or disable the CMPSS - DAC Loop Back configuration. More... | |
| void | SOC_enableCmpssbDacLoopBack (uint32_t cmpssbInstance, uint32_t dacType, uint32_t enable) |
| Enable or disable the CMPSS - DAC Loop Back configuration. More... | |
| void | SOC_setEpwmGroup (uint32_t epwmInstance, uint32_t group) |
| Configure the ePWM group. More... | |
| void | SOC_selectSdfm1Clk0Source (uint8_t source) |
| Select the SDFM1 CLK0 source. More... | |
| void | SOC_sdfmClkLoopBackConfig (uint32_t sdfmInstance, uint32_t clkInstance, uint32_t defaultValue) |
| Sets the configuraion for the loopback control. More... | |
| void | SOC_gateEpwmClock (uint32_t epwmInstance) |
| Gate the ePWM clock. More... | |
| void | SOC_ungateEpwmClock (uint32_t epwmInstance) |
| Ungate the ePWM clock. More... | |
| void | SOC_gateFsitxClock (uint32_t fsitxInstance) |
| Gate the FSI-TX clock. More... | |
| void | SOC_gateFsirxClock (uint32_t fsirxInstance) |
| Gate the FSI-RX clock. More... | |
| void | SOC_gateCmpssaClock (uint32_t cmpssaInstance) |
| Gate the CMPSS-A clock. More... | |
| void | SOC_ungateCmpssaClock (uint32_t cmpssaInstance) |
| Ungate the CMPSS-A clock. More... | |
| void | SOC_gateCmpssbClock (uint32_t cmpssbInstance) |
| Gate the CMPSS-B clock. More... | |
| void | SOC_ungateCmpssbClock (uint32_t cmpssbInstance) |
| Ungate the CMPSS-B clock. More... | |
| void | SOC_gateEcapClock (uint32_t ecapInstance) |
| Gate the ECAP clock. More... | |
| void | SOC_ungateEcapClock (uint32_t ecapInstance) |
| Ungate the ECAP clock. More... | |
| void | SOC_gateEqepClock (uint32_t eqepInstance) |
| Gate the EQEP clock. More... | |
| void | SOC_ungateEqepClock (uint32_t eqepInstance) |
| Ungate the EQEP clock. More... | |
| void | SOC_gateSdfmClock (uint32_t sdfmInstance) |
| Gate the SDFM clock. More... | |
| void | SOC_ungateSdfmClock (uint32_t sdfmInstance) |
| Ungate the SDFM clock. More... | |
| void | SOC_gateDacClock (void) |
| Gate the DAC clock. More... | |
| void | SOC_ungateDacClock (void) |
| Ungate the DAC clock. More... | |
| void | SOC_gateAdcClock (uint32_t adcInstance) |
| Gate the ADC clock. More... | |
| void | SOC_ungateAdcClock (uint32_t adcInstance) |
| ungate the ADC clock More... | |
| void | SOC_gateRdcClock (uint32_t rdcInstance) |
| Gate the HW_RESOLVER clock. More... | |
| void | SOC_ungateRdcClock (uint32_t rdcInstance) |
| Ungate the HW_RESOLVER clock. More... | |
| void | SOC_gateOttoClock (uint32_t ottoInstance) |
| Gate the OTTO clock. More... | |
| void | SOC_ungateOttoClock (uint32_t ottoInstance) |
| Ungate the OTTO clock. More... | |
| void | SOC_gateSdfmPllClock (uint32_t sdfmInstance) |
| Gate the SDFM PLL clock. More... | |
| void | SOC_ungateSdfmPllClock (uint32_t sdfmInstance) |
| Ungate the SDFM PLL clock. More... | |
| void | SOC_gateFsiPllClock (uint32_t fsiInstance) |
| Gate the FSI-TX PLL clock. More... | |
| void | SOC_generateEpwmReset (uint32_t ePWMInstance) |
| Generate ePWM reset. More... | |
| void | SOC_generateFsiTxReset (uint32_t fsitxInstance) |
| Generate FSI-TX reset. More... | |
| void | SOC_generateFsiRxReset (uint32_t fsirxInstance) |
| Generate FSI-RX reset. More... | |
| void | SOC_generateCmpssaReset (uint32_t cmpssaInstance) |
| Generate CMPSS-A reset. More... | |
| void | SOC_generateCmpssbReset (uint32_t cmpssbInstance) |
| Generate CMPSS-B reset. More... | |
| void | SOC_generateEcapReset (uint32_t ecapInstance) |
| Generate ECAP reset. More... | |
| void | SOC_generateEqepReset (uint32_t eqepInstance) |
| Generate EQEP reset. More... | |
| void | SOC_generateSdfmReset (uint32_t sdfmInstance) |
| Generate SDFM reset. More... | |
| void | SOC_generateDacReset (void) |
| Generate DAC reset. More... | |
| void | SOC_generateAdcReset (uint32_t adcInstance) |
| Generate ADC reset. More... | |
| void | SOC_generateRdcReset (uint32_t rdcInstance) |
| Generate RDC reset. More... | |
| void | Soc_enableEPWMHalt (uint32_t epwmInstance) |
| Halt EPWM with corresponding cPU. More... | |
| void | Soc_disableEPWMHalt (uint32_t epwmInstance) |
| Halt EPWM with corresponding cPU. More... | |
| void | Soc_enableECAPHalt (uint32_t ecapInstance) |
| Halt ECAP with corresponding cPU. More... | |
| void | Soc_disableECAPHalt (uint32_t ecapInstance) |
| Halt ECAP with corresponding cPU. More... | |
| void | SOC_generateOttoReset (uint32_t ottoInstance) |
| Generate OTTO reset. More... | |
| void | SOC_selectIcssGpiMux (uint8_t pru_instance, uint32_t mask) |
| Selection of ICSS GPI MUX. More... | |
| uint64_t | SOC_virtToPhy (void *virtAddr) |
| SOC Virtual (CPU) to Physical address translation function. More... | |
| void * | SOC_phyToVirt (uint64_t phyAddr) |
| Physical to Virtual (CPU) address translation function. More... | |
| uint32_t | SOC_getFlashDataBaseAddr (void) |
| This function gets the SOC mapped data base address of the flash. More... | |
| void | SOC_sendSoftwareInterrupt (uint16_t coreId) |
| Send SOC level software triggered address. More... | |
| static int32_t | UART_IsBaseAddrValid (uint32_t baseAddr) |
| API to validate UART base address. More... | |
Macros | |
| #define | MSS_CTRL_PARTITION0 (1) |
| #define | TOP_CTRL_PARTITION0 (2) |
| #define | CONTROLSS_CTRL_PARTITION0 (3) |
| #define | MSS_RCM_PARTITION0 (4) |
| #define | TOP_RCM_PARTITION0 (5) |
| #define | KICK_LOCK_VAL (0x00000000U) |
| #define | KICK0_UNLOCK_VAL (0x01234567U) |
| #define | KICK1_UNLOCK_VAL (0x0FEDCBA8U) |
| #define | ADC0_EXTCHSEL_BIT0 (0U) |
| #define | ADC0_EXTCHSEL_BIT1 (1U) |
| #define | ADC1_EXTCHSEL_BIT0 (2U) |
| #define | ADC1_EXTCHSEL_BIT1 (3U) |
| #define | ADC2_EXTCHSEL_BIT0 (4U) |
| #define | ADC2_EXTCHSEL_BIT1 (5U) |
| #define | ADC3_EXTCHSEL_BIT0 (6U) |
| #define | ADC3_EXTCHSEL_BIT1 (7U) |
| #define | ADC4_EXTCHSEL_BIT0 (8U) |
| #define | ADC4_EXTCHSEL_BIT1 (9U) |
| #define | ADC_R0_EXTCHSEL_BIT0 (10U) |
| #define | ADC_R0_EXTCHSEL_BIT1 (11U) |
| #define | ADC_R1_EXTCHSEL_BIT0 (12U) |
| #define | ADC_R2_EXTCHSEL_BIT1 (13U) |
| #define | ADC_EXTCHSELCT_DELAY_3_CYCLES (0U) |
| #define | ADC_EXTCHSELCT_DELAY_6_CYCLES (1U) |
| #define | CMPSS_LOOP_BACK_INH (0U) |
| #define | CMPSS_LOOP_BACK_INL (1U) |
| #define | IS_I2C_BASE_ADDR_VALID(baseAddr) |
| #define | IS_OSPI_BASE_ADDR_VALID(baseAddr) (baseAddr == CSL_FLASH_CONFIG_REG8_U_BASE) |
| Macro to check if the OSPI base address is valid. More... | |
| #define | IS_OSPI_DATA_BASE_ADDR_VALID(baseAddr) (baseAddr == CSL_FLASH_DATA_REG0_U_BASE) |
| Macro to check if the OSPI base address is valid. More... | |
SOC Domain ID | |
| #define | SOC_DOMAIN_ID_MAIN (0U) |
| #define SOC_DOMAIN_ID_MAIN (0U) |
| #define MSS_CTRL_PARTITION0 (1) |
| #define TOP_CTRL_PARTITION0 (2) |
| #define CONTROLSS_CTRL_PARTITION0 (3) |
| #define MSS_RCM_PARTITION0 (4) |
| #define TOP_RCM_PARTITION0 (5) |
| #define KICK_LOCK_VAL (0x00000000U) |
| #define KICK0_UNLOCK_VAL (0x01234567U) |
| #define KICK1_UNLOCK_VAL (0x0FEDCBA8U) |
| #define ADC0_EXTCHSEL_BIT0 (0U) |
| #define ADC0_EXTCHSEL_BIT1 (1U) |
| #define ADC1_EXTCHSEL_BIT0 (2U) |
| #define ADC1_EXTCHSEL_BIT1 (3U) |
| #define ADC2_EXTCHSEL_BIT0 (4U) |
| #define ADC2_EXTCHSEL_BIT1 (5U) |
| #define ADC3_EXTCHSEL_BIT0 (6U) |
| #define ADC3_EXTCHSEL_BIT1 (7U) |
| #define ADC4_EXTCHSEL_BIT0 (8U) |
| #define ADC4_EXTCHSEL_BIT1 (9U) |
| #define ADC_R0_EXTCHSEL_BIT0 (10U) |
| #define ADC_R0_EXTCHSEL_BIT1 (11U) |
| #define ADC_R1_EXTCHSEL_BIT0 (12U) |
| #define ADC_R2_EXTCHSEL_BIT1 (13U) |
| #define ADC_EXTCHSELCT_DELAY_3_CYCLES (0U) |
| #define ADC_EXTCHSELCT_DELAY_6_CYCLES (1U) |
| #define CMPSS_LOOP_BACK_INH (0U) |
| #define CMPSS_LOOP_BACK_INL (1U) |
| #define IS_I2C_BASE_ADDR_VALID | ( | baseAddr | ) |
| #define IS_OSPI_BASE_ADDR_VALID | ( | baseAddr | ) | (baseAddr == CSL_FLASH_CONFIG_REG8_U_BASE) |
Macro to check if the OSPI base address is valid.
| #define IS_OSPI_DATA_BASE_ADDR_VALID | ( | baseAddr | ) | (baseAddr == CSL_FLASH_DATA_REG0_U_BASE) |
Macro to check if the OSPI base address is valid.
|
inlinestatic |
API to validate MCSPI base address.
|
inlinestatic |
API to validate MMCSD base addresses.
| int32_t SOC_moduleClockEnable | ( | uint32_t | moduleId, |
| uint32_t | enable | ||
| ) |
Enable clock to specified module.
| moduleId | [in] see SOC_RcmPeripheralId for list of module ID's |
| enable | [in] 1: enable clock to the module, 0: disable clock to the module |
| int32_t SOC_moduleSetClockFrequency | ( | uint32_t | moduleId, |
| uint32_t | clkId, | ||
| uint64_t | clkRate | ||
| ) |
Set module clock to specified frequency.
| moduleId | [in] see SOC_RcmPeripheralId for list of module ID's |
| clkId | [in] see SOC_RcmPeripheralClockSource for list of clocks |
| clkRate | [in] Frequency to set in Hz |
| const char* SOC_getCoreName | ( | uint16_t | coreId | ) |
Convert a core ID to a user readable name.
| coreId | [in] see CSL_CoreID |
| uint64_t SOC_getSelfCpuClk | ( | void | ) |
Get the clock frequency in Hz of the CPU on which the driver is running.
| void SOC_controlModuleLockMMR | ( | uint32_t | domainId, |
| uint32_t | partition | ||
| ) |
Lock control module partition to prevent writes into control MMRs.
| domainId | [in] See SOC_DomainId_t |
| partition | [in] Partition number to unlock |
| void SOC_controlModuleUnlockMMR | ( | uint32_t | domainId, |
| uint32_t | partition | ||
| ) |
Unlock control module partition to allow writes into control MMRs.
| domainId | [in] See SOC_DomainId_t |
| partition | [in] Partition number to unlock |
| void SOC_setEpwmTbClk | ( | uint32_t | epwmInstance, |
| uint32_t | enable | ||
| ) |
Enable or disable ePWM time base clock from Control MMR.
| epwmInstance | [in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)] |
| enable | [in] TRUE to enable and FALSE to disable |
| void SOC_setMultipleEpwmTbClk | ( | uint32_t | epwmMask, |
| uint32_t | enable | ||
| ) |
Enable or disable Multiple ePWM time base clock from Control MMR.
| epwmMask | [in] ePWM instance Mask [1 - CSL_CONTROLSS_CTRL_EPWM_CLKSYNC_BIT_MAX] |
| enable | [in] TRUE to enable and FALSE to disable |
| void SOC_enableAdcReference | ( | uint32_t | adcInstance | ) |
Enable ADC references by writing to Control MMR.
| adcInstance | [in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)] |
| void SOC_enableAdcInternalReference | ( | uint32_t | adcInstance, |
| uint32_t | enable | ||
| ) |
Enables the ADC internal reference.
| adcInstance | [in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)] |
| enable | [in] TRUE to enable internal reference - FALSE to disable. |
| void SOC_enableAdcReferenceMonitor | ( | uint32_t | adcInstance, |
| uint32_t | enable | ||
| ) |
Enable ADC reference Monitors by writing to Control MMR.
| adcInstance | [in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)] |
| enable | [in] TRUE to enable internal reference Monitor - FALSE to disable. |
| uint32_t SOC_getAdcReferenceStatus | ( | uint32_t | adcInstance | ) |
Gets the Reference status.
| adcInstance | [in] ADC instance number [0 - (CSL_ADC_PER_CNT-1)] |
| void SOC_enableAdcOsdChannel | ( | uint32_t | adcInstance, |
| uint32_t | channel, | ||
| uint32_t | enable | ||
| ) |
Enable or disable the OSD circuit over the ADC channels.
| adcInstance | [in] ADC instance [0 - 4] ADC_R instance [5,6] |
| channel | [in] Channel number for the ADC. [0 - 5] |
| enable | [in] TRUE to enable and FALSE to disable the OSD circuit. |
| void SOC_setAdcOsdConfig | ( | uint32_t | adcInstance, |
| uint32_t | config | ||
| ) |
Sets the ADC OSD Configuration.
| adcInstance | [in] ADC instance [0 - 4] ADC_R instance [5,6] |
| config | [in] configuration to be enabled of the OSD circuit. |
It is recommended to wait for atleast 1uS after configuration, before sampling
| config | function | Impedance | Voltage on 5K | Voltage on 7K |
|---|---|---|---|---|
| 0 | Zero Scale | 5K // 7K | VSSA | VSSA |
| ------— | ------------— | --------— | ------------— | --------— |
| 1 | Zero Scale | 5K | VSSA | OPEN |
| ------— | ------------— | --------— | ------------— | --------— |
| 2 | Zero Scale | 7K | OPEN | VSSA |
| ------— | ------------— | --------— | ------------— | --------— |
| 3 | Full Scale | 5K // 7K | VDD | VDD |
| ------— | ------------— | --------— | ------------— | --------— |
| 4 | Full Scale | 5K | VDD | OPEN |
| ------— | ------------— | --------— | ------------— | --------— |
| 5 | Full Scale | 7K | OPEN | VDD |
| ------— | ------------— | --------— | ------------— | --------— |
| 6 | 5/12 Scale | 5K // 7K | VSSA | VDD |
| ------— | ------------— | --------— | ------------— | --------— |
| 7 | 5/12 Scale | 5K // 7K | VDD | VSSA |
| ------— | ------------— | --------— | ------------— | --------— |
| void SOC_enableAdcGlobalForce | ( | uint32_t | adcInstance, |
| uint32_t | enable | ||
| ) |
Enable or Disable the ADC instnace for Gloabl SW force.
| adcInstance | [in] ADC instances [0 - 4] ADC_R instance [ 5 - 6] |
| enable | [in] TRUE to enable and FALSE to disable the GLobal Force Selection |
| void SOC_adcSocGlobalForce | ( | uint32_t | socNumber | ) |
Triggers a global force for the SOC in enabled ADCs the ADCs may be enabled by using SOC_enableAdcGlobalForce() API.
| socNumber | [in] SOC Number [0 - 15] |
| void SOC_selectAdcExtChXbar | ( | uint32_t | extChXbarOut, |
| uint32_t | extChXbarIn | ||
| ) |
Selects the ADC External Channel Select bit for the output from each xbar out.
| extChXbarOut | [in] selects the ADC_EXTCHSEL_XBAR_OUTx x in [0 - 9] |
| extChXbarIn | [in] Valid Values are the following ADC0_EXTCHSEL_BIT0 ADC0_EXTCHSEL_BIT1 ADC1_EXTCHSEL_BIT0 ADC1_EXTCHSEL_BIT1 ADC2_EXTCHSEL_BIT0 ADC2_EXTCHSEL_BIT1 ADC3_EXTCHSEL_BIT0 ADC3_EXTCHSEL_BIT1 ADC4_EXTCHSEL_BIT0 ADC4_EXTCHSEL_BIT1 ADC_R0_EXTCHSEL_BIT0 ADC_R0_EXTCHSEL_BIT1 ADC_R1_EXTCHSEL_BIT0 ADC_R2_EXTCHSEL_BIT1 |
| void SOC_selextAdcExtChDelay | ( | uint32_t | delay | ) |
Mux select to choose delay for ADC Extchsel.
| delay | [in] 3 Cycle Delay or 6 Cycle Delay Valid Values are ADC_EXTCHSELCT_DELAY_3_CYCLES ADC_EXTCHSELCT_DELAY_6_CYCLES |
| void SOC_enableAdcDacLoopback | ( | uint32_t | enable | ) |
Enable or Disable the ADC CAL Pin to loopback with DAC.
| enable | [in] TRUE to enable, FALSE to disable |
| void SOC_enableCmpssaDacLoopBack | ( | uint32_t | cmpssaInstance, |
| uint32_t | dacType, | ||
| uint32_t | enable | ||
| ) |
Enable or disable the CMPSS - DAC Loop Back configuration.
| cmpssaInstance | Instance number of CMPSS TYPE A |
| dacType | determines which CMPSS input line Valid values are CMPSS_LOOP_BACK_INH CMPSS_LOOP_BACK_INL |
| enable |
| void SOC_enableCmpssbDacLoopBack | ( | uint32_t | cmpssbInstance, |
| uint32_t | dacType, | ||
| uint32_t | enable | ||
| ) |
Enable or disable the CMPSS - DAC Loop Back configuration.
| cmpssbInstance | Instance number of CMPSS TYPE B |
| dacType | determines which CMPSS input line Valid values are CMPSS_LOOP_BACK_INH CMPSS_LOOP_BACK_INL |
| enable |
| void SOC_setEpwmGroup | ( | uint32_t | epwmInstance, |
| uint32_t | group | ||
| ) |
Configure the ePWM group.
| epwmInstance | [in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)] |
| group | [in] The group for this ePWM instance [0 - 3] |
| void SOC_selectSdfm1Clk0Source | ( | uint8_t | source | ) |
Select the SDFM1 CLK0 source.
| source | [in] Source of SDFM1 CLK0. 0: source is SDFM1 CK0 from Pinmux. 1: source is SDFM0 CK0 from Pinmux |
| void SOC_sdfmClkLoopBackConfig | ( | uint32_t | sdfmInstance, |
| uint32_t | clkInstance, | ||
| uint32_t | defaultValue | ||
| ) |
Sets the configuraion for the loopback control.
| sdfmInstance | [in] SDFM instance number [0,1] |
| clkInstance | [in] SDFM Clock number [0 - 3] |
| defaultValue | [in] TRUE to set the default Loopback control loopback FALSE to set alternate Loopback control |
| void SOC_gateEpwmClock | ( | uint32_t | epwmInstance | ) |
Gate the ePWM clock.
| epwmInstance | [in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)] |
| void SOC_ungateEpwmClock | ( | uint32_t | epwmInstance | ) |
Ungate the ePWM clock.
| epwmInstance | [in] ePWM instance number [0 - (CSL_EPWM_PER_CNT-1)] |
| void SOC_gateFsitxClock | ( | uint32_t | fsitxInstance | ) |
Gate the FSI-TX clock.
| fsitxInstance | [in] FSITX instance number [0 - 3] |
| void SOC_gateFsirxClock | ( | uint32_t | fsirxInstance | ) |
Gate the FSI-RX clock.
| fsirxInstance | [in] FSIRX instance number [0 - 3] |
| void SOC_gateCmpssaClock | ( | uint32_t | cmpssaInstance | ) |
Gate the CMPSS-A clock.
| cmpssaInstance | [in] CMPSS-A instance number [0 - 9] |
| void SOC_ungateCmpssaClock | ( | uint32_t | cmpssaInstance | ) |
Ungate the CMPSS-A clock.
| cmpssaInstance | [in] CMPSS-A instance number [0 - 9] |
| void SOC_gateCmpssbClock | ( | uint32_t | cmpssbInstance | ) |
Gate the CMPSS-B clock.
| cmpssbInstance | [in] CMPSS-B instance number [0 - 9] |
| void SOC_ungateCmpssbClock | ( | uint32_t | cmpssbInstance | ) |
Ungate the CMPSS-B clock.
| cmpssbInstance | [in] CMPSS-B instance number [0 - 9] |
| void SOC_gateEcapClock | ( | uint32_t | ecapInstance | ) |
Gate the ECAP clock.
| ecapInstance | [in] ECAP instance number [0 - 9] |
| void SOC_ungateEcapClock | ( | uint32_t | ecapInstance | ) |
Ungate the ECAP clock.
| ecapInstance | [in] ECAP instance number [0 - 9] |
| void SOC_gateEqepClock | ( | uint32_t | eqepInstance | ) |
Gate the EQEP clock.
| eqepInstance | [in] EQEP instance number [0 - 2] |
| void SOC_ungateEqepClock | ( | uint32_t | eqepInstance | ) |
Ungate the EQEP clock.
| eqepInstance | [in] EQEP instance number [0 - 2] |
| void SOC_gateSdfmClock | ( | uint32_t | sdfmInstance | ) |
Gate the SDFM clock.
| sdfmInstance | [in] SDFM instance number [0 - 1] |
| void SOC_ungateSdfmClock | ( | uint32_t | sdfmInstance | ) |
Ungate the SDFM clock.
| sdfmInstance | [in] SDFM instance number [0 - 1] |
| void SOC_gateDacClock | ( | void | ) |
Gate the DAC clock.
| void SOC_ungateDacClock | ( | void | ) |
Ungate the DAC clock.
| void SOC_gateAdcClock | ( | uint32_t | adcInstance | ) |
Gate the ADC clock.
| adcInstance | [in] ADC instance number [0 - 4] or ADC_R instance [5 - 6] |
| void SOC_ungateAdcClock | ( | uint32_t | adcInstance | ) |
ungate the ADC clock
| adcInstance | [in] ADC instance number [0 - 4] or ADC_R instance [5 - 6] |
| void SOC_gateRdcClock | ( | uint32_t | rdcInstance | ) |
Gate the HW_RESOLVER clock.
| rdcInstance | [in] HW_RESOLVER instance number [0] |
| void SOC_ungateRdcClock | ( | uint32_t | rdcInstance | ) |
Ungate the HW_RESOLVER clock.
| rdcInstance | [in] HW_RESOLVER instance number [0] |
| void SOC_gateOttoClock | ( | uint32_t | ottoInstance | ) |
Gate the OTTO clock.
| ottoInstance | [in] OTTO instance number [0 - 3] |
| void SOC_ungateOttoClock | ( | uint32_t | ottoInstance | ) |
Ungate the OTTO clock.
| ottoInstance | [in] OTTO instance number [0 - 3] |
| void SOC_gateSdfmPllClock | ( | uint32_t | sdfmInstance | ) |
Gate the SDFM PLL clock.
| sdfmInstance | [in] SDFM instance number [0 - 1] |
| void SOC_ungateSdfmPllClock | ( | uint32_t | sdfmInstance | ) |
Ungate the SDFM PLL clock.
| sdfmInstance | [in] SDFM instance number [0 - 1] |
| void SOC_gateFsiPllClock | ( | uint32_t | fsiInstance | ) |
Gate the FSI-TX PLL clock.
| fsiInstance | [in] FSI instance number [0 - 3] |
| void SOC_generateEpwmReset | ( | uint32_t | ePWMInstance | ) |
Generate ePWM reset.
| ePWMInstance | [in] ePWM instance number [0 - 31] |
| void SOC_generateFsiTxReset | ( | uint32_t | fsitxInstance | ) |
Generate FSI-TX reset.
| fsitxInstance | [in] FSI instance number [0 - 3] |
| void SOC_generateFsiRxReset | ( | uint32_t | fsirxInstance | ) |
Generate FSI-RX reset.
| fsirxInstance | [in] FSI instance number [0 - 3] |
| void SOC_generateCmpssaReset | ( | uint32_t | cmpssaInstance | ) |
Generate CMPSS-A reset.
| cmpssaInstance | [in] CMPSS-A instance number [0 - 9] |
| void SOC_generateCmpssbReset | ( | uint32_t | cmpssbInstance | ) |
Generate CMPSS-B reset.
| cmpssbInstance | [in] CMPSS-B instance number [0 - 9] |
| void SOC_generateEcapReset | ( | uint32_t | ecapInstance | ) |
Generate ECAP reset.
| ecapInstance | [in] ECAP instance number [0 - 9] |
| void SOC_generateEqepReset | ( | uint32_t | eqepInstance | ) |
Generate EQEP reset.
| eqepInstance | [in] EQEP instance number [0 - 2] |
| void SOC_generateSdfmReset | ( | uint32_t | sdfmInstance | ) |
Generate SDFM reset.
| sdfmInstance | [in] SDFM instance number [0 - 1] |
| void SOC_generateDacReset | ( | void | ) |
Generate DAC reset.
| void SOC_generateAdcReset | ( | uint32_t | adcInstance | ) |
Generate ADC reset.
| adcInstance | [in] ADC instance number [0 - 4] |
| void SOC_generateRdcReset | ( | uint32_t | rdcInstance | ) |
Generate RDC reset.
| rdcInstance |
| void Soc_enableEPWMHalt | ( | uint32_t | epwmInstance | ) |
Halt EPWM with corresponding cPU.
| epwmInstance | [in] EPWM instance number [0 - 31] |
| void Soc_disableEPWMHalt | ( | uint32_t | epwmInstance | ) |
Halt EPWM with corresponding cPU.
| epwmInstance | [in] EPWM instance number [0 - 31] |
| void Soc_enableECAPHalt | ( | uint32_t | ecapInstance | ) |
Halt ECAP with corresponding cPU.
| ecapInstance | [in] ECAP instance number [0 - 15] |
| void Soc_disableECAPHalt | ( | uint32_t | ecapInstance | ) |
Halt ECAP with corresponding cPU.
| ecapInstance | [in] ECAP instance number [0 - 15] |
| void SOC_generateOttoReset | ( | uint32_t | ottoInstance | ) |
Generate OTTO reset.
| ottoInstance | [in] OTTO instance number [0 - 3] |
| void SOC_selectIcssGpiMux | ( | uint8_t | pru_instance, |
| uint32_t | mask | ||
| ) |
Selection of ICSS GPI MUX.
| pru_instance | [in] PRU instance number [0 - 1] |
| mask | [in] Bitwise selection of ICSSM GPI source. GPI or PWMXBar select for ICSSM port 0/1. 0-GPI, 1-PWMXBAR |
| uint64_t SOC_virtToPhy | ( | void * | virtAddr | ) |
SOC Virtual (CPU) to Physical address translation function.
| virtAddr | [IN] Virtual/CPU address |
| void* SOC_phyToVirt | ( | uint64_t | phyAddr | ) |
Physical to Virtual (CPU) address translation function.
| phyAddr | [IN] Physical address |
| uint32_t SOC_getFlashDataBaseAddr | ( | void | ) |
This function gets the SOC mapped data base address of the flash.
| void SOC_sendSoftwareInterrupt | ( | uint16_t | coreId | ) |
Send SOC level software triggered address.
| coreId | [in] see CSL_CoreID |
|
inlinestatic |
API to validate UART base address.