The Ethernet PHY driver supports auto-negotiation and manual modes. The PHY driver uses an MDIO abstraction to perform register reads and writes. The MDIO abstraction can be implemented using Enet LLD's Enet Management Data I/O (MDIO) API or any other MDIO driver.
Sub Modules | |
| Generic PHY | |
| TI DP83822 PHY | |
| TI DP83826 PHY | |
| TI DP83867 PHY | |
| TI DP83869 PHY | |
| TI DP83TC812 PHY | |
| TI DP83TG720 PHY | |
| TI DP83TG721 PHY | |
| TI PHY COMMON | |
Data Structures | |
| struct | EnetPhy_Version |
| PHY version (ID). More... | |
| struct | EnetPhy_LinkCfg |
| Link speed and duplexity configuration. More... | |
| struct | EnetPhy_FsmTimeoutCfg |
| PHY State-Machine time-out values. More... | |
| struct | EnetPhy_Cfg |
| PHY configuration parameters. More... | |
| struct | EnetPhy_Mdio |
| MDIO driver. More... | |
| struct | EnetPhy_State |
| PHY driver FSM state. More... | |
| struct | EnetPhy_Obj |
| PHY driver object. More... | |
Functions | |
| void | EnetPhy_initCfg (EnetPhy_Cfg *phyCfg) |
| Initialize PHY config params. More... | |
| void | EnetPhy_setExtendedCfg (EnetPhy_Cfg *phyCfg, const void *extendedCfg, uint32_t extendedCfgSize) |
| Set PHY extended parameters. More... | |
| EnetPhy_Handle | EnetPhy_open (const EnetPhy_Cfg *phyCfg, EnetPhy_Mii mii, const EnetPhy_LinkCfg *linkCfg, uint32_t macPortCaps, EnetPhy_MdioHandle hMdio, void *mdioArgs) |
| Open the PHY driver. More... | |
| void | EnetPhy_close (EnetPhy_Handle hPhy) |
| Close the PHY driver. More... | |
| EnetPhy_LinkStatus | EnetPhy_tick (EnetPhy_Handle hPhy) |
| Run PHY state machine. More... | |
| int32_t | EnetPhy_getId (EnetPhy_Handle hPhy, EnetPhy_Version *version) |
| Get PHY id. More... | |
| bool | EnetPhy_isAlive (EnetPhy_Handle hPhy) |
| Get PHY alive status. More... | |
| bool | EnetPhy_isLinked (EnetPhy_Handle hPhy) |
| Get link status. More... | |
| int32_t | EnetPhy_getLinkCfg (EnetPhy_Handle hPhy, EnetPhy_LinkCfg *linkCfg) |
| Get link configuration. More... | |
| int32_t | EnetPhy_readReg (void *pArgs, uint32_t reg, uint16_t *val) |
| Read PHY register. More... | |
| int32_t | EnetPhy_writeReg (void *pArgs, uint32_t reg, uint16_t val) |
| Write PHY register. More... | |
| int32_t | EnetPhy_rmwReg (void *pArgs, uint32_t reg, uint16_t mask, uint16_t val) |
| Read-modify-write PHY register. More... | |
| int32_t | EnetPhy_readExtReg (void *pArgs, uint32_t reg, uint16_t *val) |
| Read PHY extended register. More... | |
| int32_t | EnetPhy_writeExtReg (void *pArgs, uint32_t reg, uint16_t val) |
| Write PHY extended register. More... | |
| int32_t | EnetPhy_rmwExtReg (EnetPhy_Handle hPhy, uint32_t reg, uint16_t mask, uint16_t val) |
| Read-modify-write PHY extended register. More... | |
| int32_t | EnetPhy_readC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t *val) |
| Read PHY register using Clause-45 frame. More... | |
| int32_t | EnetPhy_writeC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t val) |
| Write PHY register using Clause-45 frame. More... | |
| int32_t | EnetPhy_rmwC45Reg (EnetPhy_Handle hPhy, uint8_t mmd, uint32_t reg, uint16_t mask, uint16_t val) |
| Read-modify-write PHY register using Clause-45 frame. More... | |
| void | EnetPhy_printRegs (EnetPhy_Handle hPhy) |
| Print all PHY registers. More... | |
| int32_t | EnetPhy_adjPtpFreq (EnetPhy_Handle hPhy, int64_t ppb) |
| Adjust PHY PTP clock frequency. More... | |
| int32_t | EnetPhy_adjPtpPhase (EnetPhy_Handle hPhy, int64_t offset) |
| Adjust PHY PTP clock phase. More... | |
| int32_t | EnetPhy_getPtpTime (EnetPhy_Handle hPhy, uint64_t *ts64) |
| Get current PHY PTP clock time. More... | |
| int32_t | EnetPhy_setPtpTime (EnetPhy_Handle hPhy, uint64_t ts64) |
| Set PHY PTP clock time. More... | |
| int32_t | EnetPhy_getPtpTxTime (EnetPhy_Handle hPhy, uint32_t domain, uint32_t msgType, uint32_t seqId, uint64_t *ts64) |
| Get PHY PTP TX packet timestamp. More... | |
| int32_t | EnetPhy_getPtpRxTime (EnetPhy_Handle hPhy, uint32_t domain, uint32_t msgType, uint32_t seqId, uint64_t *ts64) |
| Get PHY PTP RX packet timestamp. More... | |
| int32_t | EnetPhy_waitPtpTxTime (EnetPhy_Handle hPhy, uint32_t domain, uint32_t msgType, uint32_t seqId) |
| Add PHY PTP TX packet info to a waiting TX timestamp list. More... | |
| int32_t | EnetPhy_procStatusFrame (EnetPhy_Handle hPhy, uint8_t *frame, uint32_t size, uint32_t *types) |
| Process PHY status frame. More... | |
| int32_t | EnetPhy_getStatusFrameEthHeader (EnetPhy_Handle hPhy, uint8_t *ethhdr, uint32_t size) |
| Get PHY status frame header. More... | |
| int32_t | EnetPhy_enablePtp (EnetPhy_Handle hPhy, bool on, uint32_t srcMacStatusFrameType) |
| Enable/Disable PHY PTP module. More... | |
| int32_t | EnetPhy_tickDriver (EnetPhy_Handle hPhy) |
| Provide timer tick to the driver. More... | |
| int32_t | EnetPhy_enableEventCapture (EnetPhy_Handle hPhy, uint32_t eventIdx, bool falling, bool on) |
| Enable/Disable an event capture on a PHY GPIO pin. More... | |
| int32_t | EnetPhy_enableTriggerOutput (EnetPhy_Handle hPhy, uint32_t triggerIdx, uint64_t start, uint64_t period, bool repeat) |
| Enable/Disable clock trigger on a GPIO pin. More... | |
| int32_t | EnetPhy_getEventTs (EnetPhy_Handle hPhy, uint32_t *eventIdx, uint32_t *seqId, uint64_t *ts64) |
| Get event timestamp. More... | |
Typedefs | |
| typedef EnetPhy_Mdio * | EnetPhy_MdioHandle |
| MDIO driver handle. More... | |
| typedef struct EnetPhy_Obj_s * | EnetPhy_Handle |
| PHY driver object handle. More... | |
Macros | |
| #define | ENETPHY_IS_ADDR_VALID(addr) ((addr) <= 31U) |
| Check if PHY address is valid (0 - 31). More... | |
| #define | ENETPHY_BIT(n) (1U << (n)) |
| Macro to set bit at given bit position. More... | |
| #define | ENETPHY_IS_BIT_SET(val, n) (((val) & ENETPHY_BIT(n)) != 0U) |
| Macro to check if bit at given bit position is set. More... | |
| #define | ENETPHY_ARRAYSIZE(x) (sizeof(x) / sizeof(x[0])) |
| Macro to get the size of an array. More... | |
| #define | ENETPHY_EXTENDED_CFG_SIZE_MAX (128U) |
| Max extended configuration size, arbitrarily chosen. More... | |
| #define | ENETPHY_FSM_TICK_PERIOD_MS (100U) |
| Enet PHY State Machine tick period. More... | |
| #define | ENETPHY_INVALID_PHYADDR (~0U) |
| Invalid PHY address indicator. More... | |
| #define | ENETPHY_TIMEOUT_WAIT_FOREVER (0xFFFFFFFFU) |
| State timeout value to set to disable timeout. More... | |
| #define | ENETPHY_TIMEOUT_NO_WAIT (0U) |
| State timeout value to set to expire immediately. More... | |
Ethernet PHY driver error codes | |
|
Error codes returned by the Ethernet PHY driver APIs. | |
| #define | ENETPHY_SOK (CSL_PASS) |
| Success. More... | |
| #define | ENETPHY_EFAIL (CSL_EFAIL) |
| Generic failure error condition (typically caused by hardware). More... | |
| #define | ENETPHY_EBADARGS (CSL_EBADARGS) |
| Bad arguments (i.e. NULL pointer). More... | |
| #define | ENETPHY_EINVALIDPARAMS (CSL_EINVALID_PARAMS) |
| Invalid parameters (i.e. value out-of-range). More... | |
| #define | ENETPHY_ETIMEOUT (CSL_ETIMEOUT) |
| Time out while waiting for a given condition to happen. More... | |
| #define | ENETPHY_EALLOC (CSL_EALLOC) |
| Allocation failure. More... | |
| #define | ENETPHY_EPERM (CSL_EALLOC - 4) |
| Operation not permitted. More... | |
| #define | ENETPHY_ENOTSUPPORTED (CSL_EALLOC - 5) |
| Operation not supported. More... | |
| #define | ENETPHY_EUNAVAILABLE (CSL_EALLOC - 6) |
| Operation not supported. More... | |
Ethernet PHY link capability masks | |
|
Error codes returned by the Ethernet PHY driver APIs. | |
| #define | ENETPHY_LINK_CAP_HD10 ENETPHY_BIT(1) |
| 10-Mbps, half-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_FD10 ENETPHY_BIT(2) |
| 10-Mbps, full-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_HD100 ENETPHY_BIT(3) |
| 100-Mbps, half-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_FD100 ENETPHY_BIT(4) |
| 100-Mbps, full-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_HD1000 ENETPHY_BIT(5) |
| 1-Gbps, half-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_FD1000 ENETPHY_BIT(6) |
| 1-Gbps, full-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_10 |
| 10-Mbps, full and half-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_100 |
| 100-Mbps, full and half-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_1000 |
| 1-Gbps, full and half-duplex capability mask. More... | |
| #define | ENETPHY_LINK_CAP_ALL |
| Auto-negotiation mask with all duplexity and speed values set. More... | |
| #define ENETPHY_IS_ADDR_VALID | ( | addr | ) | ((addr) <= 31U) |
Check if PHY address is valid (0 - 31).
| #define ENETPHY_BIT | ( | n | ) | (1U << (n)) |
Macro to set bit at given bit position.
| #define ENETPHY_IS_BIT_SET | ( | val, | |
| n | |||
| ) | (((val) & ENETPHY_BIT(n)) != 0U) |
Macro to check if bit at given bit position is set.
| #define ENETPHY_ARRAYSIZE | ( | x | ) | (sizeof(x) / sizeof(x[0])) |
Macro to get the size of an array.
| #define ENETPHY_SOK (CSL_PASS) |
Success.
| #define ENETPHY_EFAIL (CSL_EFAIL) |
Generic failure error condition (typically caused by hardware).
| #define ENETPHY_EBADARGS (CSL_EBADARGS) |
Bad arguments (i.e. NULL pointer).
| #define ENETPHY_EINVALIDPARAMS (CSL_EINVALID_PARAMS) |
Invalid parameters (i.e. value out-of-range).
| #define ENETPHY_ETIMEOUT (CSL_ETIMEOUT) |
Time out while waiting for a given condition to happen.
| #define ENETPHY_EALLOC (CSL_EALLOC) |
Allocation failure.
| #define ENETPHY_EPERM (CSL_EALLOC - 4) |
Operation not permitted.
| #define ENETPHY_ENOTSUPPORTED (CSL_EALLOC - 5) |
Operation not supported.
| #define ENETPHY_EUNAVAILABLE (CSL_EALLOC - 6) |
Operation not supported.
| #define ENETPHY_LINK_CAP_HD10 ENETPHY_BIT(1) |
10-Mbps, half-duplex capability mask.
| #define ENETPHY_LINK_CAP_FD10 ENETPHY_BIT(2) |
10-Mbps, full-duplex capability mask.
| #define ENETPHY_LINK_CAP_HD100 ENETPHY_BIT(3) |
100-Mbps, half-duplex capability mask.
| #define ENETPHY_LINK_CAP_FD100 ENETPHY_BIT(4) |
100-Mbps, full-duplex capability mask.
| #define ENETPHY_LINK_CAP_HD1000 ENETPHY_BIT(5) |
1-Gbps, half-duplex capability mask.
| #define ENETPHY_LINK_CAP_FD1000 ENETPHY_BIT(6) |
1-Gbps, full-duplex capability mask.
| #define ENETPHY_LINK_CAP_10 |
10-Mbps, full and half-duplex capability mask.
| #define ENETPHY_LINK_CAP_100 |
100-Mbps, full and half-duplex capability mask.
| #define ENETPHY_LINK_CAP_1000 |
1-Gbps, full and half-duplex capability mask.
| #define ENETPHY_LINK_CAP_ALL |
Auto-negotiation mask with all duplexity and speed values set.
| #define ENETPHY_EXTENDED_CFG_SIZE_MAX (128U) |
Max extended configuration size, arbitrarily chosen.
| #define ENETPHY_FSM_TICK_PERIOD_MS (100U) |
Enet PHY State Machine tick period.
| #define ENETPHY_INVALID_PHYADDR (~0U) |
Invalid PHY address indicator.
| #define ENETPHY_TIMEOUT_WAIT_FOREVER (0xFFFFFFFFU) |
State timeout value to set to disable timeout.
| #define ENETPHY_TIMEOUT_NO_WAIT (0U) |
State timeout value to set to expire immediately.
| typedef EnetPhy_Mdio* EnetPhy_MdioHandle |
MDIO driver handle.
| typedef struct EnetPhy_Obj_s* EnetPhy_Handle |
PHY driver object handle.
PHY driver opaque handle used to call any PHY related APIs.
| enum EnetPhy_Magic |
| enum EnetPhy_Mii |
| enum EnetPhy_Speed |
| enum EnetPhy_Duplexity |
| enum EnetPhy_LinkStatus |
| enum EnetPhy_FsmState |
PHY driver state-machine states.
| void EnetPhy_initCfg | ( | EnetPhy_Cfg * | phyCfg | ) |
Initialize PHY config params.
Initializes PHY driver configuration parameters.
| phyCfg | PHY configuration params |
| void EnetPhy_setExtendedCfg | ( | EnetPhy_Cfg * | phyCfg, |
| const void * | extendedCfg, | ||
| uint32_t | extendedCfgSize | ||
| ) |
Set PHY extended parameters.
Sets the PHY-specific extended parameters to the PHY config structure.
| phyCfg | Pointer to the PHY config |
| extendedCfg | Pointer to the PHY extended config |
| extendedCfgSize | Size of the PHY extended config |
| EnetPhy_Handle EnetPhy_open | ( | const EnetPhy_Cfg * | phyCfg, |
| EnetPhy_Mii | mii, | ||
| const EnetPhy_LinkCfg * | linkCfg, | ||
| uint32_t | macPortCaps, | ||
| EnetPhy_MdioHandle | hMdio, | ||
| void * | mdioArgs | ||
| ) |
Open the PHY driver.
Open the Ethernet PHY driver for the given MAC port number. The PHY driver takes PHY specific configuration parameters, the MAC port type connection and the desired link configuration (auto or manual).
| phyCfg | PHY configuration params |
| mii | PHY MII interface type |
| linkCfg | Link configuration (speed and duplexity) |
| macPortCaps | MAC port speed/duplex capabilities. It's a bit mask of EnetPhy_LinkCaps |
| hMdio | MDIO driver to be used for PHY register read/write |
| mdioArgs | Private data passed to the MDIO driver functions |
| void EnetPhy_close | ( | EnetPhy_Handle | hPhy | ) |
Close the PHY driver.
Closes the Ethernet PHY driver.
| hPhy | PHY device handle |
| EnetPhy_LinkStatus EnetPhy_tick | ( | EnetPhy_Handle | hPhy | ) |
Run PHY state machine.
Runs the PHY FSM.
| hPhy | PHY device handle |
| int32_t EnetPhy_getId | ( | EnetPhy_Handle | hPhy, |
| EnetPhy_Version * | version | ||
| ) |
Get PHY id.
Gets the device ID of a PHY, read from IDR1 and IDR2 registers.
| hPhy | PHY device handle |
| version | Pointer to PHY version. |
| bool EnetPhy_isAlive | ( | EnetPhy_Handle | hPhy | ) |
Get PHY alive status.
Gets the PHY alive status. Whether PHY is responding to read accesses.
| hPhy | PHY device handle |
| bool EnetPhy_isLinked | ( | EnetPhy_Handle | hPhy | ) |
Get link status.
Gets the link status: linked or not, based on driver's state machine. The PHY driver state machine can take a little longer to detect link up because it runs on tick period intervals and need to traverse few states to reach link up FSM state.
| hPhy | PHY device handle |
| int32_t EnetPhy_getLinkCfg | ( | EnetPhy_Handle | hPhy, |
| EnetPhy_LinkCfg * | linkCfg | ||
| ) |
Get link configuration.
Gets the link configuration, that is, the configuration that the PHY has negotiated with the link partner or the manual link configuration it was set to.
| hPhy | PHY device handle |
| linkCfg | Link configuration |
| int32_t EnetPhy_readReg | ( | void * | pArgs, |
| uint32_t | reg, | ||
| uint16_t * | val | ||
| ) |
Read PHY register.
Reads a PHY register. It's not meant for extended registers.
| pArgs | PHY device handle |
| reg | Register number |
| val | Pointer to the read value |
| int32_t EnetPhy_writeReg | ( | void * | pArgs, |
| uint32_t | reg, | ||
| uint16_t | val | ||
| ) |
Write PHY register.
Writes a PHY register. It's not meant for extended registers.
| pArgs | PHY device handle |
| reg | Register number |
| val | Value to be written |
| int32_t EnetPhy_rmwReg | ( | void * | pArgs, |
| uint32_t | reg, | ||
| uint16_t | mask, | ||
| uint16_t | val | ||
| ) |
Read-modify-write PHY register.
Read-modify-write a PHY register. It's not meant for extended registers.
| pArgs | PHY device handle |
| reg | Register number |
| mask | Bitmask to be applied on read value and value to be written |
| val | Value to be written |
| int32_t EnetPhy_readExtReg | ( | void * | pArgs, |
| uint32_t | reg, | ||
| uint16_t * | val | ||
| ) |
Read PHY extended register.
Reads a PHY extended register.
| pArgs | PHY device handle |
| reg | Register number |
| val | Pointer to the read value |
| int32_t EnetPhy_writeExtReg | ( | void * | pArgs, |
| uint32_t | reg, | ||
| uint16_t | val | ||
| ) |
Write PHY extended register.
Writes a PHY extended register.
| pArgs | PHY device handle |
| reg | Register number |
| val | Value to be written |
| int32_t EnetPhy_rmwExtReg | ( | EnetPhy_Handle | hPhy, |
| uint32_t | reg, | ||
| uint16_t | mask, | ||
| uint16_t | val | ||
| ) |
Read-modify-write PHY extended register.
Read-modify-write a PHY extended register.
| hPhy | PHY device handle |
| reg | Register number |
| mask | Bitmask to be applied on read value and value to be written |
| val | Value to be written |
| int32_t EnetPhy_readC45Reg | ( | EnetPhy_Handle | hPhy, |
| uint8_t | mmd, | ||
| uint32_t | reg, | ||
| uint16_t * | val | ||
| ) |
Read PHY register using Clause-45 frame.
Reads a PHY register using Clause-45 frame.
| hPhy | PHY device handle |
| mmd | MMD |
| reg | Register number |
| val | Pointer to the read value |
| int32_t EnetPhy_writeC45Reg | ( | EnetPhy_Handle | hPhy, |
| uint8_t | mmd, | ||
| uint32_t | reg, | ||
| uint16_t | val | ||
| ) |
Write PHY register using Clause-45 frame.
Writes a PHY register using Clause-45 frame.
| hPhy | PHY device handle |
| mmd | MMD |
| reg | Register number |
| val | Value to be written |
| int32_t EnetPhy_rmwC45Reg | ( | EnetPhy_Handle | hPhy, |
| uint8_t | mmd, | ||
| uint32_t | reg, | ||
| uint16_t | mask, | ||
| uint16_t | val | ||
| ) |
Read-modify-write PHY register using Clause-45 frame.
Read-modify-write a PHY register using Clause-45 frame.
| hPhy | PHY device handle |
| mmd | MMD |
| reg | Register number |
| mask | Bitmask to be applied on read value and value to be written |
| val | Value to be written |
| void EnetPhy_printRegs | ( | EnetPhy_Handle | hPhy | ) |
Print all PHY registers.
Prints all registers of a PHY.
| hPhy | PHY device handle |
| int32_t EnetPhy_adjPtpFreq | ( | EnetPhy_Handle | hPhy, |
| int64_t | ppb | ||
| ) |
Adjust PHY PTP clock frequency.
Adjust PHY PTP clock frequency.
| hPhy | PHY device handle |
| ppb | Part per billion |
| int32_t EnetPhy_adjPtpPhase | ( | EnetPhy_Handle | hPhy, |
| int64_t | offset | ||
| ) |
Adjust PHY PTP clock phase.
Adjust PHY PTP clock phase.
| hPhy | PHY device handle |
| offset | Offset to current clock time in nanosec unit. |
| int32_t EnetPhy_getPtpTime | ( | EnetPhy_Handle | hPhy, |
| uint64_t * | ts64 | ||
| ) |
Get current PHY PTP clock time.
Get current PHY PTP clock time.
| hPhy | PHY device handle |
| ts64 | Output current PTP clock time in nanosec unit. |
| int32_t EnetPhy_setPtpTime | ( | EnetPhy_Handle | hPhy, |
| uint64_t | ts64 | ||
| ) |
Set PHY PTP clock time.
Set PHY PTP clock time.
| hPhy | PHY device handle |
| ts64 | PTP time in nanosec unit will be set. |
| int32_t EnetPhy_getPtpTxTime | ( | EnetPhy_Handle | hPhy, |
| uint32_t | domain, | ||
| uint32_t | msgType, | ||
| uint32_t | seqId, | ||
| uint64_t * | ts64 | ||
| ) |
Get PHY PTP TX packet timestamp.
Get PHY PTP TX packet timestamp.
| hPhy | PHY device handle |
| domain | PTP domain (in the packet header) |
| msgType | PTP message type (in the packet header) |
| seqId | PTP packet sequence ID (in the packet header) |
| ts64 | Output PTP TX packet timestamp in nanosec unit. |
| int32_t EnetPhy_getPtpRxTime | ( | EnetPhy_Handle | hPhy, |
| uint32_t | domain, | ||
| uint32_t | msgType, | ||
| uint32_t | seqId, | ||
| uint64_t * | ts64 | ||
| ) |
Get PHY PTP RX packet timestamp.
Get PHY PTP RX packet timestamp.
| hPhy | PHY device handle |
| domain | PTP domain (in the packet header) |
| msgType | PTP message type (in the packet header) |
| seqId | PTP packet sequence ID (in the packet header) |
| ts64 | Output PTP RX packet timestamp in nanosec unit. |
| int32_t EnetPhy_waitPtpTxTime | ( | EnetPhy_Handle | hPhy, |
| uint32_t | domain, | ||
| uint32_t | msgType, | ||
| uint32_t | seqId | ||
| ) |
Add PHY PTP TX packet info to a waiting TX timestamp list.
Add PHY PTP TX packet info to a waiting TX timestamp list.
| hPhy | PHY device handle |
| domain | PTP domain (in the packet header) |
| msgType | PTP message type (in the packet header) |
| seqId | PTP packet sequence ID (in the packet header) |
| int32_t EnetPhy_procStatusFrame | ( | EnetPhy_Handle | hPhy, |
| uint8_t * | frame, | ||
| uint32_t | size, | ||
| uint32_t * | types | ||
| ) |
Process PHY status frame.
Process PHY status frame.
| hPhy | PHY device handle |
| frame | Ethernet PHY status frame |
| size | Frame size |
| types | Types of processed frame |
| int32_t EnetPhy_getStatusFrameEthHeader | ( | EnetPhy_Handle | hPhy, |
| uint8_t * | ethhdr, | ||
| uint32_t | size | ||
| ) |
Get PHY status frame header.
Get PHY status frame header.
| hPhy | PHY device handle |
| ethhdr | Buffer to get the ethernet header of the PHY status frame. |
| size | Buffer size (at least 14 bytes) |
| int32_t EnetPhy_enablePtp | ( | EnetPhy_Handle | hPhy, |
| bool | on, | ||
| uint32_t | srcMacStatusFrameType | ||
| ) |
Enable/Disable PHY PTP module.
Enable/Disable PHY PTP module.
| hPhy | PHY device handle |
| on | Flag indicate enable (on=true) or disable(on=false) PTP module |
| srcMacStatusFrameType | The PHY-specific src MAC of the status frame. |
| int32_t EnetPhy_tickDriver | ( | EnetPhy_Handle | hPhy | ) |
Provide timer tick to the driver.
Provide timer tick to the driver.
| hPhy | PHY device handle |
| int32_t EnetPhy_enableEventCapture | ( | EnetPhy_Handle | hPhy, |
| uint32_t | eventIdx, | ||
| bool | falling, | ||
| bool | on | ||
| ) |
Enable/Disable an event capture on a PHY GPIO pin.
Enable/Disable an event capture on a PHY GPIO pin.
| hPhy | PHY device handle |
| eventIdx | Event index |
| falling | Capture event on falling edge or rising edge if falling is false. |
| on | Enable when on is true, otherwise disable the event. |
| int32_t EnetPhy_enableTriggerOutput | ( | EnetPhy_Handle | hPhy, |
| uint32_t | triggerIdx, | ||
| uint64_t | start, | ||
| uint64_t | period, | ||
| bool | repeat | ||
| ) |
Enable/Disable clock trigger on a GPIO pin.
Enable/Disable clock trigger on a GPIO pin.
| hPhy | PHY device handle |
| triggerIdx | Trigger index |
| start | Start trigger time in nanosec unit. |
| period | Period of the clock in nanosec unit. Disable the trigger if the period is equal to 0. |
| repeat | Repeat the clock or one shot if repeat is false. |
| int32_t EnetPhy_getEventTs | ( | EnetPhy_Handle | hPhy, |
| uint32_t * | eventIdx, | ||
| uint32_t * | seqId, | ||
| uint64_t * | ts64 | ||
| ) |
Get event timestamp.
Get event timestamp
| hPhy | PHY device handle |
| eventIdx | Output event index |
| seqId | Output event sequence identifier |
| ts64 | Output event timestamp |