|
AM263Px MCU+ SDK
10.02.00
|
|
Go to the documentation of this file.
57 #include <drivers/hw_include/cslr.h>
58 #include <security_common/drivers/crypto/dthe/hw_include/cslr_aes.h>
68 #define DTHE_AES_ECB_MODE (0x00000000U)
70 #define DTHE_AES_CBC_MODE (0x00000001U)
72 #define DTHE_AES_CTR_MODE (0x00000002U)
74 #define DTHE_AES_ICM_MODE (0x00000004U)
76 #define DTHE_AES_CFB_MODE (0x00000008U)
78 #define DTHE_AES_F8_MODE (0x00000010U)
80 #define DTHE_AES_F9_MODE (0x00000020U)
82 #define DTHE_AES_XTS_MODE (0x00000040U)
84 #define DTHE_AES_CBC_MAC_MODE (0x00000080U)
86 #define DTHE_AES_CMAC_MODE (0x00000100U)
88 #define DTHE_AES_CCM_MODE (0x00000120U)
91 #define DTHE_AES_KEY_128_SIZE (0x00000001U)
93 #define DTHE_AES_KEY_192_SIZE (0x00000002U)
95 #define DTHE_AES_KEY_256_SIZE (0x00000003U)
98 #define DTHE_AES_ENCRYPT (0x016FE45DU)
100 #define DTHE_AES_DECRYPT (0xDCBA4213U)
103 #define DTHE_AES_CTR_WIDTH_16 (0x00000001U)
105 #define DTHE_AES_CTR_WIDTH_32 (0x00000002U)
107 #define DTHE_AES_CTR_WIDTH_64 (0x00000004U)
109 #define DTHE_AES_CTR_WIDTH_96 (0x00000008U)
111 #define DTHE_AES_CTR_WIDTH_128 (0x00000010U)
114 #define DTHE_AES_ONE_SHOT_SUPPORT (0x00000000U)
116 #define DTHE_AES_STREAM_INIT (0xAA11BB22U)
118 #define DTHE_AES_STREAM_UPDATE (0x33CC44DDU)
120 #define DTHE_AES_STREAM_FINISH (0xEE55FF66U)
136 typedef enum DTHE_AES_Return_e
166 typedef struct DTHE_AES_Params_t
uint32_t counterWidth
Definition: dthe_aes.h:245
AES Driver Parameters This structure has all the parameters which are need by the AES Driver to perfo...
Definition: dthe_aes.h:167
uint32_t streamState
Definition: dthe_aes.h:251
uint8_t keyLen
Length of the Key.
Definition: dthe_aes.h:199
This file contains the prototype of DTHE driver APIs.
uint32_t * ptrIV
Definition: dthe_aes.h:204
uint32_t ccmM
Definition: dthe_aes.h:282
uint32_t aadLength
Definition: dthe_aes.h:272
uint32_t algoType
Definition: dthe_aes.h:169
uint32_t streamSize
Definition: dthe_aes.h:262
uint32_t dataLenBytes
Definition: dthe_aes.h:211
uint32_t opType
Operation to be performed by the AES Driver.
Definition: dthe_aes.h:172
uint32_t * ptrPlainTextData
Definition: dthe_aes.h:235
uint32_t * ptrTag
Definition: dthe_aes.h:240
DTHE_AES_Return_t DTHE_AES_execute(DTHE_Handle handle, const DTHE_AES_Params *ptrParams)
The function is used to execute the AES Driver with the specified parameters.
DTHE_AES_Return_t DTHE_AES_close(DTHE_Handle handle)
Function to close DTHE AES Driver.
DTHE_AES_Return_t
DTHE AES Driver Error code.
Definition: dthe_aes.h:137
uint32_t ccmL
Definition: dthe_aes.h:277
uint32_t * ptrKey2
Definition: dthe_aes.h:194
uint32_t * ptrKey1
Definition: dthe_aes.h:189
void * DTHE_Handle
Handle to the DTHE driver.
Definition: dthe.h:85
uint32_t * ptrAAD
Definition: dthe_aes.h:267
uint32_t * ptrKey
Definition: dthe_aes.h:184
@ DTHE_AES_RETURN_SUCCESS
Definition: dthe_aes.h:138
uint32_t * ptrEncryptedData
Definition: dthe_aes.h:224
Bool useKEKMode
Definition: dthe_aes.h:178
@ DTHE_AES_RETURN_FAILURE
Definition: dthe_aes.h:139
DTHE_AES_Return_t DTHE_AES_open(DTHE_Handle handle)
Function to Open DTHE AES Driver.