AM263Px MCU+ SDK  10.02.00
FreeRTOS MPU usage guidelines

This section has additional useful information related to FreeRTOS MPU and its integration within MCU+ SDK.

Refer FreeRTOS - Memory Protection Unit (MPU) Support for official FreeRTOS documentation.

Using and adding FreeRTOS MPU to your project

  • You can start using FreeRTOS MPU referring to FreeRTOS MPU Task Switch Example at ${SDK_INSTALL_PATH}/examples/kernel/freertos/task_switch_mpu
  • Also refer Driver Porting Layer (DPL) demo at examples/kernel/dpl/dpl_demo for usage of DPL TaskP API to create user mode tasks.
  • Given below are some details to add FreeRTOS MPU to a project if you decide to start from scratch
  • Below paths must be added to your project include path to use FreeRTOS Kernel API with MPU support
      ${MCU_PLUS_SDK_PATH}/source/kernel/freertos/FreeRTOS-Kernel/include
      ${MCU_PLUS_SDK_PATH}/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F_MPU
      ${MCU_PLUS_SDK_PATH}/source/kernel/freertos/config/am263px/r5f_mpu
    
  • To link to FreeRTOS library, add below path to you library path
      ${MCU_PLUS_SDK_PATH}/source/kernel/freertos/lib
    
  • And link to below library for your SOC and CPU of choice
      freertos.{soc}.{cpu}-mpu.{compiler}.{profile}.lib
    
Note
Following is temporary and is expected to be removed in future releases
  • Add below define for your application build to select FreeRTOS MPU port
      MPU_FREERTOS
    

Important tips for application writers

  • For R5F with total of 16 configurable MPU regions,
    • The first 8 regions (Region 0 - Region 7) are static and can be setup via SysConfig
      • SysConfig generates DPL MpuP config and these are programmed one-time as part of startup code
    • Next region is reserved for task stack (Region 8)
      • Refer xTaskCreateRestrictedStatic API documentation description for puxStackBuffer for details on various constraints related to stack size and alignment
    • Rest of the 7 regions (Region 9 - Region 15) are task specific and can be provided while creating the task
  • Various FreeRTOS kernel APIS like create/delete tasks/semaphore/events can be used only from privileged tasks and are not available for user mode tasks
    • Refer System Call restrictions under "Changes in FreeRTOS version 10.6.0" and "Changes in FreeRTOS version 10.5.0" in FreeRTOS - Memory Protection Unit (MPU) Support - Upgrade Information for the list of APIs that are not accessible from user mode tasks
    • Hence following DPL APIs which are implemented using these restricted kernel APIs should as well be used only from a privileged task,
      • TaskP_construct
      • TaskP_constructRestricted
      • TaskP_destruct
      • SemaphoreP_constructMutex
      • SemaphoreP_constructBinary
      • SemaphoreP_constructCounting
      • SemaphoreP_destruct
      • MailboxP_create
      • MailboxP_delete
      • EventP_construct
      • EventP_destruct
      • ClockP_construct
      • TaskP_loadGet
      • TaskP_loadGetTotalCpuLoad
      • TaskP_loadUpdateAll
      • TaskP_loadResetAll
      • HeapP_alloc*
      • HeapP_free*
      • HeapP_getHeapStats*
      • HeapP_destruct
Note
HeapP_alloc, HeapP_free & HeapP_getHeapStats is temporary. This is expected to be updated in future releases such that HeapP_construct & HeapP_destruct can be used only from a privileged task, whereas HeapP_alloc, HeapP_free & HeapP_getHeapStats will be accessible even for user mode tasks.
  • RTI registers are read-only in user mode and can be modified only in privileged mode.
    • Hence various SDK APIs which are impacted due to this performs temporary switch to privileged mode when invoked from user mode tasks. This is similar to how FreeRTOS kernel system calls are implemented for user mode tasks. Following are the list of SDK APIs,
      • TimerP_setup
      • TimerP_start
      • TimerP_stop
      • TimerP_clearOverflowInt
  • Performance monitoring registers in Cortex-R5 will be accessible in user mode only if c9, User Enable Register EN bit is set. This needs to be set from privileged mode.
    • Hence SDK sets this as part of starting the scheduler before switching to the first task. This enables user mode tasks to access the PMU registers as well as use various DPL CycleCounterP APIs (APIs for Counting CPU Cycles)
  • While creating the first task for an application that uses FreeRTOS MPU, make sure to create in privileged mode so as to be able to create other tasks, semaphores, etc.
  • A privileged task is created by performing a bitwise OR of portPRIVILEGE_BIT with the task priority parameter of xTaskCreateStatic
    • Refer xTaskCreateStatic API documentation description for uxPriority parameter for more details
  • A user mode task with task specific MPU regions is created using xTaskCreateRestrictedStatic
  • Refer FreeeRTOS - Memory Protection Unit (MPU) Support - Creating Tasks for more details
  • DPL API TaskP_construct can be used to create privileged tasks whereas TaskP_constructRestricted can be used to create user mode task with task specific MPU regions
    • TaskP_constructRestricted API uses DPL MpuP structure MpuP_RegionAttrs to define the region attributes for the task specific MPU regions, similar to how the static MPU regions are configured