AM263Px MCU+ SDK  10.02.00
FOTAAgent_BufferManager.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2025 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef __FOTAAGENT_BUFFER_MANAGER_H__
34 #define __FOTAAGENT_BUFFER_MANAGER_H__
35 
36 #include <stdint.h>
37 #include "fota_agent.h"
38 
39 #ifdef __cplusplus
40 extern "C"
41 {
42 #endif
43 
44 #define FotaAgentP_BufferManager_BUFFERFULL ((int32_t)-3)
45 #define FotaAgentP_BufferManager_ADDRESS_DISCONT ((int32_t)-4)
46 #define FotaAgentP_BufferManager_ADDRESS_UNALIGNED ((int32_t)-5)
47 
60 
79 int32_t FOTAAgent_BufferManager_update(FOTAAgent_Handle *fotaAgentHandle, uint8_t newData,
80  uint32_t flashOffset);
81 
94 int32_t FOTAAgent_BufferManager_calculateFlushAddress(FOTAAgent_Handle *fotaAgentHandle, uint32_t * addr);
95 
108 
121  FOTAAgent_Handle *fotaAgentHandle, uint32_t address, uint8_t newData);
122 
123 #ifdef __cplusplus
124 }
125 #endif
126 
127 
128 #endif //__FOTAAGENT_BUFFER_MANAGER_H__
FOTAAgent_BufferManager_update
int32_t FOTAAgent_BufferManager_update(FOTAAgent_Handle *fotaAgentHandle, uint8_t newData, uint32_t flashOffset)
Update internal buffer with new data.
FOTAAgent_BufferManager_flush
int32_t FOTAAgent_BufferManager_flush(FOTAAgent_Handle *fotaAgentHandle)
Flush internal buffer to flash.
FOTAAgent_BufferManager_init
int32_t FOTAAgent_BufferManager_init(FOTAAgent_Handle *fotaAgentHandle)
Initilize buffer manager state machine.
FOTAAgent_Handle
Definition: fota_agent.h:91
FOTAAgent_BufferManager_checkAddressDiscontinuity
int32_t FOTAAgent_BufferManager_checkAddressDiscontinuity(FOTAAgent_Handle *fotaAgentHandle, uint32_t address, uint8_t newData)
Check if the new data's address is discontinuous or not.
FOTAAgent_BufferManager_calculateFlushAddress
int32_t FOTAAgent_BufferManager_calculateFlushAddress(FOTAAgent_Handle *fotaAgentHandle, uint32_t *addr)
Calculate Address at which internal buffer to be flushed at.abort.
fota_agent.h
FOTA Agent Driver API/interface file.