AM263Px MCU+ SDK  10.02.00
Optiflash XIP Benchmark with Smart Placement

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am263px-cc
Example folder examples/benchmarks/optiflash_benchmark/flash_xip_smart_placement

Introduction

This is the same application as Optiflash OCRAM Benchmark, however, target functions are kept in external flash and smart placement enabled (Smart Placement). The effect of it is seen in the execution time.

Steps to Run the Example

Building the application

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Running the application

Flash the application binary to the device, follow the steps mentioned here (see Flash a Hello World example).

Sample output

Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 133.333 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 93 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
KPI_DATA: [BOOTLOADER PROFILE] System_init : 524us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 126us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 8447us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 2744us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 22121us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 18us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 33982us
Image loading done, switching to application ...
OCMC benchmarking:: Board_init success
Filling up the buffers
master_task
master_task -- start sending
memcpy Exec Time I$ Miss I$ Acc INST ICM/sec INST/sec
0B 11014us 15315 498221 2195857 1.7 246.2
100B 11625us 15494 557616 2384970 1.6 253.4
200B 12210us 14197 579859 2584748 1.4 261.4
400B 13628us 16335 735752 2987079 1.5 270.7
700B 15389us 14986 873334 3572196 1.2 286.7
1000B 17837us 17258 1115790 4187693 1.2 289.9
1500B 22259us 13811 1278045 5179595 0.8 287.4
2250B 29759us 16555 1734787 6694864 0.7 277.8
2500B 32200us 16010 1832068 7181934 0.6 275.5
4096B 46572us 16070 2860229 10377804 0.4 275.2
All tests have passed