AM263Px MCU+ SDK  10.02.00
SDFM single channel filter sync CPU read

Introduction

A SDFM example that reads filter data from CPU

In this example, SDFM filter data is read by CPU in SDFM ISR routine. The SDFM configuration is shown below:

  • SDFM used in this example - SDFM0
  • Input control mode selected - MODE0
  • Comparator settings
    • Sinc3 filter selected
    • OSR = 32
    • HLT = 0x7FFF (Higher threshold setting)
    • LLT = 0x0000(Lower threshold setting)
  • Data filter settings
    • Single filter module enabled
    • Sinc3 filter selected
    • OSR = 128
    • Single filter is synchronized by using MFE (Main Filter enable bit)
    • Filter output represented in 16 bit format
    • In order to convert 25 bit Data filter into 16 bit format user needs to right shift by 7 bits for Sinc3 filter with OSR = 128
  • Interrupt module settings for SDFM filter
    • Single higher threshold comparator interrupt disabled
    • Single lower threshold comparator interrupt disabled
    • Single modulator failure interrupt disabled
    • Single filter will generate interrupt when a new filter data is available.

Watch Variables

  • filterResult - Output of filter 2

External Connections

  • Connect Sigma-Delta streams to SDFM0_CLK1, SDFM0_D1

AM263X-CC or AM263Px-CC or AM261x-SOM

When using with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Connect Sigma-Delta streams to HSEC Pin 99, HSEC Pin 101

If required, use PWM waveforms as SDFM data and clock

  • Connect HSEC Pin 51 to HSEC Pin 99
  • Connect HSEC Pin 49 to HSEC Pin 101

AM263X-LP

  • Connect Sigma-Delta streams to Boosterpack header J6/J8 Pin 74, J6/J8 Pin 73

If required, use PWM waveforms as data and clock

  • Connect Boosterpack header J2/J4 Pin 11 to J6/J8 Pin 73
  • Connect Boosterpack header J6/J8 Pin 59 to J6/J8 Pin 74

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/sdfm/sdfm_filter_sync_cpuread_single_channel.c/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the UART console logs for results

See Also

SDFM

Sample Output

Shown below is a sample output when the application is run,

[Cortex_R5_0] SDFM filter sync CPU read Test Started ...
All tests have passed!!