AM263Px MCU+ SDK  10.02.00
MMCSD RAW IO SD INTR LLD

Introduction

This example uses the LLD driver to demonstrates basic read write operations to the SD device in interrupt mode. The SD instance and the media connected to it are selectable via Sysconfig.

The example writes known data to a particular offset in the media and then reads it back. The read data is then compared with the written known data. When both the comparisons match, test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/mmcsd/mmcsd_raw_io_sd_intr_lld

Steps to Run the Example

See Also

MMCSD

Sample Output

[MMCSD] SD Interrupt LLD Starting...
Data Matched !!
All tests have passed!!