AM263Px MCU+ SDK  10.02.00
I2C Memory Read

Introduction

This example demonstrates writing 10 Bytes of data to I2C based EEPROM devices present in the board and then reading back the same data from the EEPROM.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/i2c/i2c_memory_read

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

[I2C] Writing data to EEPROM ... !!!
[I2C] Reading data from EEPROM ... !!!
[I2C] Data at address 0x400 : 0x0
[I2C] Data at address 0x401 : 0x1
[I2C] Data at address 0x402 : 0x2
[I2C] Data at address 0x403 : 0x3
[I2C] Data at address 0x404 : 0x4
[I2C] Data at address 0x405 : 0x5
[I2C] Data at address 0x406 : 0x6
[I2C] Data at address 0x407 : 0x7
[I2C] Data at address 0x408 : 0x8
[I2C] Data at address 0x409 : 0x9
All tests have passed!!