AM263Px MCU+ SDK  10.02.00
EQEP Frequency Calculation

Introduction

Frequency Measurement Using eQEP

This example is used to measure the frequency of an input signal using the eQEP module. ePWM1A is configured to generate this input signal with a frequency of 5KHz. eQEP unit timeout is set which will generate an interrupt evey UNIT_PERIOD microsecond for frequency measurement. The PWM signal is passed internally via input XBAR to PWMXBAR to EQEPA/B.

Signal path: GPIO45/46 -> INPUTXBAR0/1 -> PWMXBAR0/1 -> EQEPA/B

The configuration for this example is as follows

  • PWM frequency is specified as 5000Hz
  • UNIT_PERIOD is specified as 10000 us
  • Min frequency is (1/(2*10ms)) i.e 50Hz
  • Highest frequency can be (2^32)/(2*10ms)
  • Resolution of frequency measurement is 50hz
  • freq : Simulated signal frequency measured by counting the external input pulses for UNIT_PERIOD (unit timer set to 10 ms).

The example does the below:

Configures EPWM to generate a signal and EQEP to measure frequency of this generated signal (a loopback connection is done internally). The application runs for the specified time and the frequency calculation is done using the EQEP ISR. After the specified time, the application checks if the measured frequency was within range of the generated frequency.

Internal connections

  • ePWM1A to eQEP0A (EPWM_A simulates eQEP Phase A signal)
  • ePWM1B to eQEP0B (EPWM_B simulates eQEP Phase B signal)

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/eqep/eqep_freq_cal_interrupt/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the UART console logs for results

See Also

EQEP

Sample Output

Shown below is a sample output when the application is run,

EQEP Frequency Measurement Test Started ...
Please wait few seconds ...
Expected frequency = 5000 Hz, Measured frequency = 5000 Hz
EQEP Frequency Measurement Test Passed!!
All tests have passed!!