AM263Px MCU+ SDK  10.02.00
ADC SOC software

Introduction

This example uses the ADC to perform an ADC SOC conversion triggered by software.

The example does the below

  • Configures SOC0 to be triggered by software.
  • Configures ADC interrupt 1 to be generated at end of conversion of SOC0.
  • Forces the SOC0 through software and waits for completion by polling ADC interrupt 1 status.

External Connections

  • ADC0_AIN2 pin should be connected to signals to be converted.

AM263PX-CC E2 or AM263X-CC E2 or AM263X-CC E1 or AM261X-SOM E1

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Feed analog input for the following
    • ADC0_AIN2 - HSEC 15

AM263PX-LP or AM263X-LP or AM261X-LP

When using AM263x-LP, AM263Px-LP or AM261x-LP

  • Feed analog input (non-zero voltage) to boosterpack header J5/J7 Pin 66 (J5/7 pin 63 in case of AM261x-LP).

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc, am263px-lp
Example folder examples/drivers/adc/adc_soc_software/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the ADC conversion results in UART console logs

See Also

ADC

Sample Output

Shown below is a sample output when the application is run,

ADC Software Triggered Conversion Test Started ...
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Result register value : 4095
ADC Software Triggered Conversion Test Passed!!
All tests have passed!!