AM263Px MCU+ SDK  10.02.00
MDIO

MDIO driver provides an interface to the MDIO management interface module which implements the 802.3 serial management interface to interrogate and control the Ethernet PHYs on the board.

Features Supported

  • Initialize MDIO clock
  • Ethernet PHY register access (IEEE defined registers and extended registers)
  • Read the link status of Ethernet PHY
  • Enable link change Interrupt

Features NOT Supported

NA

Example Usage

Include the below file to access the APIs

#include <drivers/mdio.h>

Initializing MDIO clock

status = MDIO_initClock(mdioBaseAddress);

Reading PHY link status for a PHY connected to MDIO

status = MDIO_phyLinkStatus(mdioBaseAddress, phyAddress);

Reading/writing a PHY register using MDIO

uint16_t phyRegVal;
/* Read a PHY register */
status = MDIO_phyRegRead(mdioBaseAddress, NULL, phyAddress, 0, &phyRegVal);
/* Write a PHY register */
status = MDIO_phyRegWrite(mdioBaseAddress, NULL, phyAddress, 0, phyRegVal);

API

APIs for MDIO

MDIO_phyLinkStatus
int32_t MDIO_phyLinkStatus(uint32_t baseAddr, uint32_t phyAddr)
This API reads the link status of all PHY connected to this MDIO. The bit corresponding to the PHY ad...
MDIO_phyRegRead
int32_t MDIO_phyRegRead(uint32_t baseAddr, void *pUserGroup, uint32_t phyAddr, uint32_t regNum, uint16_t *pData)
This API reads an IEEE defined PHY register using MDIO. It should be called only after successful exe...
MDIO_initClock
int32_t MDIO_initClock(uint32_t baseAddr)
This function initializes the MDIO clock.
MDIO_phyRegWrite
int32_t MDIO_phyRegWrite(uint32_t baseAddr, void *pUserGroup, uint32_t phyAddr, uint32_t regNum, uint16_t wrVal)
This API writes an IEEE defined PHY register using MDIO. It should be called only after successful ex...
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
mdio.h
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:177