AM263Px INDUSTRIAL COMMUNICATIONS SDK  10.02.00
tiescbsp.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef TIESC_BSP_H_
34 #define TIESC_BSP_H_
35 
92 /* ========================================================================== */
93 /* Include Files */
94 /* ========================================================================== */
95 
96 #ifndef DISABLE_UART_PRINT
97 #include <stdio.h>
98 #endif
99 
100 #include <industrial_comms/ethercat_slave/icss_fwhal/tiesc_pruss_intc_mapping.h>
101 #include <drivers/pruicss.h>
102 #include <industrial_comms/ethercat_slave/icss_fwhal/tiesc_def.h>
103 
104 #ifdef __cplusplus
105 extern "C" {
106 #endif
107 
108 /* ========================================================================== */
109 /* Macros & Typedefs */
110 /* ========================================================================== */
111 
112 
117 #define TIESC_MAX_FRAME_SIZE (0x7CF)
118 
119 /*Single datagram accessing contiguous multiple FMMU mapped areas in a single slave for process data
120 is supported now by TI ESC firmware.
121 Process path latency in TI ESC is high when this support is active
122 For specific use cases (4SM with 3 FMMUs or multiple FMMUs (in a given ESC) are not accessed in a single datagram)
123 process path latency improvement can be achieved by disabling below define */
124 #define ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM 0
125 
126 #define MAX_SYNC_MAN 8
127 #define SIZEOF_SM_REGISTER 8
128 
129 #define TIESC_EEPROM_SIZE 0x800
130 
131 #define MAILBOX_WRITE 0
132 #define MAILBOX_READ 1
133 #define PROCESS_DATA_OUT 2
134 #define PROCESS_DATA_IN 3
135 
136 #define MBX_WRITE_EVENT ((uint16_t) 0x0100)
137 #define MBX_READ_EVENT ((uint16_t) 0x0200)
138 
139 //Below constants are not defined in esc.h
140 #define ESC_ADDR_REV_TYPE 0x000
141 #define ESC_ADDR_BUILD 0x002
142 
143 #define ESC_ADDR_CONFIG_STATION_ALIAS 0x012
144 #define ESC_ADDR_DLSTATUS 0x110
145 #define ESC_ADDR_ALCONTROL 0x120
146 #define ESC_ADDR_ALSTATUS 0x130
147 #define ESC_ADDR_PDI_CONTROL 0x140
148 #define ESC_PDI_CONTROL_ELD_ALL_PORTS_MASK (1 << 1)
149 #define ESC_ADDR_PDI_CONFIG 0x150
150 #define ESC_ADDR_AL_EVENT_MASK 0x204
151 #define ESC_ADDR_AL_EVENT_REQ 0x220
152 #define ESC_ADDR_SM_WD_STATUS 0x440
153 #define ESC_ADDR_EEPROM_CTRL 0x502
154 #define ESC_ADDR_MI_ECAT_ACCESS 0x516
155 #define ESC_ADDR_MI_PDI_ACCESS 0x517
156 
157 #define ESC_EEPROM_CMD_MASK 0x0700 //Description (0x502.8:10): Command bit mask
158 #define ESC_EEPROM_CMD_READ_MASK 0x0100 //Description (0x502.8): Currently executed read command
159 #define ESC_EEPROM_CMD_WRITE_MASK 0x0200 //Description (0x502.9): Initialize Write Command
160 #define ESC_EEPROM_CMD_RELOAD_MASK 0x0400 //Description (0x502.10): Trigger EEPROM reload
161 #define ESC_EEPROM_ERROR_MASK 0x7800 //Description : Mask all EEPROM error bits; Checksum error (0x0502.11); EEPROM not loaded (0x0502.12); Missing EEPROM Acknowledge (0x0502.13); Write Error (0x0502.14)
162 #define ESC_EEPROM_ERROR_CRC 0x0800 //Description (0x502.11): EEPROM CRC Error
163 #define ESC_EEPROM_ERROR_CMD_ACK 0x2000 //Description (0x502.13): EEPROM Busy
164 #define ESC_EEPROM_BUSY_MASK 0x8000 //Description (0x502.15): EEPROM Busy
165 
166 #define ESC_ADDR_SYNCMAN 0x800
167 
168 #define ESC_ADDR_SM1_STATUS 0x80D
169 #define SM_STATUS_MBX_FULL 0x08
170 
171 #define ESC_ADDR_SM0_STATUS 0x805
172 #define ESC_ADDR_SM0_ACTIVATE 0x806
173 #define ESC_ADDR_SM1_ACTIVATE 0x806+8
174 #define ESC_ADDR_SM2_ACTIVATE 0x806+8*2
175 #define ESC_ADDR_SM3_ACTIVATE 0x806+8*3
176 #define ESC_ADDR_SM4_ACTIVATE 0x806+8*4
177 #define ESC_ADDR_SM5_ACTIVATE 0x806+8*5
178 #define ESC_ADDR_SM6_ACTIVATE 0x806+8*6
179 #define ESC_ADDR_SM7_ACTIVATE 0x806+8*7
180 #define ESC_ADDR_SM0_PDI_CONTROL 0x807
181 #define ESC_ADDR_SM1_PDI_CONTROL 0x807+8
182 #define ESC_ADDR_SM2_PDI_CONTROL 0x807+8*2
183 #define ESC_ADDR_SM3_PDI_CONTROL 0x807+8*3
184 #define ESC_ADDR_SM4_PDI_CONTROL 0x807+8*4
185 #define ESC_ADDR_SM5_PDI_CONTROL 0x807+8*5
186 #define ESC_ADDR_SM6_PDI_CONTROL 0x807+8*6
187 #define ESC_ADDR_SM7_PDI_CONTROL 0x807+8*7
188 
189 #define SM_PDI_CONTROL_SM_DISABLE 1
190 
191 #define ESC_ADDR_SYSTIME 0x910
192 #define ESC_ADDR_SYSTIME_HIGH 0x914
193 #define ESC_ADDR_SYSTIME_OFFSET 0x920
194 #define ESC_ADDR_SYSTIME_DELAY 0x928
195 #define ESC_ADDR_SPEEDCOUNTER_START 0x930
196 #define ESC_ADDR_TIMEDIFF_FILTDEPTH 0x934
197 #define ESC_ADDR_SPEEDDIFF_FILTDEPTH 0x935
198 #define ESC_ADDR_SYNC_PULSE_LENGTH 0x982
199 #define ESC_ADDR_SYNC_STATUS 0x98E
200 #define ESC_ADDR_LATCH0_CONTROL 0x9A8
201 #define ESC_ADDR_LATCH1_CONTROL 0x9A9
202 #define ESC_ADDR_LATCH0_POS_EDGE 0x9B0
203 #define ESC_ADDR_LATCH0_NEG_EDGE 0x9B8
204 #define ESC_ADDR_LATCH1_POS_EDGE 0x9C0
205 #define ESC_ADDR_LATCH1_NEG_EDGE 0x9C8
206 #define ESC_ADDR_TI_PORT0_ACTIVITY 0xE00
207 #define ESC_ADDR_TI_PORT1_ACTIVITY 0xE04
208 #define ESC_ADDR_TI_PORT0_PHYADDR 0xE08
209 #define ESC_ADDR_TI_PORT1_PHYADDR 0xE09
210 #define ESC_ADDR_TI_PDI_ISR_PINSEL 0xE0A
211 #define ESC_ADDR_TI_PHY_LINK_POLARITY 0XE0C
212 #define ESC_ADDR_TI_PROCESS_PATH_TX_START_DELAY 0xE10
213 #define ESC_ADDR_TI_AUTOFORWARD_PATH_TX_START_DELAY 0xE12
214 #define ESC_ADDR_TI_ESC_RESET 0xE14
215 #define ESC_ADDR_TI_EDMA_LATENCY_ENHANCEMENT 0xE24
216 #define ESC_ADDR_TI_PHY_RX_ER_REG 0xE28
217 #define ESC_ADDR_TI_PRU_CLK_FREQUENCY 0xE34
218 #define ESC_ADDR_TI_MDIO_MANUAL_MODE 0xE35
219 #define ESC_ADDR_TI_ENHANCED_LINK_DETECT 0xE36
220 #define ESC_ADDR_TI_IEP_CLK_FREQUENCY 0xED1
221 #define TI_ESC_RST_CMD_U 0x545352
222 #define TI_ESC_RST_CMD_L 0x747372
223 
224 #define ESC_ADDR_MEMORY 0x1000
225 
226 #define CMD_DL_USER_CLEAR_AL_EVENT_HIGH 0x0
227 #define CMD_DL_USER_GET_BUFFER_READ_ADDR 0x1
228 #define CMD_DL_USER_GET_BUFFER_WRITE_ADDR 0x2
229 #define CMD_DL_USER_SET_BUFFER_WRITE_DONE 0x3
230 
234 #define CMD_DL_USER_ACK_MBX_READ 0x4
235 
239 #define CMD_DL_USER_ACK_MBX_WRITE 0x5
240 
244 #define CMD_DL_USER_EEPROM_CMD_ACK 0x6
245 
249 #define CMD_DL_USER_READ_SYNC_STATUS 0x7
250 #define SYNC0 0
251 #define SYNC1 1
252 
256 #define CMD_DL_USER_READ_AL_CONTROL 0x8
257 
261 #define CMD_DL_USER_WRITE_AL_STATUS 0x9
262 
266 #define CMD_DL_USER_READ_PD_WD_STATUS 0xA
267 
271 #define CMD_DL_USER_READ_SM_ACTIVATE 0xB
272 
276 #define CMD_DL_USER_WRITE_SM_PDI_CTRL 0xC
277 
281 #define CMD_DL_USER_READ_LATCH_TIME 0xD
282 #define LATCH0_POS_EDGE 0
283 #define LATCH0_NEG_EDGE 1
284 #define LATCH1_POS_EDGE 2
285 #define LATCH1_NEG_EDGE 3
286 
291 #define CMD_DL_USER_READ_SYS_TIME 0xE
292 
296 #define CMD_DL_USER_CLEAR_AL_EVENT_LOW 0xF
297 #ifdef SYSTEM_TIME_PDI_CONTROLLED
298 
302 #define CMD_DL_USER_SYSTIME_PDI_CONTROL 0x10
303 #define WRITE_SYSTIME 0
304 #define WRITE_SYSTIME_OFFSET 1
305 #define WRITE_FILTER_CONFIG 2
306 #endif
307 
308 #define SWAPWORD
309 #define SWAPDWORD
310 
311 #define ICSS_MDIO_USRPHYSEL_LINKINT_ENABLE 0x40
312 #define ICSS_MDIO_USRPHYSEL_LINKSTAT_MLINK 0x80
313 
314 #define TIESC_PERM_RW 0x0
315 #define TIESC_PERM_WRITE_ONLY 0x1
316 #define TIESC_PERM_READ_ONLY 0x2
317 
318 #define TIESC_PERM_WRITE TIESC_PERM_WRITE_ONLY
319 #define TIESC_PERM_READ TIESC_PERM_READ_ONLY
320 
321 #define PDI_PERM_RW 0x0
322 #define PDI_PERM_READ_ONLY 0x1
323 
324 #define PDI_PERM_WRITE PDI_PERM_RW
325 #define PDI_PERM_READ PDI_PERM_READ_ONLY
326 
327 #define TIESC_MDIO_CLKDIV 79 //For 2.5MHz MDIO clock: 200/(TIESC_MDIO_CLKDIV+1)
328 
329 /* For EtherCAT, Fast link detection using MLINK mode is required to support complete functionality */
330 #define TIESC_MDIO_RX_LINK_DISABLE 0 //Slow MDIO state m/c based link detection
331 #define TIESC_MDIO_RX_LINK_ENABLE 1 //Fast link detect using RXLINK forward from PHY to MDIO MLINK
332 #define TIESC_LINK_POL_ACTIVE_LOW 1
333 #define TIESC_LINK_POL_ACTIVE_HIGH 0
334 
339 #define PDI_WD_TRIGGER_RX_SOF (0 << 4)
340 
345 #define PDI_WD_TRIGGER_LATCH_IN (1 << 4)
346 
351 #define PDI_WD_TRIGGER_SYNC0_OUT (2 << 4)
352 
357 #define PDI_WD_TRIGGER_SYNC1_OUT (3 << 4)
358 
359 #if ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM
360 /*
361 * 0x98 corresponds to MII port - MII port delay of 760ns
362 * 0x48 corresponds to MII port - MII port delay of 360ns
363 * 0x38 corresponds to MII port - MII port delay of 280ns
364 */
365 
366 #define TIESC_PROCESS_PATH_TX_DELAY_200_MHZ_CLOCK 0x98
367 #else
368 #define TIESC_PROCESS_PATH_TX_DELAY_200_MHZ_CLOCK 0x48
369 #endif
370 #define TIESC_AUTOFORWARD_PATH_TX_DELAY_200_MHZ_CLOCK 0x38
371 
372 #if ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM
373 /*
374 * 0xA0 corresponds to MII port - MII port delay of 800ns
375 * 0x50 corresponds to MII port - MII port delay of 400ns
376 * 0x30 corresponds to MII port - MII port delay of 240ns
377 */
378 #define TIESC_PROCESS_PATH_TX_DELAY_333_MHZ_CLOCK 0xA0
379 #else
380 #define TIESC_PROCESS_PATH_TX_DELAY_333_MHZ_CLOCK 0x50
381 #endif
382 #define TIESC_AUTOFORWARD_PATH_TX_DELAY_333_MHZ_CLOCK 0x30
383 
384 #define PDI_ISR_EDIO_NUM 7 //GPMC_CSN(2) -> pr1_edio_data_out7 for ICEv2.J4.Pin21
385 
386 /* PDI side register protection using register permission table (4KB) in memory - disable if you care for performance and memory foot print */
387 /* #define ENABLE_PDI_REG_PERMISSIONS */
388 
389 /* Use ESC system time instead of SYS/BIOS Timestamp_get32 for timing info */
390 #define USE_ECAT_TIMER
391 
392 
393 /* Uncomment following to enable DC feature of system time compensation via PDI interface instead of ECAT interface
394  for synchronizing two independent EtherCAT networks */
395 //#define SYSTEM_TIME_PDI_CONTROLLED
396 /*Comment to following to enable PDI ISR and SYNC ISR in HWI context */
397 #define ENABLE_PDI_TASK
398 #define ENABLE_SYNC_TASK
399 
406 /* #define SUPPORT_CMDACK_POLL_MODE */
407 
408 #if defined (__aarch64__)
409 #define ASSERT_DMB() __asm__(" dmb ISH")
410 #define ASSERT_DSB() __asm__(" dsb ISH")
411 #else
412 #define ASSERT_DMB() __asm__ __volatile__ (" dmb" "\n\t": : : "memory")
413 #define ASSERT_DSB() __asm__ __volatile__ (" dsb" "\n\t": : : "memory")
414 #endif
415 
416 #ifdef USE_ECAT_TIMER
417 #define ECAT_TIMER_INC_P_MS 1000000
418 #else
419 #define ECAT_TIMER_INC_P_MS ecat_timer_inc_p_ms /* ARM frequency: Will be detected during bsp_init*/
420 extern volatile uint32_t ecat_timer_inc_p_ms;
421 #endif
422 
423 #define ESC_SYSTEMTIME_OFFSET_OFFSET 0x0920
424 #define ESC_SPEED_COUNTER_START_OFFSET 0x0930
425 #define ESC_DC_START_TIME_CYCLIC_OFFSET 0x0990
426 
427 #define DRIFTCTRL_TASK_SYNC_ZERO_CROSS_ADJUST 0xE0 //PRU_DMEM0
428 
433 #define LOCK_PD_BUF_AVAILABLE_FOR_HOST 0
434 
438 #define LOCK_PD_BUF_HOST_ACCESS_START 1
439 
443 #define LOCK_PD_BUF_HOST_ACCESS_FINISH 2
444 
451 #define LOCK_PD_BUF_CHECK_AVAILABILITY_RETRY_COUNT (10U)
452 
457 #define TIESC_PRUICSS_CLOCK_FREQUENCY_200_MHZ (0)
458 
463 #define TIESC_PRUICSS_CLOCK_FREQUENCY_333_MHZ (1)
464 
469 #define TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_200_MHZ (0)
470 
475 #define TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_250_MHZ (1)
476 
481 #define TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_333_MHZ (2)
482 
487 #define TIESC_MDIO_HW_MODE (0)
488 
493 #define TIESC_MDIO_MANUAL_MODE_FW (1)
494 
495 typedef int32_t (*bsp_eeprom_read_t)(uint8_t *buf, uint32_t len);
496 typedef int32_t (*bsp_eeprom_write_t)(uint8_t *buf, uint32_t len);
497 typedef void (*bsp_init_spinlock_t)(void);
498 typedef uint32_t (*bsp_hwspinlock_lock_t)(int num);
499 typedef void (*bsp_hwspinlock_unlock_t)(int num);
500 typedef void (*bsp_ethphy_init_t)(PRUICSS_Handle pruIcssHandle, uint8_t phy0addr, uint8_t phy1addr, uint8_t enhancedlink_enable);
501 typedef int8_t (*bsp_get_phy_address_t)(uint8_t instance, uint8_t portNumber);
502 typedef void (*bsp_ethercat_stack_isr_function)(void);
503 
504 /* ========================================================================== */
505 /* Structure Declarations */
506 /* ========================================================================== */
507 
511 typedef struct bsp_params_s
512 {
513  PRUICSS_Handle pruicss_handle;
535  uint32_t link0_polarity;
537  uint32_t link1_polarity;
539  uint32_t phy0_address;
541  uint32_t phy1_address;
543  const unsigned char *default_tiesc_eeprom;
554  uint16_t phy_rx_err_reg;
562  uint8_t pruicssClkFreq;
566  uint8_t mdioManualMode;
570 } bsp_params;
571 
575 typedef struct
576 {
577  uint8_t sm_buf_index;
578  uint8_t lock_state;
579  uint16_t addr;
581 
586 typedef struct
587 {
588  uint8_t reserved1[0x90];
589  uint32_t system_time_low;
590  uint32_t system_time_high;
592  uint8_t reserved2[7];
593  uint16_t cmdlow;
594  uint16_t cmdlow_ack;
595  uint16_t param1low;
596  uint16_t param2low;
597  uint16_t resp1low;
598  uint16_t resp2low;
599 #ifndef SYSTEM_TIME_PDI_CONTROLLED
600  uint8_t reserved3[212];
601 #else
602  uint8_t reserved3[24];
603  uint32_t systime_offset_low;
604  uint32_t systime_offset_high;
605  uint8_t reserved4[180];
606 #endif
607  t_sm_processdata sm_processdata[6];
609 
613 typedef struct
614 {
615  uint8_t reserved[1024];
616  uint8_t reg_properties[4096];
618 
619 typedef struct
620 {
622  uint16_t length;
624 
628 typedef struct
629 {
630  uint16_t clkdiv;
631  uint8_t addr0;
632  uint8_t addr1;
633  uint8_t link0pol; /* LINK_MII signal polarity of PHY hooked to PRU-ICSS MII0. 1: Active lLow 0: Active High */
634  uint8_t link1pol; /* LINK_MII signal polarity of PHY hooked to PRU-ICSS MII1. 1: Active lLow 0: Active High */
636 } t_mdio_params;
637 
638 /* ========================================================================== */
639 /* Function Declarations */
640 /* ========================================================================== */
641 
651 void bsp_params_init(bsp_params *init_params);
652 
668 extern int32_t bsp_init(bsp_params *init_params);
669 
696 extern void bsp_esc_reg_perm_init(PRUICSS_Handle
697  pruIcssHandle); //Internal API - invoked by bsp_init
698 
706 extern void bsp_start_esc_isr(PRUICSS_Handle pruIcssHandle);
707 
718 extern void bsp_exit(PRUICSS_Handle pruIcssHandle);
719 
734 extern void bsp_set_pdi_wd_trigger_mode(PRUICSS_Handle pruIcssHandle,
735  uint32_t mode);
777 extern void bsp_send_command_to_firmware(PRUICSS_Handle pruIcssHandle,
778  uint32_t command, uint16_t param1, uint16_t param2);
793 extern void bsp_eeprom_emulation_init(void);
794 
804 extern int32_t bsp_eeprom_load_esc_registers(PRUICSS_Handle pruIcssHandle,
805  int32_t reload_flag);
806 
815 extern int32_t bsp_eeprom_emulation_reload(PRUICSS_Handle pruIcssHandle);
816 
823 extern void bsp_eeprom_emulation_command_ack(PRUICSS_Handle pruIcssHandle);
824 
830 extern void bsp_eeprom_emulation_flush(void);
831 
837 extern void bsp_eeprom_emulation_exit(void);
838 
845 extern uint8_t *bsp_get_eeprom_cache_base(void);
846 
852 
860 
868 extern void bsp_set_eeprom_update_status(uint8_t status);
869 
877 extern uint8_t bsp_get_eeprom_update_status(void);
878 
897 extern void bsp_set_sm_properties(PRUICSS_Handle pruIcssHandle, uint8_t sm,
898  uint16_t address, uint16_t len);
910 
911 extern int16_t bsp_get_sm_index(uint16_t address, uint16_t len);
927 extern uint8_t bsp_pdi_sm_config_ongoing(PRUICSS_Handle pruIcssHandle);
940 extern void bsp_pdi_mbx_read_start(PRUICSS_Handle pruIcssHandle);
941 
947 extern void bsp_pdi_mbx_read_complete(PRUICSS_Handle pruIcssHandle);
948 
955 extern void bsp_pdi_mbx_write_start(PRUICSS_Handle pruIcssHandle);
956 
963 extern void bsp_pdi_mbx_write_complete(PRUICSS_Handle pruIcssHandle);
964 
984 extern uint16_t bsp_get_process_data_address(PRUICSS_Handle pruIcssHandle,
985  uint16_t address, uint16_t len, int16_t *p_sm_index);
986 
998 extern void bsp_process_data_access_complete(PRUICSS_Handle pruIcssHandle,
999  uint16_t address, uint16_t len, int16_t sm_index);
1000 
1017 extern uint8_t bsp_read_byte(PRUICSS_Handle pruIcssHandle, uint16_t address);
1018 
1029 extern uint16_t bsp_read_word(PRUICSS_Handle pruIcssHandle, uint16_t address);
1030 
1041 extern uint32_t bsp_read_dword(PRUICSS_Handle pruIcssHandle, uint16_t address);
1042 
1052 extern void bsp_read(PRUICSS_Handle pruIcssHandle, uint8_t *pdata,
1053  uint16_t address,
1054  uint16_t len);
1055 
1065 extern uint8_t bsp_read_byte_isr(PRUICSS_Handle pruIcssHandle, uint16_t address);
1066 
1076 extern uint16_t bsp_read_word_isr(PRUICSS_Handle pruIcssHandle,
1077  uint16_t address);
1078 
1088 extern uint32_t bsp_read_dword_isr(PRUICSS_Handle pruIcssHandle,
1089  uint16_t address);
1090 
1107 extern void bsp_pdi_post_read_indication(PRUICSS_Handle pruIcssHandle,
1108  uint16_t address, uint16_t length);
1123 extern void bsp_pdi_write_indication(PRUICSS_Handle pruIcssHandle,
1124  uint16_t address, uint16_t length,
1125  uint16_t value);
1134 extern void bsp_write_byte(PRUICSS_Handle pruIcssHandle, uint8_t val,
1135  uint16_t address);
1136 
1145 extern void bsp_write_word(PRUICSS_Handle pruIcssHandle, uint16_t val,
1146  uint16_t address);
1147 
1156 extern void bsp_write_dword(PRUICSS_Handle pruIcssHandle, uint32_t val,
1157  uint16_t address);
1158 
1168 extern void bsp_write(PRUICSS_Handle pruIcssHandle, uint8_t *pdata,
1169  uint16_t address, uint16_t len);
1170 
1179 extern uint32_t bsp_pruss_mdioreg_read(PRUICSS_Handle pruIcssHandle,
1180  uint32_t regoffset);
1181 
1190 extern void bsp_pruss_mdioreg_write(PRUICSS_Handle pruIcssHandle, uint32_t val,
1191  uint32_t regoffset);
1192 
1201 extern uint32_t bsp_pruss_iepreg_read(PRUICSS_Handle pruIcssHandle,
1202  uint32_t regoffset);
1203 
1212 extern void bsp_pruss_iepreg_write(PRUICSS_Handle pruIcssHandle, uint32_t val,
1213  uint32_t regoffset);
1214 
1222 extern void bsp_pruss_cmd_intfc_write_word(uint16_t val, volatile uint16_t *ptr);
1223 
1231 extern uint16_t bsp_pruss_cmd_intfc_read_word(volatile uint16_t *ptr);
1232 
1242 extern uint8_t bsp_get_pdi_access_perm(uint16_t address, uint8_t access);
1243 
1253 extern uint8_t bsp_pdi_access_perm_word(uint16_t address, uint8_t access);
1254 
1264 extern uint8_t bsp_pdi_access_perm_dword(uint16_t address, uint8_t access);
1265 
1276 extern uint8_t bsp_pdi_access_perm_array(uint16_t address, uint8_t access,
1277  uint16_t size);
1278 
1286 extern void bsp_set_pdi_perm_read_only(uint16_t *perm_array, uint16_t address);
1287 
1295 extern void bsp_set_pdi_perm_read_write(uint16_t *perm_array, uint16_t address);
1296 
1307 extern uint8_t bsp_is_pdi_perm_read_only(uint16_t *perm_array, uint16_t address);
1308 
1316 
1324 
1342 extern int16_t bsp_pruss_mdio_init(PRUICSS_Handle pruIcssHandle,
1343  t_mdio_params *pmdio_params);
1344 
1355 extern int16_t bsp_pruss_mdio_phy_read(PRUICSS_Handle pruIcssHandle,
1356  uint8_t phyaddr, uint8_t regoffset, uint16_t *regval);
1357 
1368 extern int16_t bsp_pruss_mdio_phy_write(PRUICSS_Handle pruIcssHandle,
1369  uint8_t phyaddr, uint8_t regoffset, uint16_t regval);
1370 
1381 extern uint32_t bsp_pruss_mdio_phy_link_state(PRUICSS_Handle pruIcssHandle,
1382  uint8_t phyaddr);
1395 extern void bsp_set_digio_sw_dataout_enable(PRUICSS_Handle pruIcssHandle);
1396 
1403 extern void bsp_set_digio_out(PRUICSS_Handle pruIcssHandle, uint8_t num);
1404 
1411 extern void bsp_clear_digio_out(PRUICSS_Handle pruIcssHandle, uint8_t num);
1412 
1422 extern void bsp_hwspinlock_init(void);
1423 
1430 extern uint32_t bsp_hwspinlock_lock(int num);
1431 
1437 extern void bsp_hwspinlock_unlock(int num);
1438 
1445 #ifdef SYSTEM_TIME_PDI_CONTROLLED
1446 
1453 extern void bsp_pdi_latch0_control(PRUICSS_Handle pruIcssHandle, uint8_t val);
1454 
1462 extern void bsp_pdi_latch1_control(PRUICSS_Handle pruIcssHandle, uint8_t val);
1463 
1470 extern void bsp_pdi_write_system_time(PRUICSS_Handle pruIcssHandle,
1471  uint32_t systime);
1478 extern void bsp_pdi_write_system_timeoffset(PRUICSS_Handle pruIcssHandle,
1479  unsigned long long systime);
1486 extern void bsp_pdi_write_systime_delay(PRUICSS_Handle pruIcssHandle,
1487  uint32_t systime);
1496 extern void bsp_pdi_write_filterconfig(PRUICSS_Handle pruIcssHandle,
1497  uint16_t speedcount_start,
1498  uint8_t speedcount_filtdepth, uint8_t systime_filtdepth);
1499 #endif
1500 
1512 extern uint32_t bsp_get_timer_register(void);
1513 
1518 extern void bsp_clear_timer_register(void);
1525 extern void bsp_get_local_sys_time(uint32_t *systime_low,
1526  uint32_t *systime_high);
1527 
1535 extern void bsp_get_latch0_posedge_time(PRUICSS_Handle pruIcssHandle,
1536  uint32_t *systime_low, uint32_t *systime_high);
1537 
1545 extern void bsp_get_latch0_negedge_time(PRUICSS_Handle pruIcssHandle,
1546  uint32_t *systime_low, uint32_t *systime_high);
1547 
1555 extern void bsp_get_latch1_posedge_time(PRUICSS_Handle pruIcssHandle,
1556  uint32_t *systime_low, uint32_t *systime_high);
1557 
1565 extern void bsp_get_latch1_negedge_time(PRUICSS_Handle pruIcssHandle,
1566  uint32_t *systime_low, uint32_t *systime_high);
1567 
1579 extern void bsp_global_mutex_lock(void);
1580 
1585 extern void bsp_global_mutex_unlock(void);
1595 void Sync0Isr(void *args);
1599 void Sync1Isr(void *args);
1603 void EcatIsr(void *args);
1604 
1605 #ifndef SUPPORT_CMDACK_POLL_MODE
1606 
1609 void EscCmdLowAckIsr(void *args);
1610 #endif
1611 
1628 extern void bsp_set_pru_firmware(uint32_t *frameProc, uint32_t frameProcLen,
1629  uint32_t *hostProc, uint32_t hostProcLen);
1636 #ifdef __cplusplus
1637 }
1638 #endif
1639 
1640 #endif/*TIESC_BSP_H_ */
bsp_set_eeprom_update_status
void bsp_set_eeprom_update_status(uint8_t status)
Indicate to FWHAL whether EEPROM is written for flushing to non-volatile storage. Typically called on...
bsp_params::phy1_address
uint32_t phy1_address
Definition: tiescbsp.h:541
t_sm_processdata::sm_buf_index
uint8_t sm_buf_index
Definition: tiescbsp.h:577
bsp_get_pdi_read_access_fail_cnt
uint32_t bsp_get_pdi_read_access_fail_cnt()
Returns the count of PDI read access failures.
bsp_hwspinlock_lock
uint32_t bsp_hwspinlock_lock(int num)
Acquire selected spinlock instance.
t_host_interface::resp2low
uint16_t resp2low
Definition: tiescbsp.h:598
bsp_pdi_post_read_indication
void bsp_pdi_post_read_indication(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t length)
Invoked after reading a register or mailbox buffer from PDI side .
bsp_params::phy_rx_err_reg
uint16_t phy_rx_err_reg
Definition: tiescbsp.h:554
EscCmdLowAckIsr
void EscCmdLowAckIsr(void *args)
ESC CMD Low ACK IRQ Handler.
bsp_eeprom_emulation_exit
void bsp_eeprom_emulation_exit(void)
Call EEPROM flush on exit.
bsp_get_latch0_posedge_time
void bsp_get_latch0_posedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch0 posedge timestamp for application use(nanosec resolution)
bsp_pdi_mbx_write_start
void bsp_pdi_mbx_write_start(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side write to read mailbox has started.
bsp_hwspinlock_lock_t
uint32_t(* bsp_hwspinlock_lock_t)(int num)
Definition: tiescbsp.h:498
bsp_global_mutex_lock
void bsp_global_mutex_lock(void)
Critical section enter API using semaphore/mutex/interrupt disable primitives from RTOS....
bsp_pdi_access_perm_dword
uint8_t bsp_pdi_access_perm_dword(uint16_t address, uint8_t access)
Checks if the PDI register [Four bytes] has the requested access permission and returns the result.
bsp_params::eeprom_pointer_for_stack
uint8_t ** eeprom_pointer_for_stack
Definition: tiescbsp.h:545
bsp_eeprom_read_t
int32_t(* bsp_eeprom_read_t)(uint8_t *buf, uint32_t len)
Definition: tiescbsp.h:495
t_host_interface::system_time_low
uint32_t system_time_low
Definition: tiescbsp.h:589
t_host_interface::cmdlow_ack
uint16_t cmdlow_ack
Definition: tiescbsp.h:594
bsp_eeprom_write_t
int32_t(* bsp_eeprom_write_t)(uint8_t *buf, uint32_t len)
Definition: tiescbsp.h:496
t_sm_processdata
Struct for host to PRU-ICSS command interface.
Definition: tiescbsp.h:576
t_mdio_params::addr0
uint8_t addr0
Definition: tiescbsp.h:631
bsp_process_data_access_complete
void bsp_process_data_access_complete(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t len, int16_t sm_index)
This API is invoked after PDI side completes read/write to PD address returned by bsp_get_process_dat...
bsp_params::ethphy_init
bsp_ethphy_init_t ethphy_init
Definition: tiescbsp.h:530
bsp_read_word
uint16_t bsp_read_word(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 16-bit value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area.
t_sm_processdata::lock_state
uint8_t lock_state
Definition: tiescbsp.h:578
bsp_get_latch1_posedge_time
void bsp_get_latch1_posedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch1 posedge timestamp for application use(nanosec resolution)
bsp_get_phy_address_t
int8_t(* bsp_get_phy_address_t)(uint8_t instance, uint8_t portNumber)
Definition: tiescbsp.h:501
bsp_hwspinlock_unlock
void bsp_hwspinlock_unlock(int num)
Release selected spinlock instance.
bsp_is_pdi_perm_read_only
uint8_t bsp_is_pdi_perm_read_only(uint16_t *perm_array, uint16_t address)
Checks if the PDI register [byte] has read only access permission and returns the result.
bsp_send_command_to_firmware
void bsp_send_command_to_firmware(PRUICSS_Handle pruIcssHandle, uint32_t command, uint16_t param1, uint16_t param2)
Send command and parameters from stack to firmware to perform some action based on stack state or in ...
bsp_read_byte
uint8_t bsp_read_byte(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a byte value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area.
bsp_pdi_write_indication
void bsp_pdi_write_indication(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t length, uint16_t value)
Invoked after writing a register or mailbox buffer from PDI side .
t_sm_properties::length
uint16_t length
Definition: tiescbsp.h:622
bsp_params_init
void bsp_params_init(bsp_params *init_params)
Initialize the members of bsp_params with default values.
t_sm_properties
Definition: tiescbsp.h:620
bsp_pruss_iepreg_write
void bsp_pruss_iepreg_write(PRUICSS_Handle pruIcssHandle, uint32_t val, uint32_t regoffset)
Write a 32-bit value from PRU-ICSS IEP register at 'regoffset'.
bsp_pruss_mdioreg_read
uint32_t bsp_pruss_mdioreg_read(PRUICSS_Handle pruIcssHandle, uint32_t regoffset)
Read a 32-bit value from PRU-ICSS MDIO register at 'regoffset'.
bsp_read_dword_isr
uint32_t bsp_read_dword_isr(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 32-bit value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area.
bsp_eeprom_emulation_reload
int32_t bsp_eeprom_emulation_reload(PRUICSS_Handle pruIcssHandle)
Perform reload operation after validating EEPROM CRC.
bsp_set_pdi_wd_trigger_mode
void bsp_set_pdi_wd_trigger_mode(PRUICSS_Handle pruIcssHandle, uint32_t mode)
Configure PDI WD trigger mode, PDI WD is triggered automatically by h/w on RX_SOF(port0/port1),...
bsp_eeprom_emulation_flush
void bsp_eeprom_emulation_flush(void)
Flush the EEPROM cache to non-volatile storage. Write is performed using eeprom_write callback from b...
bsp_read
void bsp_read(PRUICSS_Handle pruIcssHandle, uint8_t *pdata, uint16_t address, uint16_t len)
Read a byte array at 'address' from ESC memory.
bsp_get_process_data_address
uint16_t bsp_get_process_data_address(PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t len, int16_t *p_sm_index)
Get the actual address of the buffer for PDI side read/write from host in 3-buffer mode.
bsp_params::pruicssIepClkFreq
uint8_t pruicssIepClkFreq
Definition: tiescbsp.h:557
bsp_read_word_isr
uint16_t bsp_read_word_isr(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 16-bit value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area.
bsp_set_sm_properties
void bsp_set_sm_properties(PRUICSS_Handle pruIcssHandle, uint8_t sm, uint16_t address, uint16_t len)
Set the address, length info from register to FWHAL layer. During INIT to PREOP transition in Mailbox...
t_host_interface::system_time_high
uint32_t system_time_high
Definition: tiescbsp.h:590
bsp_params::pdi_isr
bsp_ethercat_stack_isr_function pdi_isr
Definition: tiescbsp.h:548
bsp_ethercat_stack_isr_function
void(* bsp_ethercat_stack_isr_function)(void)
Definition: tiescbsp.h:502
bsp_pruss_mdio_phy_write
int16_t bsp_pruss_mdio_phy_write(PRUICSS_Handle pruIcssHandle, uint8_t phyaddr, uint8_t regoffset, uint16_t regval)
API to write PHY register via PRU-ICSS MDIO.
bsp_params::spinlock_base_address
uint32_t spinlock_base_address
Definition: tiescbsp.h:527
t_register_properties
Struct for register permission array.
Definition: tiescbsp.h:614
bsp_get_latch1_negedge_time
void bsp_get_latch1_negedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch0 negedge timestamp for application use(nanosec resolution)
bsp_set_pru_firmware
void bsp_set_pru_firmware(uint32_t *frameProc, uint32_t frameProcLen, uint32_t *hostProc, uint32_t hostProcLen)
This function internally sets the location from which PRU firmwares can be loaded.
bsp_pdi_access_perm_word
uint8_t bsp_pdi_access_perm_word(uint16_t address, uint8_t access)
Checks if the PDI register [Two bytes] has the requested access permission and returns the result.
bsp_set_pdi_perm_read_only
void bsp_set_pdi_perm_read_only(uint16_t *perm_array, uint16_t address)
Set the PDI register [byte] access permission to read only.
t_mdio_params::enhancedlink_enable
uint8_t enhancedlink_enable
Definition: tiescbsp.h:635
bsp_set_eeprom_updated_time
void bsp_set_eeprom_updated_time(void)
Set EEPROM update time.
bsp_write_byte
void bsp_write_byte(PRUICSS_Handle pruIcssHandle, uint8_t val, uint16_t address)
Write a byte value at 'address' in ESC memory.
bsp_eeprom_load_esc_registers
int32_t bsp_eeprom_load_esc_registers(PRUICSS_Handle pruIcssHandle, int32_t reload_flag)
For loading ESC registers from EEPROM during first boot/reload after validating CRC.
bsp_esc_reg_perm_init
void bsp_esc_reg_perm_init(PRUICSS_Handle pruIcssHandle)
Sets up register permissions for ECAT side access for TI ESC, if ENABLE_PDI_REG_PERMISSIONS is define...
bsp_write
void bsp_write(PRUICSS_Handle pruIcssHandle, uint8_t *pdata, uint16_t address, uint16_t len)
Write 'len' bytes from pdata to 'address' in ESC memory.
t_mdio_params::addr1
uint8_t addr1
Definition: tiescbsp.h:632
t_host_interface::resp1low
uint16_t resp1low
Definition: tiescbsp.h:597
bsp_write_word
void bsp_write_word(PRUICSS_Handle pruIcssHandle, uint16_t val, uint16_t address)
Write a 16-bit value at 'address' in ESC memory.
bsp_eeprom_emulation_command_ack
void bsp_eeprom_emulation_command_ack(PRUICSS_Handle pruIcssHandle)
Perform reload operation after validating EEPROM CRC, Wrapper API for SSC.
bsp_pruss_mdio_phy_read
int16_t bsp_pruss_mdio_phy_read(PRUICSS_Handle pruIcssHandle, uint8_t phyaddr, uint8_t regoffset, uint16_t *regval)
API to read PHY register via PRU-ICSS MDIO.
t_mdio_params::link1pol
uint8_t link1pol
Definition: tiescbsp.h:634
t_mdio_params
Struct for MDIO initialization parameters.
Definition: tiescbsp.h:629
bsp_hwspinlock_unlock_t
void(* bsp_hwspinlock_unlock_t)(int num)
Definition: tiescbsp.h:499
bsp_set_digio_out
void bsp_set_digio_out(PRUICSS_Handle pruIcssHandle, uint8_t num)
Set selected digital output pin.
bsp_get_pdi_access_perm
uint8_t bsp_get_pdi_access_perm(uint16_t address, uint8_t access)
Checks if the PDI register [byte] has the requested access permission and returns the result.
bsp_global_mutex_unlock
void bsp_global_mutex_unlock(void)
Critical section leave API using semaphore/mutex/interrupt enable primitives from RTOS....
t_host_interface::param2low
uint16_t param2low
Definition: tiescbsp.h:596
bsp_params::interrupt_offset
int32_t interrupt_offset
Definition: tiescbsp.h:515
bsp_exit
void bsp_exit(PRUICSS_Handle pruIcssHandle)
Cleanup of EtherCAT FWHAL It does following things: .
t_host_interface
Struct for host to PRU-ICSS command interface Starts at PRU0 DMEM.
Definition: tiescbsp.h:587
bsp_params::link0_polarity
uint32_t link0_polarity
Definition: tiescbsp.h:535
bsp_init
int32_t bsp_init(bsp_params *init_params)
Initialize the EtherCAT FWHAL It does following things: .
bsp_read_dword
uint32_t bsp_read_dword(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a 32-bit value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area.
bsp_start_esc_isr
void bsp_start_esc_isr(PRUICSS_Handle pruIcssHandle)
Register IRQ handlers for various PRU-ICSS interrupts from firmware to host to clear corresponding ev...
bsp_get_timer_register
uint32_t bsp_get_timer_register(void)
Returns the time difference from last call of bsp_clear_timer_register to this bsp_get_timer_register...
bsp_get_eeprom_updated_time
uint32_t bsp_get_eeprom_updated_time(void)
Get EEPROM Updated time.
bsp_params::pruicss_handle
PRUICSS_Handle pruicss_handle
Definition: tiescbsp.h:513
bsp_pruss_cmd_intfc_write_word
void bsp_pruss_cmd_intfc_write_word(uint16_t val, volatile uint16_t *ptr)
Read a 16-bit value from PRU-ICSS IEP command interface.
t_host_interface::param1low
uint16_t param1low
Definition: tiescbsp.h:595
t_mdio_params::link0pol
uint8_t link0pol
Definition: tiescbsp.h:633
bsp_params::pruicssClkFreq
uint8_t pruicssClkFreq
Definition: tiescbsp.h:562
bsp_get_local_sys_time
void bsp_get_local_sys_time(uint32_t *systime_low, uint32_t *systime_high)
Return EtherCAT time base for application use.
bsp_write_dword
void bsp_write_dword(PRUICSS_Handle pruIcssHandle, uint32_t val, uint16_t address)
Write a 32-bit value at 'address' in ESC memory.
bsp_pruss_cmd_intfc_read_word
uint16_t bsp_pruss_cmd_intfc_read_word(volatile uint16_t *ptr)
Read a 16-bit value from PRU-ICSS IEP command interface.
bsp_pruss_iepreg_read
uint32_t bsp_pruss_iepreg_read(PRUICSS_Handle pruIcssHandle, uint32_t regoffset)
Read a 32-bit value from PRU-ICSS IEP register at 'regoffset'.
bsp_eeprom_emulation_init
void bsp_eeprom_emulation_init(void)
Initialize the EEPROM cache in volatile RAM. If the non-volatile storage has valid data(read is perfo...
bsp_pdi_access_perm_array
uint8_t bsp_pdi_access_perm_array(uint16_t address, uint8_t access, uint16_t size)
Checks if all PDI registers starting from 'address' has the requested access permission and returns t...
t_sm_processdata::addr
uint16_t addr
Definition: tiescbsp.h:579
bsp_set_pdi_perm_read_write
void bsp_set_pdi_perm_read_write(uint16_t *perm_array, uint16_t address)
Set the PDI register [byte] access permission to read and write.
bsp_params::phy0_address
uint32_t phy0_address
Definition: tiescbsp.h:539
bsp_params::eeprom_write
bsp_eeprom_write_t eeprom_write
Definition: tiescbsp.h:525
bsp_clear_timer_register
void bsp_clear_timer_register(void)
Update the time when bsp_clear_timer_register last invoked. This is a wrapper API used by SSC.
Sync1Isr
void Sync1Isr(void *args)
SYNC1 IRQ Handler.
bsp_pdi_mbx_read_start
void bsp_pdi_mbx_read_start(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side read from write mailbox has started.
t_mdio_params::clkdiv
uint16_t clkdiv
Definition: tiescbsp.h:630
bsp_get_pdi_write_access_fail_cnt
uint32_t bsp_get_pdi_write_access_fail_cnt()
Returns the count of PDI write access failures.
bsp_pdi_mbx_read_complete
void bsp_pdi_mbx_read_complete(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side read from write mailbox has completed.
Sync0Isr
void Sync0Isr(void *args)
SYNC0 IRQ handler.
bsp_pruss_mdio_init
int16_t bsp_pruss_mdio_init(PRUICSS_Handle pruIcssHandle, t_mdio_params *pmdio_params)
Initializes PRU-ICSS MDIO for EtherCAT firmware to communicate with PHYs. Must be called after poweri...
bsp_pdi_mbx_write_complete
void bsp_pdi_mbx_write_complete(PRUICSS_Handle pruIcssHandle)
Indicates to the firmware that PDI side write to read mailbox has completed.
bsp_clear_digio_out
void bsp_clear_digio_out(PRUICSS_Handle pruIcssHandle, uint8_t num)
Clear selected digital output pin.
bsp_get_sm_properties
t_sm_properties * bsp_get_sm_properties(uint8_t sm)
Get the pointer to requested SM properties. It is used for Buffer/Mailbox read/write detection from H...
bsp_params::mdioManualMode
uint8_t mdioManualMode
Definition: tiescbsp.h:566
bsp_params::sync1_isr
bsp_ethercat_stack_isr_function sync1_isr
Definition: tiescbsp.h:552
bsp_get_eeprom_update_status
uint8_t bsp_get_eeprom_update_status(void)
Read the EEPROM update status from FWHAL. Typically called from low priority task periodically check ...
t_host_interface::cmdlow
uint16_t cmdlow
Definition: tiescbsp.h:593
bsp_params::enhancedlink_enable
uint8_t enhancedlink_enable
Definition: tiescbsp.h:532
bsp_get_sm_index
int16_t bsp_get_sm_index(uint16_t address, uint16_t len)
bsp_init_spinlock_t
void(* bsp_init_spinlock_t)(void)
Definition: tiescbsp.h:497
bsp_read_byte_isr
uint8_t bsp_read_byte_isr(PRUICSS_Handle pruIcssHandle, uint16_t address)
Read a byte value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area.
bsp_set_digio_sw_dataout_enable
void bsp_set_digio_sw_dataout_enable(PRUICSS_Handle pruIcssHandle)
Configure digio for sw controlled dataout mode.
EcatIsr
void EcatIsr(void *args)
ECAT IRQ Handler.
bsp_ethphy_init_t
void(* bsp_ethphy_init_t)(PRUICSS_Handle pruIcssHandle, uint8_t phy0addr, uint8_t phy1addr, uint8_t enhancedlink_enable)
Definition: tiescbsp.h:500
bsp_params
Struct for FWHAL initialization Parameters.
Definition: tiescbsp.h:512
bsp_get_eeprom_cache_base
uint8_t * bsp_get_eeprom_cache_base(void)
Return pointer to volatile EEPROM cache in FWHAL for processing to access the EEPROM.
bsp_pruss_mdioreg_write
void bsp_pruss_mdioreg_write(PRUICSS_Handle pruIcssHandle, uint32_t val, uint32_t regoffset)
Write a 32-bit value from PRU-ICSS MDIO register at 'regoffset'.
bsp_params::link1_polarity
uint32_t link1_polarity
Definition: tiescbsp.h:537
bsp_pdi_sm_config_ongoing
uint8_t bsp_pdi_sm_config_ongoing(PRUICSS_Handle pruIcssHandle)
Checks whether firmware has finished updating internal state for SM configuration change initiated by...
bsp_params::sync0_isr
bsp_ethercat_stack_isr_function sync0_isr
Definition: tiescbsp.h:550
bsp_params::eeprom_read
bsp_eeprom_read_t eeprom_read
Definition: tiescbsp.h:523
t_host_interface::sm_config_ongoing
uint8_t sm_config_ongoing
Definition: tiescbsp.h:591
bsp_pruss_mdio_phy_link_state
uint32_t bsp_pruss_mdio_phy_link_state(PRUICSS_Handle pruIcssHandle, uint8_t phyaddr)
Get the link status for selected PHY, this API considers MII_link signal polarity differences and rec...
t_sm_properties::physical_start_addr
uint16_t physical_start_addr
Definition: tiescbsp.h:621
bsp_params::default_tiesc_eeprom
const unsigned char * default_tiesc_eeprom
Definition: tiescbsp.h:543
bsp_get_latch0_negedge_time
void bsp_get_latch0_negedge_time(PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high)
Return latch0 negedge timestamp for application use(nanosec resolution)
bsp_hwspinlock_init
void bsp_hwspinlock_init(void)
Initialize SOC spinlock, enable clocks and init spinlock instance 0 through 7 to unlocked state.