Go to the source code of this file.
Data Structures | |
| struct | bsp_params |
| Struct for FWHAL initialization Parameters. More... | |
| struct | t_sm_processdata |
| Struct for host to PRU-ICSS command interface. More... | |
| struct | t_host_interface |
| Struct for host to PRU-ICSS command interface Starts at PRU0 DMEM. More... | |
| struct | t_register_properties |
| Struct for register permission array. More... | |
| struct | t_sm_properties |
| struct | t_mdio_params |
| Struct for MDIO initialization parameters. More... | |
Macros | |
| #define | TIESC_MAX_FRAME_SIZE (0x7CF) |
| TIESC_MAX_FRAME_SIZE Maximum frame size cutoff of 2000 bytes. More... | |
| #define | ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM 0 |
| #define | MAX_SYNC_MAN 8 |
| #define | SIZEOF_SM_REGISTER 8 |
| #define | TIESC_EEPROM_SIZE 0x800 |
| #define | MAILBOX_WRITE 0 |
| #define | MAILBOX_READ 1 |
| #define | PROCESS_DATA_OUT 2 |
| #define | PROCESS_DATA_IN 3 |
| #define | MBX_WRITE_EVENT ((uint16_t) 0x0100) |
| #define | MBX_READ_EVENT ((uint16_t) 0x0200) |
| #define | ESC_ADDR_REV_TYPE 0x000 |
| #define | ESC_ADDR_BUILD 0x002 |
| #define | ESC_ADDR_CONFIG_STATION_ALIAS 0x012 |
| #define | ESC_ADDR_DLSTATUS 0x110 |
| #define | ESC_ADDR_ALCONTROL 0x120 |
| #define | ESC_ADDR_ALSTATUS 0x130 |
| #define | ESC_ADDR_PDI_CONTROL 0x140 |
| #define | ESC_PDI_CONTROL_ELD_ALL_PORTS_MASK (1 << 1) |
| #define | ESC_ADDR_PDI_CONFIG 0x150 |
| #define | ESC_ADDR_AL_EVENT_MASK 0x204 |
| #define | ESC_ADDR_AL_EVENT_REQ 0x220 |
| #define | ESC_ADDR_SM_WD_STATUS 0x440 |
| #define | ESC_ADDR_EEPROM_CTRL 0x502 |
| #define | ESC_ADDR_MI_ECAT_ACCESS 0x516 |
| #define | ESC_ADDR_MI_PDI_ACCESS 0x517 |
| #define | ESC_EEPROM_CMD_MASK 0x0700 |
| #define | ESC_EEPROM_CMD_READ_MASK 0x0100 |
| #define | ESC_EEPROM_CMD_WRITE_MASK 0x0200 |
| #define | ESC_EEPROM_CMD_RELOAD_MASK 0x0400 |
| #define | ESC_EEPROM_ERROR_MASK 0x7800 |
| #define | ESC_EEPROM_ERROR_CRC 0x0800 |
| #define | ESC_EEPROM_ERROR_CMD_ACK 0x2000 |
| #define | ESC_EEPROM_BUSY_MASK 0x8000 |
| #define | ESC_ADDR_SYNCMAN 0x800 |
| #define | ESC_ADDR_SM1_STATUS 0x80D |
| #define | SM_STATUS_MBX_FULL 0x08 |
| #define | ESC_ADDR_SM0_STATUS 0x805 |
| #define | ESC_ADDR_SM0_ACTIVATE 0x806 |
| #define | ESC_ADDR_SM1_ACTIVATE 0x806+8 |
| #define | ESC_ADDR_SM2_ACTIVATE 0x806+8*2 |
| #define | ESC_ADDR_SM3_ACTIVATE 0x806+8*3 |
| #define | ESC_ADDR_SM4_ACTIVATE 0x806+8*4 |
| #define | ESC_ADDR_SM5_ACTIVATE 0x806+8*5 |
| #define | ESC_ADDR_SM6_ACTIVATE 0x806+8*6 |
| #define | ESC_ADDR_SM7_ACTIVATE 0x806+8*7 |
| #define | ESC_ADDR_SM0_PDI_CONTROL 0x807 |
| #define | ESC_ADDR_SM1_PDI_CONTROL 0x807+8 |
| #define | ESC_ADDR_SM2_PDI_CONTROL 0x807+8*2 |
| #define | ESC_ADDR_SM3_PDI_CONTROL 0x807+8*3 |
| #define | ESC_ADDR_SM4_PDI_CONTROL 0x807+8*4 |
| #define | ESC_ADDR_SM5_PDI_CONTROL 0x807+8*5 |
| #define | ESC_ADDR_SM6_PDI_CONTROL 0x807+8*6 |
| #define | ESC_ADDR_SM7_PDI_CONTROL 0x807+8*7 |
| #define | SM_PDI_CONTROL_SM_DISABLE 1 |
| #define | ESC_ADDR_SYSTIME 0x910 |
| #define | ESC_ADDR_SYSTIME_HIGH 0x914 |
| #define | ESC_ADDR_SYSTIME_OFFSET 0x920 |
| #define | ESC_ADDR_SYSTIME_DELAY 0x928 |
| #define | ESC_ADDR_SPEEDCOUNTER_START 0x930 |
| #define | ESC_ADDR_TIMEDIFF_FILTDEPTH 0x934 |
| #define | ESC_ADDR_SPEEDDIFF_FILTDEPTH 0x935 |
| #define | ESC_ADDR_SYNC_PULSE_LENGTH 0x982 |
| #define | ESC_ADDR_SYNC_STATUS 0x98E |
| #define | ESC_ADDR_LATCH0_CONTROL 0x9A8 |
| #define | ESC_ADDR_LATCH1_CONTROL 0x9A9 |
| #define | ESC_ADDR_LATCH0_POS_EDGE 0x9B0 |
| #define | ESC_ADDR_LATCH0_NEG_EDGE 0x9B8 |
| #define | ESC_ADDR_LATCH1_POS_EDGE 0x9C0 |
| #define | ESC_ADDR_LATCH1_NEG_EDGE 0x9C8 |
| #define | ESC_ADDR_TI_PORT0_ACTIVITY 0xE00 |
| #define | ESC_ADDR_TI_PORT1_ACTIVITY 0xE04 |
| #define | ESC_ADDR_TI_PORT0_PHYADDR 0xE08 |
| #define | ESC_ADDR_TI_PORT1_PHYADDR 0xE09 |
| #define | ESC_ADDR_TI_PDI_ISR_PINSEL 0xE0A |
| #define | ESC_ADDR_TI_PHY_LINK_POLARITY 0XE0C |
| #define | ESC_ADDR_TI_PROCESS_PATH_TX_START_DELAY 0xE10 |
| #define | ESC_ADDR_TI_AUTOFORWARD_PATH_TX_START_DELAY 0xE12 |
| #define | ESC_ADDR_TI_ESC_RESET 0xE14 |
| #define | ESC_ADDR_TI_EDMA_LATENCY_ENHANCEMENT 0xE24 |
| #define | ESC_ADDR_TI_PHY_RX_ER_REG 0xE28 |
| #define | ESC_ADDR_TI_PRU_CLK_FREQUENCY 0xE34 |
| #define | ESC_ADDR_TI_MDIO_MANUAL_MODE 0xE35 |
| #define | ESC_ADDR_TI_ENHANCED_LINK_DETECT 0xE36 |
| #define | ESC_ADDR_TI_IEP_CLK_FREQUENCY 0xED1 |
| #define | TI_ESC_RST_CMD_U 0x545352 |
| #define | TI_ESC_RST_CMD_L 0x747372 |
| #define | ESC_ADDR_MEMORY 0x1000 |
| #define | CMD_DL_USER_CLEAR_AL_EVENT_HIGH 0x0 |
| #define | CMD_DL_USER_GET_BUFFER_READ_ADDR 0x1 |
| #define | CMD_DL_USER_GET_BUFFER_WRITE_ADDR 0x2 |
| #define | CMD_DL_USER_SET_BUFFER_WRITE_DONE 0x3 |
| #define | CMD_DL_USER_ACK_MBX_READ 0x4 |
| CMD_DL_USER_ACK_MBX_READ Mailbox read ACK. More... | |
| #define | CMD_DL_USER_ACK_MBX_WRITE 0x5 |
| CMD_DL_USER_ACK_MBX_WRITE Mailbox write ACK. More... | |
| #define | CMD_DL_USER_EEPROM_CMD_ACK 0x6 |
| CMD_DL_USER_EEPROM_CMD_ACK User EEPROM ACK. More... | |
| #define | CMD_DL_USER_READ_SYNC_STATUS 0x7 |
| CMD_DL_USER_READ_SYNC_STATUS User Read sync status. More... | |
| #define | SYNC0 0 |
| #define | SYNC1 1 |
| #define | CMD_DL_USER_READ_AL_CONTROL 0x8 |
| CMD_DL_USER_READ_AL_CONTROL User Read AL Control. More... | |
| #define | CMD_DL_USER_WRITE_AL_STATUS 0x9 |
| CMD_DL_USER_WRITE_AL_STATUS User Read AL Status. More... | |
| #define | CMD_DL_USER_READ_PD_WD_STATUS 0xA |
| CMD_DL_USER_READ_PD_WD_STATUS User Read PD_WD Status. More... | |
| #define | CMD_DL_USER_READ_SM_ACTIVATE 0xB |
| CMD_DL_USER_READ_SM_ACTIVATE User Read SM Activate. More... | |
| #define | CMD_DL_USER_WRITE_SM_PDI_CTRL 0xC |
| CMD_DL_USER_WRITE_SM_PDI_CTRL User Write SM PDI control. More... | |
| #define | CMD_DL_USER_READ_LATCH_TIME 0xD |
| CMD_DL_USER_READ_LATCH_TIME User Read latch time. More... | |
| #define | LATCH0_POS_EDGE 0 |
| #define | LATCH0_NEG_EDGE 1 |
| #define | LATCH1_POS_EDGE 2 |
| #define | LATCH1_NEG_EDGE 3 |
| #define | CMD_DL_USER_READ_SYS_TIME 0xE |
| CMD_DL_USER_READ_SYS_TIME User Read sys time. More... | |
| #define | CMD_DL_USER_CLEAR_AL_EVENT_LOW 0xF |
| CMD_DL_USER_CLEAR_AL_EVENT_LOW User clear AL event low. More... | |
| #define | SWAPWORD |
| #define | SWAPDWORD |
| #define | ICSS_MDIO_USRPHYSEL_LINKINT_ENABLE 0x40 |
| #define | ICSS_MDIO_USRPHYSEL_LINKSTAT_MLINK 0x80 |
| #define | TIESC_PERM_RW 0x0 |
| #define | TIESC_PERM_WRITE_ONLY 0x1 |
| #define | TIESC_PERM_READ_ONLY 0x2 |
| #define | TIESC_PERM_WRITE TIESC_PERM_WRITE_ONLY |
| #define | TIESC_PERM_READ TIESC_PERM_READ_ONLY |
| #define | PDI_PERM_RW 0x0 |
| #define | PDI_PERM_READ_ONLY 0x1 |
| #define | PDI_PERM_WRITE PDI_PERM_RW |
| #define | PDI_PERM_READ PDI_PERM_READ_ONLY |
| #define | TIESC_MDIO_CLKDIV 79 |
| #define | TIESC_MDIO_RX_LINK_DISABLE 0 |
| #define | TIESC_MDIO_RX_LINK_ENABLE 1 |
| #define | TIESC_LINK_POL_ACTIVE_LOW 1 |
| #define | TIESC_LINK_POL_ACTIVE_HIGH 0 |
| #define | PDI_WD_TRIGGER_RX_SOF (0 << 4) |
| PDI_WD_TRIGGER_RX_SOF Watchdog RX Start of Frame Trigger. More... | |
| #define | PDI_WD_TRIGGER_LATCH_IN (1 << 4) |
| PDI_WD_TRIGGER_LATCH_IN Watchdog LATCH IN Trigger. More... | |
| #define | PDI_WD_TRIGGER_SYNC0_OUT (2 << 4) |
| PDI_WD_TRIGGER_SYNC0_OUT Watchdog SYNC0 Trigger. More... | |
| #define | PDI_WD_TRIGGER_SYNC1_OUT (3 << 4) |
| PDI_WD_TRIGGER_SYNC1_OUT Watchdog SYNC1 Trigger. More... | |
| #define | TIESC_PROCESS_PATH_TX_DELAY_200_MHZ_CLOCK 0x48 |
| #define | TIESC_AUTOFORWARD_PATH_TX_DELAY_200_MHZ_CLOCK 0x38 |
| #define | TIESC_PROCESS_PATH_TX_DELAY_333_MHZ_CLOCK 0x50 |
| #define | TIESC_AUTOFORWARD_PATH_TX_DELAY_333_MHZ_CLOCK 0x30 |
| #define | PDI_ISR_EDIO_NUM 7 |
| #define | USE_ECAT_TIMER |
| #define | ENABLE_PDI_TASK |
| #define | ENABLE_SYNC_TASK |
| #define | ASSERT_DMB() __asm__ __volatile__ (" dmb" "\n\t": : : "memory") |
| SUPPORT_CMDACK_POLL_MODE If PDI and SYNC ISR is handled in HWI context (similar to SSC) interrupt mode of CMDACK won't work as they are low priority than SYNC and PDI ISR - use polling instead. More... | |
| #define | ASSERT_DSB() __asm__ __volatile__ (" dsb" "\n\t": : : "memory") |
| #define | ECAT_TIMER_INC_P_MS 1000000 |
| #define | ESC_SYSTEMTIME_OFFSET_OFFSET 0x0920 |
| #define | ESC_SPEED_COUNTER_START_OFFSET 0x0930 |
| #define | ESC_DC_START_TIME_CYCLIC_OFFSET 0x0990 |
| #define | DRIFTCTRL_TASK_SYNC_ZERO_CROSS_ADJUST 0xE0 |
| #define | LOCK_PD_BUF_AVAILABLE_FOR_HOST 0 |
| LOCK_PD_BUF_AVAILABLE_FOR_HOST LOCK available for HOST. More... | |
| #define | LOCK_PD_BUF_HOST_ACCESS_START 1 |
| LOCK_PD_BUF_HOST_ACCESS_START Lock available for host access start. More... | |
| #define | LOCK_PD_BUF_HOST_ACCESS_FINISH 2 |
| LOCK_PD_BUF_HOST_ACCESS_FINISH Lock available for host access finish. More... | |
| #define | LOCK_PD_BUF_CHECK_AVAILABILITY_RETRY_COUNT (10U) |
| LOCK_PD_BUF_CHECK_AVAILABILITY_RETRY_COUNT Number of times the lock_state of SM is checked for availability in bsp_get_process_data_address function, in case the lock_state is not LOCK_PD_BUF_HOST_ACCESS_START. More... | |
| #define | TIESC_PRUICSS_CLOCK_FREQUENCY_200_MHZ (0) |
| TIESC_PRUICSS_CLOCK_FREQUENCY_200_MHZ PRU-ICSS Core Clock and IEP Clock running at 200 MHz. More... | |
| #define | TIESC_PRUICSS_CLOCK_FREQUENCY_333_MHZ (1) |
| TIESC_PRUICSS_CLOCK_FREQUENCY_333_MHZ PRU-ICSS Core Clock and IEP Clock running at 333 MHz. More... | |
| #define | TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_200_MHZ (0) |
| TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_200_MHZ PRU-ICSS IEP Clock running at 200 MHz. More... | |
| #define | TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_250_MHZ (1) |
| TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_250_MHZ PRU-ICSS IEP Clock running at 250 MHz. More... | |
| #define | TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_333_MHZ (2) |
| TIESC_PRUICSS_IEP_CLOCK_FREQUENCY_333_MHZ PRU-ICSS IEP Clock running at 333 MHz. More... | |
| #define | TIESC_MDIO_HW_MODE (0) |
| TIESC_MDIO_HW_MODE To set the SoC HW mode configuration for MDIO communication. More... | |
| #define | TIESC_MDIO_MANUAL_MODE_FW (1) |
| TIESC_MDIO_MANUAL_MODE_FW To set the manual mode configuration for MDIO communication using FW. More... | |
Typedefs | |
| typedef int32_t(* | bsp_eeprom_read_t) (uint8_t *buf, uint32_t len) |
| typedef int32_t(* | bsp_eeprom_write_t) (uint8_t *buf, uint32_t len) |
| typedef void(* | bsp_init_spinlock_t) (void) |
| typedef uint32_t(* | bsp_hwspinlock_lock_t) (int num) |
| typedef void(* | bsp_hwspinlock_unlock_t) (int num) |
| typedef void(* | bsp_ethphy_init_t) (PRUICSS_Handle pruIcssHandle, uint8_t phy0addr, uint8_t phy1addr, uint8_t enhancedlink_enable) |
| typedef int8_t(* | bsp_get_phy_address_t) (uint8_t instance, uint8_t portNumber) |
| typedef void(* | bsp_ethercat_stack_isr_function) (void) |
Functions | |
| void | bsp_params_init (bsp_params *init_params) |
| Initialize the members of bsp_params with default values. More... | |
| int32_t | bsp_init (bsp_params *init_params) |
| Initialize the EtherCAT FWHAL It does following things: . More... | |
| void | bsp_esc_reg_perm_init (PRUICSS_Handle pruIcssHandle) |
| Sets up register permissions for ECAT side access for TI ESC, if ENABLE_PDI_REG_PERMISSIONS is defined in tiescbsp.h, then this function also initializes register permissions for PDI side access from stack/application. More... | |
| void | bsp_start_esc_isr (PRUICSS_Handle pruIcssHandle) |
| Register IRQ handlers for various PRU-ICSS interrupts from firmware to host to clear corresponding events in PRU-ICSS INTC. More... | |
| void | bsp_exit (PRUICSS_Handle pruIcssHandle) |
| Cleanup of EtherCAT FWHAL It does following things: . More... | |
| void | bsp_set_pdi_wd_trigger_mode (PRUICSS_Handle pruIcssHandle, uint32_t mode) |
| Configure PDI WD trigger mode, PDI WD is triggered automatically by h/w on RX_SOF(port0/port1), latch0/1 input high, SYNC0/1 out high. PDI WD is also triggered whenever host sends a command to firmware. PDI WD may not expire if host stops sending commands to firmware alone, this will occur only if configured h/w events do not occur during WD period. More... | |
| void | bsp_send_command_to_firmware (PRUICSS_Handle pruIcssHandle, uint32_t command, uint16_t param1, uint16_t param2) |
| Send command and parameters from stack to firmware to perform some action based on stack state or in response to AL event interrupt or SYNC interrupt from ESC. More... | |
| void | bsp_eeprom_emulation_init (void) |
| Initialize the EEPROM cache in volatile RAM. If the non-volatile storage has valid data(read is performed using eeprom_read callback from bsp_params passed during bsp_init), load from there. Otherwise it loads predefined EEPROM in application using default_tiesc_eeprom from bsp_params passed during bsp_init. More... | |
| int32_t | bsp_eeprom_load_esc_registers (PRUICSS_Handle pruIcssHandle, int32_t reload_flag) |
| For loading ESC registers from EEPROM during first boot/reload after validating CRC. More... | |
| int32_t | bsp_eeprom_emulation_reload (PRUICSS_Handle pruIcssHandle) |
| Perform reload operation after validating EEPROM CRC. More... | |
| void | bsp_eeprom_emulation_command_ack (PRUICSS_Handle pruIcssHandle) |
| Perform reload operation after validating EEPROM CRC, Wrapper API for SSC. More... | |
| void | bsp_eeprom_emulation_flush (void) |
| Flush the EEPROM cache to non-volatile storage. Write is performed using eeprom_write callback from bsp_params passed during bsp_init. More... | |
| void | bsp_eeprom_emulation_exit (void) |
| Call EEPROM flush on exit. More... | |
| uint8_t * | bsp_get_eeprom_cache_base (void) |
| Return pointer to volatile EEPROM cache in FWHAL for processing to access the EEPROM. More... | |
| void | bsp_set_eeprom_updated_time (void) |
| Set EEPROM update time. More... | |
| uint32_t | bsp_get_eeprom_updated_time (void) |
| Get EEPROM Updated time. More... | |
| void | bsp_set_eeprom_update_status (uint8_t status) |
| Indicate to FWHAL whether EEPROM is written for flushing to non-volatile storage. Typically called on EEPROM write detection from stack. More... | |
| uint8_t | bsp_get_eeprom_update_status (void) |
| Read the EEPROM update status from FWHAL. Typically called from low priority task periodically check EEPROM dirty status for flush. More... | |
| void | bsp_set_sm_properties (PRUICSS_Handle pruIcssHandle, uint8_t sm, uint16_t address, uint16_t len) |
| Set the address, length info from register to FWHAL layer. During INIT to PREOP transition in Mailbox mode. During SAFEOP to OP transition in Buffer mode. More... | |
| t_sm_properties * | bsp_get_sm_properties (uint8_t sm) |
| Get the pointer to requested SM properties. It is used for Buffer/Mailbox read/write detection from Host PDI interface to indicate to the firmware. More... | |
| int16_t | bsp_get_sm_index (uint16_t address, uint16_t len) |
| uint8_t | bsp_pdi_sm_config_ongoing (PRUICSS_Handle pruIcssHandle) |
| Checks whether firmware has finished updating internal state for SM configuration change initiated by stack/PDI. More... | |
| void | bsp_pdi_mbx_read_start (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side read from write mailbox has started. More... | |
| void | bsp_pdi_mbx_read_complete (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side read from write mailbox has completed. More... | |
| void | bsp_pdi_mbx_write_start (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side write to read mailbox has started. More... | |
| void | bsp_pdi_mbx_write_complete (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side write to read mailbox has completed. More... | |
| uint16_t | bsp_get_process_data_address (PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t len, int16_t *p_sm_index) |
| Get the actual address of the buffer for PDI side read/write from host in 3-buffer mode. More... | |
| void | bsp_process_data_access_complete (PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t len, int16_t sm_index) |
| This API is invoked after PDI side completes read/write to PD address returned by bsp_get_process_data_address to indicate this to firmware for swapping buffers etc. More... | |
| uint8_t | bsp_read_byte (PRUICSS_Handle pruIcssHandle, uint16_t address) |
| Read a byte value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area. More... | |
| uint16_t | bsp_read_word (PRUICSS_Handle pruIcssHandle, uint16_t address) |
| Read a 16-bit value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area. More... | |
| uint32_t | bsp_read_dword (PRUICSS_Handle pruIcssHandle, uint16_t address) |
| Read a 32-bit value at 'Address' from ESC memory: SM mailbox (single buffer) mapped or register area. More... | |
| void | bsp_read (PRUICSS_Handle pruIcssHandle, uint8_t *pdata, uint16_t address, uint16_t len) |
| Read a byte array at 'address' from ESC memory. More... | |
| uint8_t | bsp_read_byte_isr (PRUICSS_Handle pruIcssHandle, uint16_t address) |
| Read a byte value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area. More... | |
| uint16_t | bsp_read_word_isr (PRUICSS_Handle pruIcssHandle, uint16_t address) |
| Read a 16-bit value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area. More... | |
| uint32_t | bsp_read_dword_isr (PRUICSS_Handle pruIcssHandle, uint16_t address) |
| Read a 32-bit value at 'Address' from ESC process data memory: SM buffer (3-buffer) mapped area. More... | |
| void | bsp_pdi_post_read_indication (PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t length) |
| Invoked after reading a register or mailbox buffer from PDI side . More... | |
| void | bsp_pdi_write_indication (PRUICSS_Handle pruIcssHandle, uint16_t address, uint16_t length, uint16_t value) |
| Invoked after writing a register or mailbox buffer from PDI side . More... | |
| void | bsp_write_byte (PRUICSS_Handle pruIcssHandle, uint8_t val, uint16_t address) |
| Write a byte value at 'address' in ESC memory. More... | |
| void | bsp_write_word (PRUICSS_Handle pruIcssHandle, uint16_t val, uint16_t address) |
| Write a 16-bit value at 'address' in ESC memory. More... | |
| void | bsp_write_dword (PRUICSS_Handle pruIcssHandle, uint32_t val, uint16_t address) |
| Write a 32-bit value at 'address' in ESC memory. More... | |
| void | bsp_write (PRUICSS_Handle pruIcssHandle, uint8_t *pdata, uint16_t address, uint16_t len) |
| Write 'len' bytes from pdata to 'address' in ESC memory. More... | |
| uint32_t | bsp_pruss_mdioreg_read (PRUICSS_Handle pruIcssHandle, uint32_t regoffset) |
| Read a 32-bit value from PRU-ICSS MDIO register at 'regoffset'. More... | |
| void | bsp_pruss_mdioreg_write (PRUICSS_Handle pruIcssHandle, uint32_t val, uint32_t regoffset) |
| Write a 32-bit value from PRU-ICSS MDIO register at 'regoffset'. More... | |
| uint32_t | bsp_pruss_iepreg_read (PRUICSS_Handle pruIcssHandle, uint32_t regoffset) |
| Read a 32-bit value from PRU-ICSS IEP register at 'regoffset'. More... | |
| void | bsp_pruss_iepreg_write (PRUICSS_Handle pruIcssHandle, uint32_t val, uint32_t regoffset) |
| Write a 32-bit value from PRU-ICSS IEP register at 'regoffset'. More... | |
| void | bsp_pruss_cmd_intfc_write_word (uint16_t val, volatile uint16_t *ptr) |
| Read a 16-bit value from PRU-ICSS IEP command interface. More... | |
| uint16_t | bsp_pruss_cmd_intfc_read_word (volatile uint16_t *ptr) |
| Read a 16-bit value from PRU-ICSS IEP command interface. More... | |
| uint8_t | bsp_get_pdi_access_perm (uint16_t address, uint8_t access) |
| Checks if the PDI register [byte] has the requested access permission and returns the result. More... | |
| uint8_t | bsp_pdi_access_perm_word (uint16_t address, uint8_t access) |
| Checks if the PDI register [Two bytes] has the requested access permission and returns the result. More... | |
| uint8_t | bsp_pdi_access_perm_dword (uint16_t address, uint8_t access) |
| Checks if the PDI register [Four bytes] has the requested access permission and returns the result. More... | |
| uint8_t | bsp_pdi_access_perm_array (uint16_t address, uint8_t access, uint16_t size) |
| Checks if all PDI registers starting from 'address' has the requested access permission and returns the result. More... | |
| void | bsp_set_pdi_perm_read_only (uint16_t *perm_array, uint16_t address) |
| Set the PDI register [byte] access permission to read only. More... | |
| void | bsp_set_pdi_perm_read_write (uint16_t *perm_array, uint16_t address) |
| Set the PDI register [byte] access permission to read and write. More... | |
| uint8_t | bsp_is_pdi_perm_read_only (uint16_t *perm_array, uint16_t address) |
| Checks if the PDI register [byte] has read only access permission and returns the result. More... | |
| uint32_t | bsp_get_pdi_read_access_fail_cnt () |
| Returns the count of PDI read access failures. More... | |
| uint32_t | bsp_get_pdi_write_access_fail_cnt () |
| Returns the count of PDI write access failures. More... | |
| int16_t | bsp_pruss_mdio_init (PRUICSS_Handle pruIcssHandle, t_mdio_params *pmdio_params) |
| Initializes PRU-ICSS MDIO for EtherCAT firmware to communicate with PHYs. Must be called after powering on PRU-ICSS domain and before PRU firmware is loaded and executed on both PRUs. This is called from bsp_init. More... | |
| int16_t | bsp_pruss_mdio_phy_read (PRUICSS_Handle pruIcssHandle, uint8_t phyaddr, uint8_t regoffset, uint16_t *regval) |
| API to read PHY register via PRU-ICSS MDIO. More... | |
| int16_t | bsp_pruss_mdio_phy_write (PRUICSS_Handle pruIcssHandle, uint8_t phyaddr, uint8_t regoffset, uint16_t regval) |
| API to write PHY register via PRU-ICSS MDIO. More... | |
| uint32_t | bsp_pruss_mdio_phy_link_state (PRUICSS_Handle pruIcssHandle, uint8_t phyaddr) |
| Get the link status for selected PHY, this API considers MII_link signal polarity differences and recommended when TIESC_MDIO_RX_LINK_ENABLE is enabled for enhanced link detection. More... | |
| void | bsp_set_digio_sw_dataout_enable (PRUICSS_Handle pruIcssHandle) |
| Configure digio for sw controlled dataout mode. More... | |
| void | bsp_set_digio_out (PRUICSS_Handle pruIcssHandle, uint8_t num) |
| Set selected digital output pin. More... | |
| void | bsp_clear_digio_out (PRUICSS_Handle pruIcssHandle, uint8_t num) |
| Clear selected digital output pin. More... | |
| void | bsp_hwspinlock_init (void) |
| Initialize SOC spinlock, enable clocks and init spinlock instance 0 through 7 to unlocked state. More... | |
| uint32_t | bsp_hwspinlock_lock (int num) |
| Acquire selected spinlock instance. More... | |
| void | bsp_hwspinlock_unlock (int num) |
| Release selected spinlock instance. More... | |
| uint32_t | bsp_get_timer_register (void) |
| Returns the time difference from last call of bsp_clear_timer_register to this bsp_get_timer_register. It handles overflow. More... | |
| void | bsp_clear_timer_register (void) |
| Update the time when bsp_clear_timer_register last invoked. This is a wrapper API used by SSC. More... | |
| void | bsp_get_local_sys_time (uint32_t *systime_low, uint32_t *systime_high) |
| Return EtherCAT time base for application use. More... | |
| void | bsp_get_latch0_posedge_time (PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high) |
| Return latch0 posedge timestamp for application use(nanosec resolution) More... | |
| void | bsp_get_latch0_negedge_time (PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high) |
| Return latch0 negedge timestamp for application use(nanosec resolution) More... | |
| void | bsp_get_latch1_posedge_time (PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high) |
| Return latch1 posedge timestamp for application use(nanosec resolution) More... | |
| void | bsp_get_latch1_negedge_time (PRUICSS_Handle pruIcssHandle, uint32_t *systime_low, uint32_t *systime_high) |
| Return latch0 negedge timestamp for application use(nanosec resolution) More... | |
| void | bsp_global_mutex_lock (void) |
| Critical section enter API using semaphore/mutex/interrupt disable primitives from RTOS. Implemented using HwiP_disableInt API. More... | |
| void | bsp_global_mutex_unlock (void) |
| Critical section leave API using semaphore/mutex/interrupt enable primitives from RTOS. Implemented using HwiP_enableInt API. More... | |
| void | Sync0Isr (void *args) |
| SYNC0 IRQ handler. More... | |
| void | Sync1Isr (void *args) |
| SYNC1 IRQ Handler. More... | |
| void | EcatIsr (void *args) |
| ECAT IRQ Handler. More... | |
| void | EscCmdLowAckIsr (void *args) |
| ESC CMD Low ACK IRQ Handler. More... | |
| void | bsp_set_pru_firmware (uint32_t *frameProc, uint32_t frameProcLen, uint32_t *hostProc, uint32_t hostProcLen) |
| This function internally sets the location from which PRU firmwares can be loaded. More... | |