real-time packet structure
Data Fields | |
| uint32_t | frameOffset |
| t_rtcMemBuff * | pBuffer |
| uint16_t | frameId |
| uint16_t | length |
| uint16_t | reduRatio |
| uint16_t | phase |
| uint8_t | type |
| uint8_t | port |
| uint8_t | crGroup |
| uint8_t | lIndex |
| uint8_t | isActive |
| uint8_t | block |
| uint8_t | next |
| uint8_t | last |
| uint8_t | validLast |
| uint8_t | proc |
| void * | userRef |
| uint32_t t_rtcPacket::frameOffset |
| t_rtcMemBuff* t_rtcPacket::pBuffer |
| uint16_t t_rtcPacket::frameId |
| uint16_t t_rtcPacket::length |
| uint16_t t_rtcPacket::reduRatio |
| uint16_t t_rtcPacket::phase |
| uint8_t t_rtcPacket::type |
| uint8_t t_rtcPacket::port |
| uint8_t t_rtcPacket::crGroup |
| uint8_t t_rtcPacket::lIndex |
| uint8_t t_rtcPacket::isActive |
| uint8_t t_rtcPacket::block |
| uint8_t t_rtcPacket::next |
| uint8_t t_rtcPacket::last |
| uint8_t t_rtcPacket::validLast |
| uint8_t t_rtcPacket::proc |
| void* t_rtcPacket::userRef |