Supervisor configuration. Attribute ID 4.
Data Fields | |
| uint8_t | superEnable |
| uint32_t | beaconInterval |
| uint32_t | beaconTimeout |
| uint16_t | vLanId |
| uint8_t | supPrecedence |
| uint8_t superConfig::superEnable |
device configured to run as supervisor default : false
| uint32_t superConfig::beaconInterval |
beacon interval value (microseconds)
| uint32_t superConfig::beaconTimeout |
beacon timeout value (microseconds)
| uint16_t superConfig::vLanId |
VLAN Id
| uint8_t superConfig::supPrecedence |
Supervisor precedence