Last active node at the end of the chain Class for Attributes 6 and 7.
Data Fields | |
| uint32_t | ipAddr |
| uint8_t | macAddr [6] |
| uint16_t | deviceNum |
| uint32_t lastActiveNode::ipAddr |
IP Address of the last active Node
| uint8_t lastActiveNode::macAddr[6] |
MAC of the last node
| uint16_t lastActiveNode::deviceNum |
from 0-N where N is the number of nodes (excluding supervisor) in the ring