List of MAC ID's which are exempted from Learning, this is for DLR implementation.
Data Fields | |
| uint8_t | MAC [6] |
| uint8_t | numExceptions |
| uint8_t exceptionList::MAC[6] |
MAC ID of supervisor which is exempt from learning
| uint8_t exceptionList::numExceptions |
number of exceptions, this is a flag where value greater than 1 indicates that exception exists