Data Fields | |
| int32_t | cDelay [DEBUG_DELAY_N_ITER] |
| uint32_t | lDelay [DEBUG_DELAY_N_ITER] |
| float | rcfPeer [DEBUG_DELAY_N_ITER] |
| uint32_t | reqDelay [DEBUG_DELAY_N_ITER] |
| uint32_t | resDelay [DEBUG_DELAY_N_ITER] |
| uint16_t | seqId [DEBUG_DELAY_N_ITER] |
| int32_t debugDelay_t::cDelay[DEBUG_DELAY_N_ITER] |
| uint32_t debugDelay_t::lDelay[DEBUG_DELAY_N_ITER] |
| float debugDelay_t::rcfPeer[DEBUG_DELAY_N_ITER] |
| uint32_t debugDelay_t::reqDelay[DEBUG_DELAY_N_ITER] |
| uint32_t debugDelay_t::resDelay[DEBUG_DELAY_N_ITER] |
| uint16_t debugDelay_t::seqId[DEBUG_DELAY_N_ITER] |