Data Fields | |
| syncState_t | syncState |
| uint32_t | cDelay [PTCP_NUM_PORTS] |
| ptcpPortStatus_t | cDelayEnable [PTCP_NUM_PORTS] |
| uint32_t | syncPllWnd |
| uint32_t | syncTimeoutFactor |
| uint32_t | takeoverTimeoutFactor |
| uint8_t | firstSyncRcv |
| uint8_t | syncRcv |
| uint32_t | nSyncMissed |
| uint8_t | subdomainUUID [16] |
| uint8_t | masterSA [6] |
| syncState_t currentPtcpStatus_t::syncState |
| uint32_t currentPtcpStatus_t::cDelay[PTCP_NUM_PORTS] |
| ptcpPortStatus_t currentPtcpStatus_t::cDelayEnable[PTCP_NUM_PORTS] |
| uint32_t currentPtcpStatus_t::syncPllWnd |
| uint32_t currentPtcpStatus_t::syncTimeoutFactor |
| uint32_t currentPtcpStatus_t::takeoverTimeoutFactor |
| uint8_t currentPtcpStatus_t::firstSyncRcv |
| uint8_t currentPtcpStatus_t::syncRcv |
| uint32_t currentPtcpStatus_t::nSyncMissed |
| uint8_t currentPtcpStatus_t::subdomainUUID[16] |
| uint8_t currentPtcpStatus_t::masterSA[6] |