Data Fields | |
| uint32_t | TorgSec |
| uint32_t | TorgNsec |
| uint32_t | TDelay |
| uint32_t | IEP_count_tS |
| uint32_t | IEP_count_tL_R |
| uint32_t | IEP_count_tL_F |
| uint32_t | IEP_count_fn |
| uint64_t | tick_S |
| uint64_t | tick_L |
| uint64_t | tick_fn |
| uint32_t LatchVars::TorgSec |
| uint32_t LatchVars::TorgNsec |
| uint32_t LatchVars::TDelay |
| uint32_t LatchVars::IEP_count_tS |
| uint32_t LatchVars::IEP_count_tL_R |
| uint32_t LatchVars::IEP_count_tL_F |
| uint32_t LatchVars::IEP_count_fn |
| uint64_t LatchVars::tick_S |
| uint64_t LatchVars::tick_L |
| uint64_t LatchVars::tick_fn |