AM263Px INDUSTRIAL COMMUNICATIONS SDK  10.02.00
ICSS_EMAC_InternalObject Struct Reference

Detailed Description

Opaque ICSS EMAC driver object.

Data Fields

uint32_t reserved [ICSS_EMAC_OBJECT_SIZE_IN_BYTES/sizeof(uint32_t)]
 

Field Documentation

◆ reserved

uint32_t ICSS_EMAC_InternalObject::reserved[ICSS_EMAC_OBJECT_SIZE_IN_BYTES/sizeof(uint32_t)]

reserved, should NOT be modified by end users