AM263Px INDUSTRIAL COMMUNICATIONS SDK  10.02.00
icss_eip_mcFltr.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ICSS_EIP_MCFLTR_H_
34 #define ICSS_EIP_MCFLTR_H_
35 
36 #ifdef __cplusplus
37 extern "C"
38 {
39 #endif
40 
41 
42 /* ========================================================================== */
43 /* Include Files */
44 /* ========================================================================== */
45 
47 
48 /* ========================================================================== */
49 /* Function Declarations */
50 /* ========================================================================== */
60 void eip_multicast_filter_config(PRUICSS_Handle pruicssHandle,
61  uint8_t command);
62 
72 void eip_multicast_stromPrev_config(PRUICSS_Handle pruicssHandle,
73  uint8_t command);
74 
85 void eip_multicast_filter_update_macid(PRUICSS_Handle pruicssHandle,
86  char *multicastAddr,
87  uint8_t command);
88 
96 void eip_multicast_filter_override_hashmask(PRUICSS_Handle pruicssHandle,
97  char *mask);
98 
105 void eip_multicast_filter_init(PRUICSS_Handle pruicssHandle);
106 
107 
108 #ifdef __cplusplus
109 }
110 #endif
111 
112 #endif /* ICSS_EIP_MCFLTR_H_ */
eip_multicast_filter_init
void eip_multicast_filter_init(PRUICSS_Handle pruicssHandle)
multicast filtering init
eip_multicast_filter_config
void eip_multicast_filter_config(PRUICSS_Handle pruicssHandle, uint8_t command)
configuration to enable/disable multicast filtering
icss_emac.h
eip_multicast_filter_override_hashmask
void eip_multicast_filter_override_hashmask(PRUICSS_Handle pruicssHandle, char *mask)
configure the mask
eip_multicast_filter_update_macid
void eip_multicast_filter_update_macid(PRUICSS_Handle pruicssHandle, char *multicastAddr, uint8_t command)
insert/delete a multicast MAC ID in the multicast filter table
eip_multicast_stromPrev_config
void eip_multicast_stromPrev_config(PRUICSS_Handle pruicssHandle, uint8_t command)
configuration to enable/disable storm prevention for multicast traffic