|
| struct | __attribute__ ((packed)) cpmDesc |
| |
| uint32_t | PN_allCpmKnown (PN_Handle pnHandle) |
| |
| void | PN_resetCpmPorts (PN_Handle pnHandle) |
| |
| void | PN_setCpmPort (PN_Handle pnHandle, t_rtcPacket *pID) |
| |
| int32_t | PN_togglePpmList (PN_Handle pnHandle, t_rtcPacket *pktID, uint8_t ppmMrpPortShift) |
| |
| int32_t | PN_writePpmDesc (PN_Handle pnHandle, t_rtcPacket *pPkt, uint8_t pos) |
| |
| int32_t | PN_writeCpmDesc (PN_Handle pnHandle, t_rtcPacket *pPkt, uint8_t pos) |
| |
| int32_t | PN_readPpmDesc (PN_Handle pnHandle, t_ppmDesc *pDesc, uint8_t pos, uint8_t act) |
| |
| int32_t | PN_readCpmDesc (PN_Handle pnHandle, t_cpmDesc *pDesc, uint8_t pos) |
| |
| int32_t | PN_setIndexInt (PN_Handle pnHandle, t_listIndex *index) |
| |
| int8_t | PN_getLastCpmBuffIndex (PN_Handle pnHandle, uint8_t pos) |
| |
| int32_t | PN_getIndexInt (t_listIndex *index) |
| |
| int32_t | PN_emptyList (t_descList *pList) |
| |
| int32_t | PN_writeSortedList (PN_Handle pnHandle, t_rtcPacket *pPkts) |
| |
| int8_t | PN_getDhtStatusEvent (PN_Handle pnHandle, t_rtcPacket **pktID) |
| |
| int8_t | PN_getListToggleStatusEvent (PN_Handle pnHandle, t_rtcPacket **pktID) |
| |
| int8_t | PN_getShadowIndex (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t lType) |
| |
| int32_t | PN_getPmStatus (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t dir, uint8_t numPm) |
| |
| int32_t | PN_setPPMARlink (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t ARgroup, uint8_t PpmNum) |
| |
| int32_t | PN_setCPMARlink (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t ARgroup, uint8_t CpmNum) |
| |
| int32_t | PN_setCpmDHT (PRUICSS_HwAttrs const *pruicssHwAttrs, uint16_t dht, uint8_t pos) |
| | Sets the Data hold timer timeout value for a given descriptor. More...
|
| |
| void | PN_clearMrpFlag (PN_Handle pnHandle) |
| | Clears the mrpFlag in ppmList data structure. More...
|
| |
| void | PN_setListToggleReq (PN_Handle pnHandle, uint8_t enable) |
| | Sets or clears the listToggleReq flag in ppmList data structure. More...
|
| |