Go to the source code of this file.
Macros | |
| #define | PNISO_MAX_NUM_EVENTS 2 |
| #define | PNISO_MODE_NONE 0 |
| #define | PNISO_MODE_INTERRUPT 1 |
| #define | PNISO_MODE_GPIO 2 |
| #define | PNISO_MODE_DISABLE 0 |
| #define | PNISO_MODE_ENABLE 1 |
| #define | PNISO_TI_EVENT 1 |
| #define | PNISO_TI_EVENT_REG_SHIFT 0 |
| #define | PNISO_TO_EVENT 2 |
| #define | PNISO_TO_EVENT_REG_SHIFT 1 |
| #define | PNISO_ERR_SUCCESS 0 |
| #define | PNISO_ERR_INVALID_EVENT -1 |
| #define | PNISO_ERR_EVENTS_EXHAUSTED -2 |
Functions | |
| void | PN_event1IsrHandler (void *arg) |
| Event1 ISR handler. Used to call the application ISR Handler in case a Ti ISOM event/signal is triggered. More... | |
| void | PN_event2IsrHandler (void *arg) |
| Event2 ISR handler. Used to call the application ISR Handler in case a To ISOM event/signal is triggered. More... | |
| int8_t | PN_ISO_initGPIOEvent (PN_Handle pnHandle, uint8_t isoMode, uint8_t isoEvent, uint32_t timeval, uint32_t duration) |
| API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled by default. More... | |
| void | PN_ISO_enableGPIOEvent (PN_Handle pnHandle) |
| API to enable the ISOM event/signal generation. More... | |
| void | PN_ISO_disableGPIOEvent (PN_Handle pnHandle) |
| API to disable the ISOM event/signal generation. More... | |
| void | PN_ISO_deInitGPIOEvent (PN_Handle pnHandle) |
| API to De init the ISOM event/signal. More... | |
| #define PNISO_MAX_NUM_EVENTS 2 |
| #define PNISO_MODE_NONE 0 |