Functions | |
| void | bsp_pdi_mbx_read_start (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side read from write mailbox has started. More... | |
| void | bsp_pdi_mbx_read_complete (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side read from write mailbox has completed. More... | |
| void | bsp_pdi_mbx_write_start (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side write to read mailbox has started. More... | |
| void | bsp_pdi_mbx_write_complete (PRUICSS_Handle pruIcssHandle) |
| Indicates to the firmware that PDI side write to read mailbox has completed. More... | |
| void bsp_pdi_mbx_read_start | ( | PRUICSS_Handle | pruIcssHandle | ) |
Indicates to the firmware that PDI side read from write mailbox has started.
| pruIcssHandle | PRUSS Handle |
| void bsp_pdi_mbx_read_complete | ( | PRUICSS_Handle | pruIcssHandle | ) |
Indicates to the firmware that PDI side read from write mailbox has completed.
| pruIcssHandle | PRUSS Handle |
| void bsp_pdi_mbx_write_start | ( | PRUICSS_Handle | pruIcssHandle | ) |
Indicates to the firmware that PDI side write to read mailbox has started.
| pruIcssHandle | PRUSS Handle |
| void bsp_pdi_mbx_write_complete | ( | PRUICSS_Handle | pruIcssHandle | ) |
Indicates to the firmware that PDI side write to read mailbox has completed.
| pruIcssHandle | PRUSS Handle |