AM263Px INDUSTRIAL COMMUNICATIONS SDK  10.02.00
Release Notes 09.02.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
For release notes of MCU+ SDK, please refer to AM263PX MCU+ SDK Release Notes 09.02.00.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless noted otherwise, the SW modules would work on all supported EVMs

New in this Release

Feature
EtherCAT SubDevice Beckhoff SSC Demo

Device and Validation Information

SOC Supported CPUs Boards Host PC
AM263Px R5F AM263Px ControlCard E2 Rev (referred to as am263Px-cc in code).
Windows 10 64b or Ubuntu 18.04 64b
AM263Px R5F AM263Px LaunchPad (referred to as am263Px-lp in code).
Windows 10 64b or Ubuntu 18.04 64b

Tools, Compiler and Other Open Source SW Module Information

Tools / SW module Supported CPUs Version
Code Composer Studio R5F 12.7.0
SysConfig R5F 1.20.0, build 3587
TI ARM CLANG R5F 3.2.2.LTS
FreeRTOS Kernel R5F 10.4.3
LwIP R5F STABLE-2_2_0_RELEASE
Mbed-TLS R5F mbedtls-2.13.1

Key Features

Fixed Issues

ID Head Line Module Applicable Releases Resolution/Comments

Known Issues

ID Head Line Module Applicable Releases Workaround
- - - - -

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Examples

Module Affected API Change Additional Remarks

Drivers

Module Affected API Change Additional Remarks