This software is designed for the TI SoCs with PRU-ICSS IP to enable customers add EtherNet/IP Adapter protocol support to their system. It implements EtherNet/IP + PTP + DLR functionality and provides EtherNet/IP ASIC like functionality integrated into TI SoCs.
EtherNet/IP firmware for PRU-ICSS is a black box product maintained by TI. EtherNet/IP Adapter FWHAL(Firmware and Hardware Abstraction Layer) allows loading and running EtherNet/IP firmware and acts as an interface with the firmware. FWHAL implements the key interface between EtherNet/IP Adapter firmware and EtherNet/IP Adapter stack.
| Record ID | Details | Workaround |
|---|---|---|
| PINDSW-4982 | SQE and Carrier Sense Errors counters not supported in EtherNet/IP | - |
| Folder/Files | Description |
|---|---|
| ${SDK_INSTALL_PATH}/examples/industrial_comms | |
| ethernetip_adapter_demo | EtherNet/IP Adapter Examples (based on pre-integrated stack) |
| ${SDK_INSTALL_PATH}/source/industrial_comms/ethernetip_adapter | |
| icss_fwhal/firmware | Firmware for the PRU cores in PRU-ICSS. Firmware Version : 5.5.7 |
| icss_fwhal/lib/ | FWHAL library for EtherNet/IP Adapter |
| icss_fwhal/*.c | FWHAL source files |
| icss_fwhal/*.h | FWHAL interface files |
| stack | Stack header files and stack library |
| Abbreviation | Expansion |
|---|---|
| PRU-ICSS | Programmable Real-Time Unit Industrial Communication Subsystem |
| DLR | Device Level Ring (A redundancy protocol) |
| PTP | Precision Time Protocol |
| OC | Ordinary Clock |
| TC | Transparent Clock |
| E2E | End to End |
Please see APIs for EtherNet/IP Adapter FWHAL for API documentation. It is recommended to use these FWHAL APIs in the stack adaptation files.
| Signal Name | Requirement | Description |
|---|---|---|
| PRU-ICSS MDIO | ||
| PR0_MDIO0_MDC | Mandatory | MDIO clock |
| PR0_MDIO0_MDIO | Mandatory | MDIO Data |
| PRU-ICSS Distributed Clocks (Network Clock synchronization) | ||
| PRGx_IEP0_EDC_SYNC_OUT0 | Mandatory (for PTP support) | SYNC0 out - Time synchronized OUT0 |
| PRGx_IEP0_EDC_SYNC_OUT1 | Optional | SYNC1 out |
| PRU-ICSS MII Port0 (IN Port) & PRU-ICSS MII Port1 (OUT Port) | ||
| MII0_RXD0 | Mandatory | MII0 and MII1 Receive Data0 |
| MII1_RXD0 | ||
| MII0_RXD1 | Mandatory | MII0 and MII1 Receive Data1 |
| MII1_RXD1 | ||
| MII0_RXD2 | Mandatory | MII0 and MII1 Receive Data2 |
| MII1_RXD2 | ||
| MII0_RXD3 | Mandatory | MII0 and MII1 Receive Data3 |
| MII1_RXD3 | ||
| MII0_RXDV | Mandatory | MII0 and MII1 RX Data Valid |
| MII1_RXDV | ||
| MII0_RXER | Optional | MII0 and MII1 RXERR |
| MII1_RXER | ||
| MII0_TXD0 | Mandatory | MII0 and MII1 Transmit Data0 |
| MII1_TXD0 | ||
| MII0_TXD1 | Mandatory | MII0 and MII1 Transmit Data1 |
| MII1_TXD1 | ||
| MII0_TXD2 | Mandatory | MII0 and MII1 Transmit Data2 |
| MII1_TXD2 | ||
| MII0_TXD3 | Mandatory | MII0 and MII1 Transmit Data3 |
| MII1_TXD3 | ||
| MII0_TXEN | Mandatory | MII0 and MII1 TX enable |
| MII1_TXEN | ||
| MII0_RXCLK | Mandatory | MII0 and MII1 Receive clock |
| MII1_RXCLK | ||
| MII0_TXCLK | Mandatory | MII0 and MII1 Transmit clock |
MII1_TXCLK | ||
Ethernet/IP Adapter examples uses the ICSS-EMAC as its base switch layer. The PRU Firmware provides switch functionality and additional PTP and DLR functionalities. The NRT(non-real time) traffic is handled by ICSS-EMAC, wherein the packets are forwarded either to the TCP stack or a custom callback (configurable in ICSS-EMAC).
Ethernet/IP packets are standard Ethernet frames and all protocol specific data is embedded in TCP/IP payload. Hence the standard switch model applies. Packets are segregated based on VLAN PCP field. The 8 priorities which map to 4 queues, with highest and next highest priorities going to Queue 0 and Queue 1 and so on. If PCP field does not exist, then frames go to Queue 3. All queues except the highest priority queue forward the frames to TCP/IP stack. Further if packet type does not match PTP or DLR then that frame goes to TCP/IP stack. The highest priority queues are used for PTP and DLR. These packets are directly forwarded to the registered callback in ICSS-EMAC (using rxRTCallBack).
EtherNet/IP firmware generates the following interrupts.
8 Host Interrupts (Host Interrupts 2 through 9) are exported from the PRU_ICSSG internal INTC for signaling the device level interrupt controllers. PRU_EVTOUT0 to PRU_EVTOUT7 correspond to these eight interrupts in the following table. Please check PRUICSS Interrupt Controller section for more details.
| Name | Host Interrupt | Description |
|---|---|---|
| Frame Receive | PRU_EVTOUT0 | Notifies host when firmware has stored a frame in host receive queue |
| DLR Port 0 Interrupt | PRU_EVTOUT1 | Raised when there is a state change in DLR on Port 0 |
| DLR Port 1 Interrupt | PRU_EVTOUT2 | Raised when there is a state change in DLR on Port 1 |
| Tx Callback Interrupt | PRU_EVTOUT3 | Raised when a PTP/1588 frame which requires Tx Timestamping is sent out |
| DLR Beacon Timeout Interrupt for Port 0 | PRU_EVTOUT4 | Raised when the beacon timeout timer on Port 0 expires |
| DLR Beacon Timeout Interrupt for Port 1 | PRU_EVTOUT7 | Raised when the beacon timeout timer on Port 1 expires |
| Link Change | PRU_EVTOUT6 | Interrupt is raised when the link on Ethernet PHY comes up or goes down |
Device Level Ring on EtherNet/IP firmware provides redundancy to the switch implementation. It is a beacon based implementation with support for a minimum beacon of 200us and timeout of 400us. More information is available in ICSS DLR Design.
PTP/1588 on EtherNet/IP provides time synchronization support. The implementation is driven by CIP Sync requirements which require End to End clock support over UDP (Annex D). EtherNet/IP adapter application supports both OC and TC implementations along with syntonization.
The VLAN Filter provides a robust and flexible way to filter the incoming traffic to the host processor. It enables precise control over the network traffic, allowing for improved network security and performance. For more details on the VLAN Filter implementation, refer to the ICSS EtherNet/IP VLAN Filter Design.
Please refer to below documents to understand more about EtherNet/IP Adapter on TI platforms and EtherNet/IP Adapter protocol specifications.
| Document | Description |
|---|---|
| EtherNet/IP on TI's Sitara processors | Application note by TI on the EtherNet/IP Adapter implementation on TI's Sitara Processors. |