AM263Px INDUSTRIAL COMMUNICATIONS SDK  10.02.00
EtherCAT SubDevice Setup with TwinCAT

Creating TwinCAT Project

  • Install TwinCAT3. A 7 days free trial license is available for free download from the Beckhoff's website. Select the eXtended Automation Engineering (XAE) mode of installation.
  • Copy the ESI file to {TWINCAT_INSTALL_DIR}\TwinCAT\3.1\Config\Io\EtherCAT folder.
    • ESI file for EtherCAT SubDevice application based on ETG stack is ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_slave/beckhoff_stack/esi/{PLATFORM}/TI_ESC.xml
  • Start the TwinCAT XAE Shell application.
  • Create a new TwinCAT XAE Project (XML format) by going to "File -> New -> Project -> TwinCAT Project"

    Creating a new TwinCAT Project
  • Go to "TwinCAT -> Show Realtime Ethernet Compatible Devices" and install TwinCAT RT Ethernet intermediate driver. For best performance, it is recommended to use a compatible NIC card listed in Supported network controllers . For the first time only you need to do this for the PC's Ethernet port, which is used as the EtherCAT port. Go to "TwinCAT -> Show Realtime Ethernet Compatible Devices" and check if the ethernet adapter is listed below "Installed and ready to use devices" before attempting to scan the SubDevice

Note
If your computer go to sleep and after awake it TwinCAT lost connection with SubDevice(s) and/or is not able to discover EtherCAT IO devices, you can fix this issue by going in TwinCAT to your Ethernet adapters, and disabling / enabling your NIC.
  • Connect Ethernet cable from PC running TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the EVM. If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).

Scanning the SubDevice

  • In Solution Explorer, go to "TwinCAT project -> I/O -> Devices". Right click on Devices and select Scan. Press OK in the next dialog to start scanning for EtherCAT devices.

  • Once an EtherCAT compatible device has been detected on this Ethernet port, the following dialog shows up. Note that there is a tick mark next to the adapter to which the EVM is connected. Press OK and confirm to start "Scan for boxes".

  • TI Box n(TIESC) will be detected automatically. The TI device will be listed "Box n (TIESC-*)". Press Yes to activate Free Run. This will put TI ESC into OP mode. TIESC number is based on the platform and application. Please check the ESI file for more details.

  • The EtherCAT device state can be displayed by selecting a "Device" (Double click on "Device") and then selecting the "Online" tab. The device should be in the OP state with no Lost Frames or Tx/Rx Errors.

  • The user can control 8 digital out LEDs using TwinCAT. LED[0] to LED[7] in "Box n (TIESC-*) -> DO Outputs -> LED". Each LED can be turned on and off by selecting "Online write 1" and "Online write 0" respectively.

Note
On am263px-cc, LED control is not supported right now.
  • Above steps test the SubDevice in Free Run Operation Mode. For testing Distributed Clock (DC) Synchronization mode, refer to the Testing DC Synchronization mode section.

Testing DC Synchronization mode

  • Launch TwinCAT XAE Shell application and discover all the SubDevices in SubDevice chain. Multiple SubDevices are required to make use of distributed clocks. Here, we have used two devices in the chain.
  • Choose DC Synchronization for all devices in the chain. Click on Box n (TIESC-*). Open the DC tab, and choose DC-Synchron option in Operation Mode. Do this for all SubDevices in the chain.

  • In Solution Explorer, go to TwinCAT project, select "SYSTEM -> Real-Time". In the Settings tab, choose the desired Base Time. With compatible NIC cards, a base time of as low as 50 us can be chosen.

  • Right-click on "SYSTEM -> Tasks". Click "Add New Item" on the pop-up menu. Select "TwinCAT Image with Task" in the next dialog box. Type a name for the task, and choose OK.

  • In the "Task" tab for the created task, select Auto Priority Management. Press OK in dialog box saying "Global Priority Management should be turned on".
  • Choose "Auto start" for the task. Choose 2 cycle ticks’ frequency for the task.

  • Add an output variable to the task. Right-click on "[Task name] -> Outputs", and choose "Add New Item". You may choose default options for the variable.

  • Link the variable to an output for the last SubDevice in the chain. Right-click on [Variable name], and choose "Change Link...".

  • Choose an output from the last SubDevice. You may need to choose "All Types" in "Show Variable Types".

  • You can launch into Run mode by clicking the "Activate Configuration" button on the toolbar.
  • Choose Yes to generate mapping after modifying configuration, click on OK to "Activate Configuration?", and Yes to Restart in RUN mode.

Configuring SYNC1 Shift from TwinCAT

The SYNC1 signal is used to synchronize the EtherCAT slave with the EtherCAT master. The SYNC1 shift configuration determines the timing of the SYNC1 signal with respect to the EtherCAT clock. This section provides a step-by-step guide on how to configure the SYNC1 shift from TwinCAT.

  • Launch TwinCAT XAE Shell application and discover all the SubDevices in SubDevice chain by following Scanning the SubDevice.
  • Choose DC Synchronization for all devices in the chain by following Testing DC Synchronization mode.
  • Once the variable is linked to an output for the last SubDevice in the chain, navigate to Box n (TIESC-*) > DC > Advanced Settings ...
  • Enable SYNC1 by checking the box and configure Shift Time in microseconds as follows:
    Configure EtherCAT SubDevice SYNC1 Shift
  • Post this, you can launch into Run mode by clicking the "Activate Configuration" button on the toolbar.

Check if SYNC1 Shift is correctly configured within the SubDevice

  • You can verify if the SYNC1 Shift is configured in the SubDevice by reading the ESC Register 0x09A4 through TwinCAT.
  • Navigate to Box n (TIESC-*) > EtherCAT > Advanced Settings ... > ESC Access > Memory. Here, you can see the register value (in nanosecond) of the SYNC1 Shift.
    SYNC1 Cycle Time Configuration

Testing Cable Redundancy

Cable redundancy is a feature which ensures that all SubDevices are accessible even if there is a single link break in the network between two ports of MainDevice. We need to ports of MainDevice for testing this feature.

It can be tested as follows:

  • Launch TwinCAT XAE Shell application and discover all the SubDevices in SubDevice chain. Here, we used two devices in the chain. The connections should be made as below:
    • MainDevice Port 0 to IN/Port0 of first device
    • OUT/Port1 of first device to IN/Port0 of second device
    • OUT/Port1 of second device to MainDevice Port 1
  • The topology can be verified by selecting a "Device" (Double click on "Device") and then selecting the "EtherCAT" tab and click on "Topology". It is also possible to use Beckhoff CU2508 (Real-time Ethernet port multiplier) if you do not have two ports available on MainDevice. You can connect CU2508 to PC running TwinCAT, and use two ports of CU2508 to connect to two EtherCAT SubDevice devices.

    In our case, we have used CU2508 , therefore you see three devices (one CU2508 and two SubDevice devices) between MainDevice ports in the image below.

  • Configure the redundancy mode in TwinCAT. Available options are described in Redundancy Mode section of TwinCAT 3 documentation. Please refer to Setting up: Device EtherCAT with cable redundancy for details on redundancy mode options to be used with CU2508.
  • Activate DC mode as shown in Testing DC Synchronization mode.
  • Ensure that both devices are in OP state. It can be displayed by selecting the "Device" (Double click on "Device") and then selecting the "Online" tab.

  • Break the link between OUT/Port1 of first device and IN/Port0 of second device. Both devices should still be in OP state.

Note
For this feature to work, enhancedlink_enable of bsp_params should be set to TIESC_MDIO_RX_LINK_ENABLE while initializing the EtherCAT SubDevice FWHAL. This configuration is done in tiesc_socParamsInit() in tiescsoc.c file.

Generating ESI Header file From ESI XML file

EtherCAT SubDevice Beckhoff SSC Example is expected to be used with ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_slave/beckhoff_stack/esi/{PLATFORM}/TI_ESC.xml file. If the application is modified to work with a different ESI XML file, user will need to update the corresponding ESI header file (tiesc_eeprom.h) and rebuild the application project.

  • Generate the binary file equivalent to ESI XML file:
    • Configure TwinCAT as mentioned in Creating TwinCAT Project and Scanning the SubDevice.
    • Click on the TI Box. Select "EtherCAT" Tab. Click on the "Advanced Settings" button.
    • Select "ESC Access -> E2PROM -> Hex Editor". Select "Write to File" and save the binary as a ".bin" file.
Note
Please make sure that "Upload" button is not clicked any time during this step. It will load the EEPROM data from TI ESC to TwinCAT memory.
  • Convert the binary file to header file using the bin2c tool. This tool can be found in ${SDK_INSTALL_PATH}/tools/bin2c folder. Example usage is shown below.
    python ${SDK_INSTALL_PATH}/tools/bin2c/bin2c.py "Box 1 (TIESC-004).bin" new_tiesc_eeprom.c new_tiesc_eeprom
Note
Please do not directly replace the existing tiesc_eeprom.h file with new header file.
  • Rebuild the application.

Online Application Upgrade

Note
Application should be loaded with SBL OSPI method to test this feature using following steps
  • Configure TwinCAT as mentioned in Creating TwinCAT Project and Scanning the SubDevice.
  • Click on TI Box. Select "Online" tab.
  • Click "Bootstrap" button. This will take the SubDevice to BOOT state.

  • Once the state has changed to "BOOT", Click "Download" button.

  • Rename your EtherCAT application binary (.appimage file) as ECATFW__, and use this file as your new EtherCAT application.

  • Locate the new application to be dowloaded click "Open".
  • Click OK on the new dialog shown.

  • This will download the new application. The progress bar will show the status of download.
  • Once the download has finished, change the state back to "Init" by clicking "Init" button.
  • Note that after changing from "Bootstrap" to "Init" state, the application will do a warm reset using SOC_generateSwWarmReset() API.
\image html EtherCAT_SubDevice_FOE_5.PNG

Load ESI file to EEPROM

The "EtherCAT SubDevice Information" is stored in the ESI EEPROM. The ESI EEPROM is located in the EtherCAT SubDevice Controller (ESC). It is a non-volatile memory used to store the ESC configuration and the device description. Reprogramming EEPROM is necessary to update the device details.

It can be reprogrammed as follows:

  • Copy the ESI file to {TWINCAT_INSTALL_DIR}\TwinCAT\3.1\Config\Io\EtherCAT folder.
  • Launch TwinCAT XAE Shell application and discover all the SubDevices in SubDevice chain and Activate Free Run.
  • Double click on the device(Box). Go to EtherCAT -> Advanced Settings.

  • Navigate to ESC Access -> EEPROM -> Hex Editor.

  • Choose the corresponding ESI to be loaded into the EEPROM and the press "OK".
  • Once above process is complete, come back to subdevice detail page and select the "Online" tab which has the "State Machine" options displayed.

  • Toggle the state from OP -> INIT -> PREOP -> SAFEOP -> OP.
  • Now the required ESI file is loaded to the EEPROM.