PROFINET Device4.2.0
 
Loading...
Searching...
No Matches
PN_APP_IOD_Nvdata Struct Reference

Profinet application non volatile structure. More...

#include <pn_app_iod_bsp.h>

Data Fields

uint32_t checkSum
 
uint32_t version
 
uint16_t ipSuiteLen
 
PN_API_IOD_IpSuite_t ipSuite
 
PN_API_IOD_Im1Data_t im1 [PN_API_IOD_MAX_NUM_OF_SUBSLOTS]
 
PN_API_IOD_Im2Data_t im2 [PN_API_IOD_MAX_NUM_OF_SUBSLOTS]
 
PN_API_IOD_Im3Data_t im3 [PN_API_IOD_MAX_NUM_OF_SUBSLOTS]
 
PN_API_IOD_Im4Data_t im4 [PN_API_IOD_MAX_NUM_OF_SUBSLOTS]
 
uint16_t snmpSysNameLen
 
uint8_t snmpSysName [PN_API_IOD_SNMP_SYSNAME_LEN]
 
uint16_t snmpSysContLen
 
uint8_t snmpSysCont [PN_API_IOD_SNMP_SYSCONT_LEN]
 
uint16_t snmpSysLocLen
 
uint8_t snmpSysLoc [PN_API_IOD_SNMP_SYSLOC_LEN]
 
uint16_t devNameLen
 
uint8_t devName [PN_API_IOD_DEVICE_NAME_LEN]
 
uint16_t pdevLen
 
uint8_t pdev [PN_API_IOD_PDEV_LEN]
 
uint16_t arfsuLen
 
uint8_t arfsu [PN_API_IOD_ARFSU_LEN]
 
uint16_t subCfgLen
 
PN_API_IOD_RemaDataSubmodCfgInfo_t subCfgList [PN_API_IOD_MAX_NUM_OF_SUBSLOTS]
 

Detailed Description

Profinet application non volatile structure.